This is the final blog for my project!
I have created a project that uses a dual-core system. Firstly there is the Arduino Uno, which is the main unit and which handles all the heavy lifting and the algorithmic work, and the ESP32, which is li...
As part of the element14 Smart Home & Healthcare Challenge, I am developing VitalSense Desktop R&D Workbench, an experimental PC-based platform for physiological data acquisition, visualization, and analysis.
The project is built around two e...
Recap: VitaRF is a small wrist sensor that reads heart rate, blood oxygen (SpO₂), skin temperature and movement, and sends it over Bluetooth to Home Assistant. The idea is simple: keep an eye on someone who lives alone, without making them wear anyth...
Introduction
At the very beginning, I would like to express my sincere gratitude to element14 for selecting me as one of the official challengers and providing the opportunity to develop and share this project. I also thank the kit sponsors for suppo...
Abstract
This project presents EdgeCare, an experimental wearable system designed for continuous physiological monitoring and metabolic trend analysis through the integration of multiple biomedical and environmental sensors. The proposed architecture...