Smart Home & Healthcare Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Home & Healthcare Challenge
  • More
  • Cancel
Smart Home & Healthcare Challenge
Forum EdgeCare: phase 3 - bracelet with two dry electrodes placed on the skin for the dielectric profile and more
  • News
  • Projects
  • Forum
  • Details
  • Leaderboard
  • Files
  • Members
  • DC
  • More
  • Cancel
  • New
Join Smart Home & Healthcare Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 17 subscribers
  • Views 178 views
  • Users 0 members are here
  • esp32C6
  • spo2
  • gsr
Related

EdgeCare: phase 3 - bracelet with two dry electrodes placed on the skin for the dielectric profile and more

mihaita802003
mihaita802003 1 month ago

EdgeCare: phase 1 - setup IDE, MCU and BLE - element14 Community

EdgeCare: phase 2 - setup I2C, read MAX30100 and create VI in LabView - element14 Community

EdgeCare will be a Multi-Sensor Metabolic & Autonomic Datalogging Wearable with LabVIEW R&D Analytics.

***********************************************************************************************************************************************************

OBS: at this moment, the sensors sent by element14 to me for this contest are blocked in custom because an issue with my EORI code.

I will continue to work on this project using MAX30100 and DS18B20 temperature sensor.

These sensors will be replaced if the competition package reaches me in time.

***********************************************************************************************************************************************************

In this post I will present the following implementations:

A. Determination of body hydration using the dielectric profile (using GSR, Tau and Temp);

B. Cardiorespiratory efficiency and tissue perfusion (using HR and SpO2);

C. The body's thermoregulatory response (using Temp + GSR);

A. Determination of body hydration using the dielectric profile (using GSR, Tau and Temp);

The circuit used to determine the dielectric profile for skin and to show the hydratation indes on the body can be one of the following solutions:

- a simple one with two resistors;

- with a specialized circuit, like AD5933 or MAX30009 (future implementation/upgrade).

I used first option, with two resistors and two ports from ESP32C6, like in the schematic diagram:

image

OBS: the circuit used to read the braceled dry electrodes are powered borm an power bank to avoid interferenced induced by the switching power supply and to have a total separation between sensors and PC with Labview.

All the calculation are done in LabView.

Parameter used:

- GSR (Rskin in Kohm) - measure the DC resistance of the skin; It is particularly influenced by surface moisture, perspiration and electrolytes.

- Skin capacity (Cskin) - It reflects the dielectric properties of deep cellular tissue (dermis and living epidermis); It depends directly on the bound and free water within the cells and in the interstitial space.

- Tau (Rskin x Cskin in us) - It measures the response speed to a transient pulse; It measures the rate at which the skin's dielectric capacitance charges and discharges in response to a pulse applied by the ESP32-C6.

The parameters Temp (using DS10B20 one-wire temp sensor with metalic capsule), GSR and Tau (using the bracelet two electrodes) are read by the ESP32C6  (see the photos below) and sent to LabVIEW for processing and display:

image    image    image

Algorithm: the processing is carried out in four main stages in LabVIEW (within the Formula Node):

Step 1: Thermal Compensation (DS18B20 Sensor)
Skin temperature alters electrical resistance through vasodilation/vasoconstriction. To eliminate temperature-induced errors:

Rcorr = GSR x (1 + alpha x (Tmasurat - 33.0))
(where alpha = 0.02, meaning a 2% correction per degree Celsius relative to the 33.0°C reference).
Step 2: Extraction of Dielectric Capacitance Cskin
By mathematically separating the time constant tau and the corrected resistance Rcorr:
Cskin (nF) = Tau (us) / Rcorr ()
OBS: The actual physical values ​​for the equivalent skin capacitance (Cskin) obtained using dry electrodes on the epidermis fall within the range of 0.2 nF – 5.0 nF (200 pF – 5000 pF),
depending on the hydration state, electrode surface area, and contact pressure.
Step 3: Normalization and Calculation of Hydration Index (0 - 100%)
The obtained value Cskin_nF is linearly scaled between the threshold for very dry skin (Cmin = 0.5 nF) and that for optimal hydration (Cmax = 3.0 nF):
Ih(%) = Clamp x [(Cskin - Cmin) / (Cmax - Cmin) X 100, 0, 100), 
where Clamp is a limitation fucntion used to mantined an interval between 0 and 100
Step 4: Safety Mask and Status Classification (status_code)
- Status 0 --> (Disconnected): used for GSR >= 9999 or Tau = 0; braceled/sensors are not in contact with skin;
- Status 1 --> (Dehydrated / Dried): Ih < 30%;
- Status 2 --> (Moderate hydratation): 30% <= Ih < 60%;
- Status 3 --> (Hydrated / Optimal): Ih >= 60%;
- Status 4 --> (Surface perspiration): Detected when Rcorr < 40 kΩ (presence of surface electrolytes, independent of the deep layer).
Status GSR value (Rskin) Skin capacity Cskin Fisiologin interpretation
Dehydrated / Dried  Big (> 200 kΩ) Low (<0.8 nF) Dry stratum corneum, low cellular volume.
Moderate hydratation  Medium (80 - 180 kΩ) Medium (1.0 - 2.2 nF) Optimal dermal/epidermal water balance.
Hydrated / optimal Normal-low (50 - 100kΩ) Big (2.2 - 3.5 nF) Well-hydrated interstitial tissue.
Surface perspiration  Very low (< 40 kΩ) Rapidly Changing Excess electrolytes on the surface (surface perspiration, not cellular hydration).

The function used in Labview for all above calculatiuon is this (in formula node):

// Intrari: gsr, tau, temp
// Iesiri: hydratation_index, c_skin_nF, status_code

if (gsr >= 9999.0 || tau == 0) {
    c_skin_nF = 0.0;
    hydratation_index = 0.0;
    status_code = 0; // Deconectat
} else {
    // 1. Compensare termica pentru GSR (Referinta: 33.0 °C, Coeficient: 2% per °C)
    float t_ref = 33.0;
    float alpha = 0.02;
    
    // Corectam GSR-ul daca temperatura este valida
    float gsr_corr = gsr;
    if (temp > 25.0 && temp < 42.0) {
        gsr_corr = gsr * (1.0 + alpha * (temp - t_ref));
    }

    // 2. Calcul capacitate dielectrici compensata
    c_skin_nF = tau / gsr_corr;
    // 3. Scalare Indice de Hidratare (0 - 100%)
    float c_min = 0.5; // nF
    float c_max = 3.0; // nF
    
    float raw_index = ((c_skin_nF - c_min) / (c_max - c_min)) * 100.0;
    
    if (raw_index < 0.0) raw_index = 0.0;
    if (raw_index > 100.0) raw_index = 100.0;
    
    hydratation_index = raw_index;

    // 4. Clasificare stare
    if (gsr_corr < 40.0) {
        status_code = 4; // Transpiratie / Hiperhidroza
    } else if (hydratation_index >= 60.0) {
        status_code = 3; // Hidratat / Optim
    } else if (hydratation_index >= 30.0) {
        status_code = 2; // Hidratare Moderata
    } else {
        status_code = 1; // Deshidratat / Uscat
    }
}
     image

Demo: 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

OBS: The EdgeCare system utilizes the parallel RC equivalent model for epidermal impedance described by Geddes & Baker (1989) and Martinsen & Grimnes (2011).

The determination of the dielectric capacitance (Cskin = Tau / R) and its scaling to derive the hydration index follow the dynamics of electrodermal activity (EDA) variation established by Boucsein (2012),

with a thermal correction using an alpha coefficient of 0.02°C applied in accordance with Wenig & Martinsen (2000).

B. Cardiorespiratory efficiency and tissue perfusion; apnea detection

This module assesses in real time how efficiently the cardiovascular system delivers oxygen to peripheral tissues and how the body reacts to stress or hypoxia.

To achive this, an new parameter is introduced: PI (Tissue Perfusion Index).

How it is working: PI it represents the ratio between the pulsatile alternating component (AC, pulsating arterial blood) and the non-pulsatile continuous component (DC, tissue, bone, static venous blood)

The formula used is this: PI = (AC / DC ) * 100%

Interpretation: 

- PI >=1.0%  - indicates good tissue perfusion in the finger;

- PI < 0.5% - indicates peripheral vasoconstriction, cold fingers, or a weak signal.

SpO2 and HR are both displayed on the same Waveform Chart with double Y-axes:

- on the left side is displayed HW that monitors variations in ventricular rate (40 --180 BPM), in pink colour;

-  on the right side is displayed SpO2 that mMonitors arterial oxygenation levels (70-100\%).

Apnea detection: the algorithm runs inside the Formula Node block in LabVIEW and evaluates the conditions for an episode of obstructive or central sleep apnea.

The algorithm and Labview implementation:

// Intrari: gsr, tau, temp, pi, spo2
// Iesiri: hydratation_index, c_skin_nF, status_code, low_perfusion, cardio_status, apnea_alert

// ==========================================
// 1. EVALUARE PROFIL DIELECTRIC (GSR + TAU)
// ==========================================

if (gsr >= 9999.0 || tau == 0) {
    c_skin_nF = 0.0;
    hydratation_index = 0.0;
    status_code = 0; // Deconectat
} else {
    // 1. Compensare termica pentru GSR (Referinta: 33.0 °C, Coeficient: 2% per °C)
    float t_ref = 33.0;
    float alpha = 0.02;
    
    // Corectam GSR-ul daca temperatura este valida
    float gsr_corr = gsr;
    if (temp > 25.0 && temp < 42.0) {
        gsr_corr = gsr * (1.0 + alpha * (temp - t_ref));
    }

    // 2. Calcul capacitate dielectrici compensata
    c_skin_nF = tau / gsr_corr;
    // 3. Scalare Indice de Hidratare (0 - 100%)
    float c_min = 0.5; // nF
    float c_max = 3.0; // nF
    
    float raw_index = ((c_skin_nF - c_min) / (c_max - c_min)) * 100.0;
    
    if (raw_index < 0.0) raw_index = 0.0;
    if (raw_index > 100.0) raw_index = 100.0;
    
    hydratation_index = raw_index;

    // 4. Clasificare stare
    if (gsr_corr < 40.0) {
        status_code = 4; // Transpiratie / Hiperhidroza
    } else if (hydratation_index >= 60.0) {
        status_code = 3; // Hidratat / Optim
    } else if (hydratation_index >= 30.0) {
        status_code = 2; // Hidratare Moderata
    } else {
        status_code = 1; // Deshidratat / Uscat
    }
}

// ==========================================
// 2. EVALUARE INDICE DE PERFUZIE (PI)
// ==========================================
int low_perfusion = 0;
if (pi > 0.0 && pi < 0.5) {
    low_perfusion = 1; // Vasoconstruc?ie / Degete reci
}

// ==========================================
// 3. STARE CARDIORESPIRATORIE
// ==========================================
// 0: Deconectat | 1: Normal | 2: Hipoxie | 3: Aritmie/Anormal
if (spo2 == 0 || hr == 0) {
    cardio_status = 0;
} else if (spo2 >= 95.0 && hr >= 50.0 && hr <= 100.0) {
    cardio_status = 1; 
} else if (spo2 < 90.0) {
    cardio_status = 2; 
} else {
    cardio_status = 3; 
}

// ==========================================
// 4. ALGORITM ALERTA APNEE ÎN SOMN
// Scadere SpO2 <= 92% corelata cu micro-trezire (HR >= 85 BPM)
// ==========================================
int apnea_alert;
if (spo2 > 0 && spo2 <= 92.0 && hr >= 85.0) {
    apnea_alert = 1; // Alerta apnee / desaturare
} else {
    apnea_alert = 0;
}
  image

Working mechanism:

- Respiratory pause (Apnea): During the cessation of breathing, blood oxygen levels begin to drop progressively;

- Desaturation (SpO_2 <= 92\%): When the SpO_2 level falls below the critical threshold of 92\%, the body enters a state of mild hypoxia;

- Micro-arousal / Sympathetic stress response (HR >= 85 BPM): The brain detects the lack of oxygen and activates the sympathetic nervous system, triggering a sudden increase in heart rate (compensatory tachycardia) to circulate the remaining oxygenated blood more rapidly;

- Signal validation (SpO_2 > 0): Prevents false alarms from triggering when the sensor is removed from the finger (disconnected state).

Demo:
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

OBS: The perfusion index (PI) was evaluated according to the methodology described by Allen [5], while the arterial desaturation thresholds for apnea follow the recommendations of Penzel et al. [7].

C. Detection of febrile conditions or heat shock.

The Temp + GSR (Body Thermoregulatory Response) module complements the EdgeCare biometric system by adding the component of metabolic and autonomic nervous system (ANS) assessment.

If oximetry (HR, SpO_2, PI) measures cardiorespiratory function, the combination Temperature + GSR monitors heat stress and electrodermal reactivity.

The role of parameters:
a. Peripheral/Skin Temperature (Temp):
- Febrile State / Hyperthermia (Temp > 37.5C): The body tries to eliminate excessive heat through peripheral vasodilatation and sweating.
- Heat Shock / Hypothermia / Vasoconstriction (Temp < 35.0C): The body redirects blood from the periphery to the vital organs (fingers become cold, correlated with a massive drop in PI).
b. Galvanic Skin Response (GSR / Electrodermal Conductance)
- The eccrine sweat glands are innervated exclusively by the sympathetic nervous system.
- In case of intense physical exertion, thermal shock, pain or emotional stress, sweat activity increases instantly.
- Water and minerals in sweat remove skin resistance and increase GSR conductance.

Code for this module (this code will be added in Formula node from Labview):

// Detectie Soc Termic sau Stare Febrila
if (temp > 38.0) {
    fever_alert = 1; // Indicator Febrăa/ Hipertermie
} else if (temp < 35.0 && pi < 0.5) {
    shock_alert = 1; // Indicator Posibil Soc Termic / Hipotermie
} else {
    fever_alert = 0;
    shock_alert = 0;
}
    image

Demo:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

OBS: to simulate fever in "The Body's termoregulatory Response" area I heated the temperature sensor a little above the trigger threshold of the alert.

D. Estimated Metabolic Inflection Indicator.

What is "Estimated Metabolic Inflection Indicator": this is a multisensor fusion algorithm that evaluates, in real time, the direction of blood glucose fluctuation (rising, stable, or rapidly falling). Without requiring blood sampling or subcutaneous sensors, the method monitors the neurovascular and autonomic footprint that metabolic changes leave on the body.

How is working: the algorithm relies on the involuntary reaction of the sympathetic nervous system (SNS) and the cardiovascular response to glucose fluctuations:
- During rapid drops in blood glucose (risk of hypoglycemia): The body releases adrenaline, triggering an acute "fight-or-flight" response. This manifests as cold sweating (a sudden rise in skin conductance/GSR), compensatory tachycardia (increased heart rate/HR), and peripheral vasoconstriction (a drop in the perfusion index/PI).
- During postprandial states (rise in blood glucose): The reaction is more gradual, characterized by incremental adjustments in skin temperature and GSR, without sudden adrenergic surges.

Code for this module (this code will be added in Formula node from Labview):

// ==========================================
// 6. ALGORITM pentru Indicator Estimat de Inflexiune Metabolica
// ==========================================
// Declarare variabile interne pentru stocare stare anterioara memorare esantion
float gsr_prev;
float hr_prev;

// Calculul variatiei rapide (derivata discreta)
float delta_gsr = gsr - gsr_prev;
float delta_hr = hr - hr_prev;

// Initializare scor: 0 = Stabil / Homeostazie
glycemic_trend = 0; 
glycemic_alert = 0;

// Verificare validitate date (evita alarme false la deconectare)
if (spo2 > 0.0 && hr > 0.0) {

    // 1. Trend de Scadere Rapida / Stres Metabolic Sympathetic (Risc Hipoglicemic)
    // Caracterizat prin: crestere brusca GSR (transpiratie) + accelerare HR + PI scazut (vasoconstructie)
    if (delta_gsr > 15.0 && delta_hr > 3.0 && pi < 1.0) {
        glycemic_trend = -1; // Trend descrescator (Scadere rapida)
        glycemic_alert = 1;  // Declansare alerta vizuala
    }
    
    // 2. Trend de Crestere / Raspuns Postprandial
    // Caracterizat prin: crestere lenta Temp/GSR fara peak-uri sau fluctuatii majore de HR
    else if (delta_gsr < -5.0 && temp > 36.6 && delta_hr >= -2.0 && delta_hr <= 2.0) {
        glycemic_trend = 1;  // Trend crescator
        glycemic_alert = 0;
    }
    
    // 3. Stare Stabila / Homeostazie
    else {
        glycemic_trend = 0;  // Stare neutra / stabila
        glycemic_alert = 0;
    }
}

// Salvare valori curente pentru esantionul urmator
gsr_prev = gsr;
hr_prev = hr;
   image

The front panel in Labview (no video provided, see last note):

image

OBS: The metabolic trend monitoring method integrated into the EdgeCare system is based on the multisensory fusion hypothesis validated in the scientific literature.

According to recent studies on autonomic responses to metabolic imbalances, a drop in glucose levels triggers acute sympathetic activation, manifested as rapid variations in electrodermal conductance (GSR) and peripheral hemodynamic adjustments derived from the PPG signal (HR, PI).

The algorithm developed in LabVIEW utilizes these discrete metrics to classify the trend of variation without requiring invasive devices.

IMPORTANT: With this final feature, I aimed to create a device capable of indicating potential rises, falls, or periods of stability in estimated blood glucose levels. To generate this estimate, I utilized GSR, HR, PI, and temperature parameters. This device is not intended to replace a standard glucometer, as the goal is to provide a rough estimate of the trend rather than a precise blood glucose reading; consequently, it should be regarded as an experimental device.

Note: this last module is purely theoretical and experimental; calibrating the algorithm requires a significant number of measurements taken at various times of the day, such as in the morning, after breakfast, before and after lunch, before and after dinner, and at night.
Therefore, this module will be updated once I have created the final hardware version: the wristband with the sensors and power supply installed.

Bibliography:

- Geddes, L. A., & Baker, L. E. (1989). Principles of Applied Biomedical Instrumentation (3rd ed.). John Wiley & Sons.

- Martinsen, O. G., & Grimnes, S. (2011). Bioimpedance and Bioelectricity Basics (3rd ed.). Academic Press.

- Wenig, P. B., & Martinsen, O. G. (2000). Thermal influence on skin bioimpedance measurements. Annals of Biomedical Engineering, 28(5), 582–588.

- Boucsein, W. (2012). Electrodermal Activity (2nd ed.). Springer Science & Business Media.

- J. Allen, „Photoplethysmography and its application in clinical physiological measurement”, Physiological Measurement, vol. 28, no. 3, pp. R1–R39, 2007.

- MAXIM Integrated, „MAX30100: Pulse Oximeter and Heart-Rate Sensor IC”, Datasheet & Application Notes, Rev. 0, 2014.

- T. Penzel, et al., „The apnea-hypopnea index: history, clinical use, and future potential”, Journal of Clinical Sleep Medicine, 2012.

  • Sign in to reply
  • Cancel
Parents
  • Qbit
    Qbit 14 days ago

    Nice update on the project mihaita802003 ! But if you used slightly bigger images it would be better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Qbit
    Qbit 14 days ago

    Nice update on the project mihaita802003 ! But if you used slightly bigger images it would be better.