Start a Movement Challenge
  • Challenges & Projects
  • Design Challenges
  • Start a Movement Challenge
  • More
  • Cancel
Start a Movement Challenge
Forum Thread Tapping System (Start a Movement Design Challenge))
  • Blog
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Start a Movement Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 45 subscribers
  • Views 1027 views
  • Users 0 members are here
  • dougw
  • thread tapping system
  • start a movement
  • tmc5272 evaluation kit
Related

Thread Tapping System (Start a Movement Design Challenge))

dougw
dougw over 1 year ago

Intro

This is a quick update in the Start a Movement Design Challenge to demonstrate the assembled thread tapping system with both stepper motors running.

The 6-32 tap that is in the chuck requires the lead screw to provide 1 inch of forward travel, for every 32 rotations of the tap bit.

Video - Assembled Thread Tapping System With Motors Running

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

The hardware for the thread tapping machine is now complete and working very well. The Analog Devices Trinamic stepper motor control system provides micro stepping control which allows the linear actuator to be precisely synchronized to the rotary actuator so that any tap can be accommodated. I am still at a loss as to how to get the system to use more than 30 mA, but the planetary gearbox provides so much torque multiplication, not much current is needed.

Links

  • Project Blog 1 - Unboxing
  • Project Blog 2 - Connector Tester Electronics and Firmware
  • Project Blog 3 - Linear Actuator
  • Project Blog 4 - Rotary Actuator
  • Project Blog 5 - Connector Tester Demo
  • Project Blog 6 - Thread Tapping System
  • Project Blog 7 - Project Summary and discussion
  • Start a Movement Design Challenge page
  • Analog Devices TMC5272 page
  • TMCL-IDE page
      • Sign in to reply
      • Cancel
      Parents
      • DAB
        DAB over 1 year ago

        Interesting approach.

        What types of materials do you think you can tap with it?

        • Cancel
        • Vote Up 0 Vote Down
        • Sign in to reply
        • Cancel
      • dougw
        dougw over 1 year ago in reply to DAB

        The taps can handle any material up to steel, but I only intend to tap plastic. For steel construction I would likely use screws and nuts or possibly sheet metal screws.

        • Cancel
        • Vote Up 0 Vote Down
        • Sign in to reply
        • Cancel
      Reply
      • dougw
        dougw over 1 year ago in reply to DAB

        The taps can handle any material up to steel, but I only intend to tap plastic. For steel construction I would likely use screws and nuts or possibly sheet metal screws.

        • Cancel
        • Vote Up 0 Vote Down
        • Sign in to reply
        • Cancel
      Children
      • DAB
        DAB over 1 year ago in reply to dougw

        That should work.