Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Documents Summer Of FPGAs - Design Challenge
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 23 Aug 2021 3:18 PM Date Created
  • Last Updated Last Updated: 3 Mar 2022 5:47 PM
  • Views 10656 views
  • Likes 15 likes
  • Comments 16 comments
Related
Recommended

Summer Of FPGAs - Design Challenge

image
Summer of FPGA Design Challenge

About this Challenge | Dates | The Judges | The Kit | The Prizes | Technical Resources | Example Application | Terms & Conditions | Related Blog | Summer of FPGAs: Digilent | The Challengers | The Winners

 

The Summer of FPGAs has been a groovy series of educational events on FPGA-related topics. Now, this is your chance to flex your FPGA muscles and put your skills to the test, by enrolling in our latest design challenge!

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Challenge

 

The element14 Community is pleased to introduce the Summer of FPGAs Design Challenge, in partnership with Digilent.

 

Submit your application with a summary describing an FPGA project of your choice, using Diglient's Cmod S7 for a chance to win a range of amazing prizes. The possibilities are endless—refer to the examples below to see what you could build.

 

The Cmod S7 is a small, 48‐pin DIP form factor board, built around the Xilinx Spartan 7 FPGA. The selected 30 challengers will receive the FREE board to help power up their FPGA project!

 

What can you build?

Example applications could include:

 

  • Image Recognition
  • Home Scientific Equipment
  • Signal Processor
  • Proof of Concept
  • Processor Off Loading System

 

The Sponsored Kit The Specs

Digilent Cmod S7

image

 

 

Buy NowBuy Now

It has 32 FPGA digital I/O signals, 2 FPGA analogue input signals, an external power input rail, and ground are routed to 100‐mil‐spaced through‐hole pins. The Cmod S7 is well suited for use with solderless breadboards. At just 0.7" by 3.05" inches, it can be loaded in a standard socket and used in embedded systems.

 

The board also includes a programming ROM, clock source, USB programming and data transfer circuit, power supplies, LEDs, and buttons.

  • Xilinx Spartan‐7 FPGA (XC7S25‐1CSGA225C)
  • 4MB quad‐SPI flash memory
  • Powered from USB or 5V external supply connected to DIP pin 24
  • USB‐JTAG programming circuitry, USB‐UART bridge
  • Push‐buttons and LEDs
  • Expansion connectors
  • 48‐pin DIP form‐factor header

 

 

Be Rewarded on the Community

For entering and taking part in the Design Challenge competition, you'll be rewarded the following badges:

 

image Apply to join the Design Challenge and receive a badge and points for applying! Make sure you've thought your application through, made it original and your own work. If you are building upon someone else's work, make sure you cite your sources. Direct copies of work will not be accepted.
image Post your first blog! We expect updates on how your Design Challenge project is going, so don't hold back, tell us your thoughts, difficulties, and how you're progressing. Remember that you're assessed based upon your updates, and don't be afraid - other challengers and members are there to help you with any problems you have, and it helps the staff to keep an eye on you!
image 5 blogs! Wow, has it really been that long? We hope you'll keep us updated about your project at least once every two weeks, for 10 weeks. We'll not be impressed if you only put a one-liner in there, that's what messages are for. Blogs are to make sure you're giving us all of the juicy detail, trials and tribulations of what's going on, and it keeps everyone honest!
image Even if you're not a challenger in the Design Challenge, we appreciate every member who joins in and gives a helping hand to applicants and members. If your messages are found to be helpful, we want to acknowledge that and reward you!

 

The Prizes

 

Prize Prize Category

image

Grand Prize*

  • Digilent Analog Discovery Pro AD3450 USB

image

Runner Up*

  • Digilent Analog Discovery Pro ADP 3250
  • Digilent Digital Discovery
finisher prize

Finisher Prize

 

Multicomp Digital Multimeter

*Or local equivalent

 

The Judges

 

Digilent
Technical Judge Team
image
element14 Community Judges
element14 Community Team
image

 

 

Need help? Comment and read the resources below:

Technical Resources:

image

Start up Reference:

https://reference.digilentinc.com/reference/programmable-logic/cmod-s7/start

 

User Manual:

https://digilent.com/reference/programmable-logic/cmod-s7/reference-manual?redirect=1

 

Use Xilinx Analog-to-Digital (XADC) with breadboardable Spartan 7 FPGA module

Use Xilinx Analog-to-Digital (XADC) with breadboardable Spartan 7 FPGA module

 

Mechanical Drawings (DXF)

https://digilent.com/reference/_media/reference/programmable-logic/cmod-s7/cmod_s7_dimensions.zip

 

image

Callout Description Callout Description
1 48-pin DIP form factor head 7 UART status LED
2 FPGA programming DONE LED 8 Shared USB JTAG/UART port
3 Pmod connector 9 Power good LED
4 User push buttons 10 Spartan-7 FPGA
5 User LEDs 11 SPI Flash
6 Use tri-color LED

 

Example Projects

  • Analyzing DAC, ADC, and SPI Data with the Analog Discovery Studio
  • Cmod S7-25 Microblaze XADC Demo
  • Cmod S7-25 Out-Of-Box Demo
  • Pmod I2S2 FPGA Volume Control Demo

 

Software Notes:

The Cmod S7 can be programmed with Digilent's Adept software. Digilent Adept is a unique and powerful solution which allows you to communicate with Digilent system boards and a wide assortment of logic devices. Find out more about Adept here.

To create and modify designs for your Cmod S7, you can use Xilinx's Vivado Design Suite. Vivado is a software designed for the synthesis and analysis of HDL designs. Both variants of the Cmod S7 are supported by the free WebPACK edition of the Vivado Design Suite.

If you are using the MicroBlaze Soft Processor Core from Xilinx, you can make use of the Vitis Core Development Kit or Xilinx Software Development Kit to create embedded applications for your Cmod S7.

The Dates

 

To make enough time for the holiday period and delivery of the kits, we have updated the Project Due deadlines.

 

Updated Competition Dates

Project Phases

Dates

Application Period CLOSED
Application Deadline CLOSED
Challengers Announced CLOSED
Build Period 22nd November 2021 - 31st January 2022
Projects Due 31st January 2022
Winners Announced February 2022
Prizes Shipped February 2022

 

 


The Terms

 

Selected official applicants will be chosen to receive the "Kit" listed above. These successful applicants will be our sponsored challengers, and they must use Diglient's Cmod S7 within their project, and publish their final code and designs on the Community for others to use. Those not chosen as sponsored challengers may also join the competition and be eligible to win prizes, but they must base their projects around the kit listed above and adhere to all terms and conditions of the challenge.

They need to post their progress and final project as at least 5 blog posts before the closing date (see above), when projects are due.

Posts which use the FPGA most creatively, are media rich with photos, videos, and code samples will be viewed more favorably in the judging process.

Please read the full terms and conditions of the challenge, attached below.

 

Ready to join the challenge? Then Apply Here!

 

If you are not successful in becoming a sponsored challenger but still want to enter, all you need to do is use the Kit as described above in your project and adhere to the same Terms and Conditions for a chance to be our winner! Non-sponsored challengers are eligible for the Finisher and Winner Prizes as well.

Attachments:
image Summer Of FPGA Design Challenge Terms Version 1.pdf
  • design_challenge
  • summer_of_fpga
  • digilent
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14phil
    e14phil over 4 years ago +2
    Hello, Challengers and extended Deadlines will be announced by Tuesday 16th of November. riyosasuke76
  • e14phil
    e14phil over 4 years ago +2
    The element14 Community is pleased to introduce the Summer of FPGAs Design Challenge , in partnership with Digilent . Join me in congratulating the Official Challengers of the Summer of FPGA Design Challenge…
  • jc2048
    jc2048 over 5 years ago +1
    Useful prizes - the VNA and impedance analyser capabilities of the Discovery Pro look interesting. A great way to learn analog electronics. The FPGA on the Cmod S7 board looks quite capable, so hopefully…
Parents
  • kluivertcorreia
    kluivertcorreia over 4 years ago

    Hello e14phil, Is it possible to extend the deadline for the submissions by say a week or more (ideally 10 days)? Since I need to order a few parts that may take some time.

    Regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kluivertcorreia
    kluivertcorreia over 4 years ago

    Hello e14phil, Is it possible to extend the deadline for the submissions by say a week or more (ideally 10 days)? Since I need to order a few parts that may take some time.

    Regards