Summer of Sensors Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Summer of Sensors Design Challenge
  • More
  • Cancel
Summer of Sensors Design Challenge
Blog Phase 3: Build - Intergration with Golfcart, Final Thoughts
  • Blog
  • Forum
  • Documents
  • DesignChallenge
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Summer of Sensors Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: DeltaPi
  • Date Created: 17 Nov 2022 3:54 AM Date Created
  • Views 1547 views
  • Likes 8 likes
  • Comments 5 comments
  • vishay
  • build
  • Summer of Sensors Design Challenge
  • SensorXploror
Related
Recommended

Phase 3: Build - Intergration with Golfcart, Final Thoughts

DeltaPi
DeltaPi
17 Nov 2022
Phase 3: Build - Intergration with Golfcart, Final Thoughts

Welcome 

Welcome back to my final blog of this competition. These last few months were fun and very educational, and I hope to compete again in one of these again someday. In this final blog post I will show you how I got the circuit and sensors integrated in my golfcart. 

Circuit Board

Here is a picture of the board I used to solder the circuit from last blog on. It fits right on top of the Arduino Uno using some pins on the bottom. This is called a 'hat' for the Arduino, and is common practice used with small circuits to save space. Some manufacturers make premade boards that sit on Arduinos and have function such as reading an SD card or adding a GPS module. The often have headers on top that allows them to be stacked as well. I only need four wire to go to the sensors, the I2C bus (SDA + SCL), 3.3v, and GND. The two large red and black wires go to the buzzer.

image

image

The Build

The wire I used for the sensors I got at a yard sale for cheap and has five solid core wires running through it.

image

image

On the golfcart itself I drilled some holes to mount the sensors, the gesture sensor on the back between the brake lights, and the color sensor on the front in the empty space under the dash.

image

image

I also put the Arduino & circuit board under the dash behind the ignition key, where I ran the wire for the proximity sensor.

image

To protect the sensors from the elements I put them each in a waterproof clear plastic box, since when I ran test on the I found they both work fine with a thin piece of clear plastic in front of the sensors.

Here is a simple video showing the sensors on the golfcart. The color sensor isn't installed on the cart yet, but I do have it connected. The proximity sensor is installed and working, which I am happy about. Final Video

Final Thoughts

I am happy I was able to complete my project, as well as learn along the way. There are a few changes I would make in retrospect, among these would be using a music player module with the Arduino instead of the Raspberry pi, as it has a longer start up time then I would prefer, as well as finding a use for the gesture sensing part of the VCNL4035X01 sensor. I also hope I was able to present my journey of discovery well over the last few months and would like to thank the Element14 community for picking me for this competition! Thank you all for reading my blogs, if you missed the last few, I'll put the links to each of my previous blogs below. 

Phase 1: Planning

Phase 2: Research and Design - Building a Low Voltage Disconnect (LVD) Circuit

Phase 2: Research and Design - Solar Panel Mounting & LVD Circuit Findings

Phase 2: Research and design - Pseudo code for SensorXplorer Board and Programming Raspberry Pi

Phase 2: Research and Design - Prototypes and Programs

Unboxing: They Came!

Phase 2: Research and Design - Arduino Integration of Sensors

  • Sign in to reply
Parents
  • dougw
    dougw over 3 years ago

    It would be nice to see a walk around video/demo showing all the features in operation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DeltaPi
    DeltaPi over 3 years ago in reply to dougw

    Here you are, I am also putting it in the post itself. It is not an amazing video, but I hope it displays the systems on the golfcart.

    https://youtu.be/ynv6Bkd-11Q

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DeltaPi
    DeltaPi over 3 years ago in reply to dougw

    Here you are, I am also putting it in the post itself. It is not an amazing video, but I hope it displays the systems on the golfcart.

    https://youtu.be/ynv6Bkd-11Q

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 3 years ago in reply to DeltaPi

    Thanks, That provides a good perspective of what the system is. Nice project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DeltaPi
    DeltaPi over 3 years ago in reply to dougw

    Thank you.