Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Sustain the World with Smart Farm Hoe (Blog 10)
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
  • Author Author: asokfair
  • Date Created: 6 Oct 2020 4:59 PM Date Created
  • Views 2743 views
  • Likes 6 likes
  • Comments 3 comments
  • infineon
  • hoe
  • sustain_the_world
  • winners
  • smart
  • farming
Related
Recommended

Sustain the World with Smart Farm Hoe (Blog 10)

asokfair
asokfair
6 Oct 2020

Introduction:

Hi everyone, this is my final project demonstration of "Smart Farming Hoe". Checkout my earlier blogs [Blog1 , Blog2 , Blog3, Blog4, Blog5, Blog6, Blog7, Blog8, Blog9 ]

from unboxing to product prototype design. This blog explains about the overall design concepts and how it works.

 

Smart farming Hoe:

The problem what i see in today's world is "Farmers" count is decrementing day by day. Since I'm from the background of agriculture family i had seen

what are the problems farmers will face in the field. To overcome that i have build this smart farming hoe. 15 years back i had idea of adding LED lights

into the hoe to help the farmers during night time. And today i have but this smart hoe to control the water flow and lights.

image

 

Smart Farming Hoe has two setup.

1. Base Station

2. Remote

 

Base Station:

Base station is build with Infineon XMC4200 Platform2GO kit and PROFET 12V Switch Shield. The Cypress BLE MESH kit is interfaced to XMC4200

over UART communication. The Base Station is powered through 12V 7.5Ah battery. This battery is changed via 20watt solar panel with Luminous controller.

12V DC submersible water pump and 12V LED's are connected to PROFET+2 switch outputs.

image

Remote:

The remote is just BLE mesh Kit. OLED display is interfaced for user interface. The kit has push button used for control and changing the mode .

This setup is powered via AAA battery. The removable battery holder is attached in it. This entire setup is wrapped into the small size Wooden Hoe.

Its just concept demonstration , in practical scenario this setup will be embedded inside the wood with carving.  I painted the wood and did some

stickering.

 

Blocks:

image

Working:

The base station MESH kits act as a server,it works in a vendor specific model. It receives the data from the client (smart hoe)

and sends to the XMC4200 kit over uart communication with 921600 baudrate. The XMC4200 MCU processes the UART data

and controls the port pins based on the data status.

The data frame is 8 bytes length UTF-8. RTC is used for getting time for timer mode. E Ink display shows the status of the

system. Also the battery information charging status can be monitored through wirelessly but currently not implemented.

 

In the smart Hoe side, the MESH kit acts as a client and sends the data on button status change. Short button press changes the

states of the Light or Motor.Button press and hold for 3 secs, changes the modes (LIGHT,MOTOR & TIMER). Also some of the

features can be added in future like sensing soil or plants and etc.

 

The experimental code is here https://github.com/embeddedclub/sustaintheworld/upload/main

image

Use-cases:

1. Farmers can control the water flow from hand.

2. Outdoor lights control in home gardening

3. Sensing the Hoe usage for AI robotics.

 

The working video is here.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Some more details may be added in future.

 

Thank you!

Ashok r

  • Sign in to reply

Top Comments

  • rati89
    rati89 over 6 years ago +2
    Wow really great work! The prototype looks amazing, as well as the overall setup, which is super clean and tidy! Also nice descriptions of your blogs. Well done, you can be proud of yourself. BR Brew
  • asokfair
    asokfair over 6 years ago in reply to rati89 +1
    Thank you Mr Brew
  • dubbie
    dubbie over 6 years ago +1
    Looks interesting. Dubbie
  • dubbie
    dubbie over 6 years ago

    Looks interesting.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • asokfair
    asokfair over 6 years ago in reply to rati89

    Thank you Mr Brew image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rati89
    rati89 over 6 years ago

    Wow really great work! The prototype looks amazing, as well as the overall setup, which is super clean and tidy! Also nice descriptions of your blogs.

    Well done, you can be proud of yourself.

     

    BR

    Brew