Twist, Turn and Move Design Challenge with TE Robotics
  • Challenges & Projects
  • Design Challenges
  • Twist, Turn and Move Design Challenge with TE Robotics
  • More
  • Cancel
Twist, Turn and Move Design Challenge with TE Robotics
Blog ARDUMOBO blog 2: Testing
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: a33333
  • Date Created: 14 Aug 2022 12:54 PM Date Created
  • Views 1058 views
  • Likes 6 likes
  • Comments 2 comments
Related
Recommended

ARDUMOBO blog 2: Testing

a33333
a33333
14 Aug 2022

Preliminary work

I removed the cabin of the truck and took out the windshield so I have more room for mounting the control hardware and power supplies on the truck.

image

I then tested the remote controlled car. It is in working condition. Car is powered by 5 AA batteries in series (7.5V). I made a couple of measurements: the two engines (direction and traction) are controlled by applying a 7.5V voltage directly to the engine. To reverse traction (forward/reverse) and steering (left/right), the polarity of the control voltage is changed. 

I plan to use two independent power supply for the Arduino and the two engines:

  • one 5V power bank to power up the Arduino Uno.
  • one 6V power supply. (4 AA batteries in a plastic case with an on/off switch) to power up the two electric motors.   

I disconnected the cables from the two motors and connected them to the 6V power supply. I measured the current through the engines: 460mA for the direction engine, 350mA for the steering engine. When powered from 6V the steering engine does not turn the wheel to the maximum steering angle but I think that the smaller steering angle might be enough for my robot. If a larger steering angle is needed, I will have to use a higher voltage power supply.

I would like to keep the existing female connectors on the engine wires so that I can restore the truck to its original condition, just in case future younger generations in my family would favor manual control over autonomous robot control for this toy truck. Luckily I found a matching set of male contacts in my parts box (no idea of type/brand) and built two pairs of cables to connect the engines to the Arduino driver shield.

  image

After the testing is completed, I will start using the connectors from the kit.  

Testing

I plugged the DFROBOT DRI0017 shield into the Arduino Uno, connected the engines wires and the power supply to the shield.

image

I wrote an Arduino sketch that loops through this testing sequence:

  • turn traction engine in forward mode for 3 seconds
  • stop for 3 seconds
  • turn traction engine in reverse mode for 3 seconds
  • stop for 3 seconds
  • turn steering engine right for 3 seconds
  • stop for 3 seconds
  • turn steering engine left for 3 seconds
  • stop for 3 seconds

The following clip shows the testing sequence.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

  • Sign in to reply
Parents
  • robogary
    robogary over 4 years ago

    Depending on the The 5V power bank ratings,  may have enough guts to power the motors as well. Yes it wont be fast but saves the weight of 4 AA batteries. The steering motor in the smaller cars just use a DC motor and drive it until it stalls into the return spring. A smaller voltage gives smaller stall current. A these small amps, a boost power supply can be used too.   You can also reference a similar past project if it can be helpful.  /challenges-projects/project14/radiocontrol/b/blog/posts/rc-toy-hack---rc-car-rescue-restore-recycle-retrofit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago

    Depending on the The 5V power bank ratings,  may have enough guts to power the motors as well. Yes it wont be fast but saves the weight of 4 AA batteries. The steering motor in the smaller cars just use a DC motor and drive it until it stalls into the return spring. A smaller voltage gives smaller stall current. A these small amps, a boost power supply can be used too.   You can also reference a similar past project if it can be helpful.  /challenges-projects/project14/radiocontrol/b/blog/posts/rc-toy-hack---rc-car-rescue-restore-recycle-retrofit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • a33333
    a33333 over 4 years ago in reply to robogary

    Thanks for the link. Nice project!