Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog PDU 10 - The Mount and Successful Test! [Upcycle It]
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
  • Author Author: jasonwier92
  • Date Created: 20 May 2017 7:58 PM Date Created
  • Views 1196 views
  • Likes 7 likes
  • Comments 5 comments
  • mqtt
  • upcycle it
  • upcycled_pdu
Related
Recommended

PDU 10 - The Mount and Successful Test! [Upcycle It]

jasonwier92
jasonwier92
20 May 2017

Success Is Worth Sharing

Today was my test of my system and it was successful.  Here is a video showing it working.

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

(Video is not the best as it shows extra command that are in the future.)

 

Here are some pictures of what I tested

{gallery} My Gallery Title

image

Edison interface to protoboard

image

Ribbon header goes to Relay board

image

Top view!!

image

Relay board hooked up and running.

 

 

 

Here is the Node-Red flow that I used to test with.  Note the first flow, it does monitor the GPIO for changes and with the RBE (Report By Exception) will tell us when the value changes.  I will use this to send out messages on change of outlet statuses and to store that information in the Mongo database.

image

Edison Interface

I used my protoboard to create 4 rows of male header pins to interface with the 4 rows of female header pins I had put on the Edison Mini board earlier.  Then I wired up pin J17-4 to 12V and pin J19-3 to ground.  I wired up GPIO lines from J20-4 through J20-11 to the header going to the relay board. The 12V is also taken to this header so that it can be converted to 5V and returned for future use.

 

This week gpolder posted the following image on Workshopshed's post and it gets my vote for the most useful.  Some pins cannot be used, so I tested them before hand to make sure that J20-4 ... J20-11 could all be used for GPIO.  For example GP134 on pin J20-3 does not work in Node-Red with the Johnny-Five controls.

image

 

GPIO
Output Label
GP78Outlet 1
GP41Outlet 2
GP84Outlet 3
GP42Outlet 4
GP15Outlet 5
GP49Outlet 6
GP47Outlet 7
GP45Outlet 8

 

 

About The Video

Video was a screen capture with a webcam feed and putty shell.  Here is my webcam setup.  Yes, it is an old Android phone running as a web cam.

image

 

Finishing List

  • Shift converters with LCD
  • Mount LCD
  • Mount Relay board and Edison board
  • Wire relay board to outlets
  • Web interface
  • MQTT emergency response
  • LED indicators
  • Something cool in the old Serial port hole
  • Sign in to reply
Parents
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago

    Good job.

    Up and running, great.

    Node-red, helpful or not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago

    Good job.

    Up and running, great.

    Node-red, helpful or not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jasonwier92
    jasonwier92 over 9 years ago in reply to konstantinoskonstas

    I could have done it faster using just Node, but I wanted to learn to do things in Node-Red.  I think  you can do stuff faster in Node-Red and the visual makes it great to share.  People can look at a glance to see what is happening rather than parsing through many lines of code.