Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Funeka - The Skull #9 : I smell heat...
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
  • Author Author: sakthi.1260
  • Date Created: 21 May 2017 1:00 PM Date Created
  • Views 2017 views
  • Likes 4 likes
  • Comments 6 comments
  • upcycled_funeka
  • i2c
  • omron d6t
  • servo
  • intel edison
Related
Recommended

Upcycle It - Funeka - The Skull #9 : I smell heat...

sakthi.1260
sakthi.1260
21 May 2017

Hey fellas...

 

Here comes this week's update, something I wanted to do for a long time, but the Upcycle Challenge made me to do it image...

 

I wanted to re-purpose the Omron D6T, I2C MEMS IR sensor to track movement and direction. The one I'm using here is Omron D6T-8L, with 8 pixels.

 

How its works:

 

The sensor has a resolution of 1x8, what I've done is read all the 8 pixel values and find the largest of it and the  corresponding pixel and map the value to a Servo.

 

The Setup:

image

 

Connections

 

Omron D6T     EDISON

SCL        -->        SCL

SDA        -->        SDA

5V           -->         5V

GND        -->        GND

 

Servo                     Edison

Signal      -->     Any PWM pin

5V            -->             5V

GND        -->            GND

 

The Code :

 

#include <Servo.h>
#include <Wire.h>

#define D6T_addr 0x0A // Address of OMRON D6T is 0x0A in hex
#define D6T_cmd 0x4C // Standard command is 4C in hex

Servo myservo;

int tmax, imax;
int numbytes = 19;
int numel = 8;
int rbuf[19];
int tdata[8];
float t_PTAT;
int deg;
int i;

void setup()
{
  Wire.begin();
  Serial.begin(9600);
  myservo.attach(5);
  myservo.write(90);
  }

void loop()
{
  tmax = 0;
  imax=0;
  Wire.beginTransmission(D6T_addr);
  Wire.write(D6T_cmd);
  Wire.endTransmission();

  delay(70);
  Wire.requestFrom(D6T_addr, numbytes); // D6T-8 returns 19 bytes

  if (0 <= Wire.available()) { // If there is data still left in buffer
    i = 0;
    for (i = 0; i < numbytes; i++) {
      rbuf[i] = Wire.read();
    }
    t_PTAT = (rbuf[0] + (rbuf[1] << 8) ) * 0.1;
    for (i = 0; i < numel; i++) {
      tdata[i] = (rbuf[(i * 2 + 2)] + (rbuf[(i * 2 + 3)] << 8 )) * 0.1;
      //Serial.print(tdata[i]);
      //Serial.print(",");
    }
    //Serial.println();

  }

      for (i = 0; i < numel; i++)
    {
      if (tmax <= tdata[i])
      { tmax = tdata[i];
        imax = i;
        Serial.println(imax);
      }
    }
  deg = map(imax, 0, 7, 60 , 120);
  myservo.write(deg);
  delay(10);
  
  
}

 

Lets Track...

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I made a simple mechanism to make the eyes move, i thought of 3d printing them but old acrylic pieces and a few match sticks came handy. also mounted with the skull.

imageimage

 

You guys will be meeting Funeka mostly my 28th image Here's some sneak peek

 

image

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +2
    Heat seeking eyeballs - that is simply awesome.
  • Workshopshed
    Workshopshed over 9 years ago +2
    Great result with the Omron board, I think following eyes is going to freak most people out.
  • sakthi.1260
    sakthi.1260 over 9 years ago in reply to dougw +1
    wanted to do this for a long time, this challenge was the right excuse
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Great result with the Omron board, I think following eyes is going to freak most people out.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 9 years ago

    Great result with the Omron board, I think following eyes is going to freak most people out.