Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Washing Machine Hydroponic Grower - #9 Interfacing Edison X Grower
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
  • Author Author: nandohila
  • Date Created: 4 Jun 2017 12:13 PM Date Created
  • Views 1593 views
  • Likes 2 likes
  • Comments 7 comments
  • hydroponics
  • upcycle it
  • washing_machine
Related
Recommended

Upcycle It - Washing Machine Hydroponic Grower - #9 Interfacing Edison X Grower

nandohila
nandohila
4 Jun 2017

Details of electrical connections for the grow light and water pump

 

The relays that switch the light and the water pump were enclosed inside a junction box so there are no exposed wires and terminals for this part of the circuit.

The control cables came through the bottom of the box, just next to the Edison Board. The relay block has 4 relays but at this stage, I am using only 2.

The other 2 I will have as spare as I have plans to install an air blower to force air into the drum if it gets too hot or too humid and an air pump to aerate the nutrient.

imageimage

imageimage

 

Edison/Arduino Board & LCD Display

 

The Edison board was fixed next to the relay "junction" box. The display was mounted in a piece of timber and fixed on the top frame facing the front of the machine. The PH sensor board was mounted on the back of the same mounting.

imageimage

imageimage

image

 

Temperature/Humidity & Light Sensors

 

The sensors to monitor the drum temperature, humidity and light intensity were fixed on the light mounting. This is the only spot I could find that will not be on the way of the moving plants or blocking the light.

imageimage

 

Stepper Motor/Driver

 

It was mounted in the frame next to the stepper motor.

 


image

 

 

PH probe/board

 

The PH probe was fixed in the dump pipe with a metal clip secured by a cable tie.

 

imageimage

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +2
    Fernando, I saw the video you posted in replay to my answer about the gravity question and - obviously - I compared this industrial versions with your setup and I should admit that you was really good…
  • DAB
    DAB over 9 years ago +1
    Nice clean build. Looks good and easy to maintain/mod. DAB
  • Workshopshed
    Workshopshed over 9 years ago +1
    Hey Fernando, just catching up on the posts. A good setup you've got there!
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    Fernando, I saw the video you posted in replay to my answer about the gravity question and - obviously - I compared this industrial versions with your setup and I should admit that you was really good in your building. Maybe a good recycling project for all.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nandohila
    nandohila over 9 years ago in reply to balearicdynamics

    Thank you, Enrico.

     

    I also found that using the washing machine ended up in a very solid and reliable mechanism, probably stronger than the commercial units. The only disadvantage I see is the size as I cannot grow anything taller than 30cm. Anyway, I might look for an industrial washing machine to upgrade it in the future.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • nandohila
    nandohila over 9 years ago in reply to balearicdynamics

    Thank you, Enrico.

     

    I also found that using the washing machine ended up in a very solid and reliable mechanism, probably stronger than the commercial units. The only disadvantage I see is the size as I cannot grow anything taller than 30cm. Anyway, I might look for an industrial washing machine to upgrade it in the future.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to nandohila

    The size maybe an issue, especially if you plan to grow palm plants (bu banas are better, duh?)

    Seriously, ss far as what i see also the industrial systems are just for an averagr small plants.

    Thisbmethos is great for lettuce growing and it is already a great building... I have in mind to do something similar replicating your project in the future. I need a couple of months befote starting but I will do.

     

    BTW... Instead of a only kne jndustrial washing machine why not to occupy a public laundry? It will be very ecological and with great socual impact! LoL  

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nandohila
    nandohila over 9 years ago in reply to balearicdynamics

    Yeah, the size might not be an issue for most of the herbs and salad leaves.

    It would be great seeing you replicating this project. I will keep upgrading mine so by the time you start yours I might have more info to share. The idea is to keep this blog alive so I can keep posting improvements and hopefully the havesting results.

    I loved the idea to transform a loundrette into a veggies producer. People living in the city would have access to fresh local produced!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to balearicdynamics

    Sorry for the typos, I wrote this comment from my mobile image

    (just to say my English is bad but not so bad!)

     

    Enrico