Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Hotrodding the Edison
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
  • Author Author: Workshopshed
  • Date Created: 11 May 2017 8:24 AM Date Created
  • Views 3602 views
  • Likes 8 likes
  • Comments 21 comments
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Hotrodding the Edison

Workshopshed
Workshopshed
11 May 2017

The observant amongst you will have spotted that there was an item in the  [Upcycle It] Interactive Race Car Driver - 3D Printed Parts article that did not relate to any of the things I was printing. That was because I did not know if it was going to print ok or not. The part is some "exhaust pipes" to add to the Edison to turn my "engine" into a hotrod.

imageimage

Because I was concerned about the exhausts wobbling about when printing I added some 1mm horizontal supports to the model which were then cut off using a knife following the print. The print went well until layer 165 of 168 at which point it came detached from the print bed. As I was printing at 100% fill this did not actually matter and I've gone with fractionally shorter pipes by 0.9mm. If I was going to print it again I'd likely use a brim around the base to give it a bit more grip.

image

You can find all the models at https://github.com/Workshopshed/UpcyclingDesignChallenge/tree/master/3DModels

 

I don't think my modification will make any difference to the Edison's performance but I do think it looks cool. Hopefully, I'll have time to give it a coat of silver paint so it looks more like exhaust pipes.

 

Previous Posts

Upcycle It Blogs tagged with upcycled_interactiveracecardriver

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 9 years ago in reply to mcb1 +4
  • dougw
    dougw over 9 years ago +3
    Superb - those pipes are absolutely iconic. Of course if you printed a "blower" for the air intake it would be spectacular if you could squeeze in a real fan. Not trying to mess up your already impressive…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to mcb1 +2
    Mark, it seems there is not sufficient space to fit the Edison Enrico
Parents
  • mcb1
    mcb1 over 9 years ago

    Nice.

    Hope you're adding a supercharger.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to mcb1

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to mcb1

    Mark, it seems there is not sufficient space to fit the Edison image

     

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to mcb1

    Mark, it seems there is not sufficient space to fit the Edison image

     

     

    Enrico