Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Nixie Display #1 - Introduction
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
  • Author Author: gpolder
  • Date Created: 22 Mar 2017 7:01 PM Date Created
  • Views 3366 views
  • Likes 10 likes
  • Comments 9 comments
  • vintage_electronics
  • i2c
  • nixie
  • counter
  • intel_edison
  • iot
  • nixie_tube
  • upcycled_nixie
Related
Recommended

[Upcycle It] Nixie Display #1 - Introduction

gpolder
gpolder
22 Mar 2017
Blog IndexNext >>

 

Upcycled Intel Edison Nixie Display

Look what I recently found on my attic. A nice box with a six digit nixie display. Even some documentation was in the box, showing that this is a 'Impulszähler EZK' from 'electromatic'. I can't remember how it found the way to my home. It might be that I bought it long ago on a flee market, or maybe I got it from a friend.

Currently there is a lot of interest in bringing these nixie tubes to life. Lot's of nixie tube clock kits are available on the market. There appeared to be a lively trade on old stock of russian nixie tubes. Even very nostalgic designs are available (Digitale Nixieröhrenuhr). And the idea was also sent as  Top Build Suggestions  for the element14's The Ben Heck Show  (Nixie Bulbs). So I was quite happy when I found this device and my first thought was to make a clock out of it.

 

image

imageimage

 

But tell me,

modify it to a clock? I can make much more fun out of it by putting in some intelligence such as the IntelRegistered Edison.

Then this Element 14 Design challenge came up and I realised that modifying this 'Impulszähler EZK' is a perfect candidate for up cycling.

 

So the plan is:

to add the IntelRegistered Edison to this display, in order to display a six digit number using IntelRegistered Edison's wifi connection connected to the internet. An IoT nixie display so to say. The number displayed can be anything, of course it can be the current local time, from a time server, or the local time elsewhere in the world. It can be the temperature and humidity of the closest weather station, or the forecast for tomorrow. It can be the number of visitors of the project webpage, the internet speed, the position of the ISS space station from space.com, you name it.

My plan is to implement an IoT protocol in order to program the behaviour of the display from a web page.

 

How?

First I connected the device to the mains power and lucky me, it worked out of the box. The documentation showed me how to add some wires on the back in order to count  the pulses.

imageimage

 

Next I opened it and again I concluded that I'm lucky since it looks like very easy to modify. The circuit is very straightforward, the very well known SN74141 nixie tube driver is used, driven by SN7490 BCD counters, as can be seen on the photo and circuit diagram below.

 

image

image

 

Another good thing is that these IC's are not soldered to the PCB, but placed in sockets instead. So I easily can remove the 7490 IC's and replace them with a connection to the  IntelRegistered Edison.

image

In total 6 digits, times 4 BCD inputs so 24 digital GPIO outputs are needed, 4 more than provided with the IntelRegistered Edison Kit for Arduino with its 20 IO pins. Furthermore connecting all those wires between the kit and the 7490 sockets is quite a challenge.

A better option is using  IO expanders, such as the PCF8574 (PCF8574N - TEXAS INSTRUMENTS - I/O Expander, 8bit, 100 kHz, I2C, 2.5 V, 6 V, DIP | Farnell element14 ) from which we need three since these are 8 bit, or a 24 bit alternative (TCA6424ARGJR - TEXAS INSTRUMENTS - I/O Expander, 24bit, 400 kHz, I2C, SMBus, 1.65 V, 5.5 V, UQFN | Farnell element14 ), in which we need just one.

The plan is to make a small PCB which connects to the 7490 sockets. On the PCB I will put an IO expander which connects via I2C to the IntelRegistered Edison Kit for Arduino.

 

The IntelRegistered Edison Kit for Arduino will implement an IoT interface connected to the internet using the WiFi connection. From there it can be controlled. It will display any six digit number found on the internet as described previously.

If there is time left I also will use the supplied Seeed Studio Grove Start Kit for Arduino and display the measures from the sound sensor, light sensor, touch sensor or temperature sensor from this kit.

 

References:

I did a similar project long ago when I replaced a rom for a frequency synthesiser from a Mobile Radio in order to modify it for Ham Radio. Control by then was from the internet using a Tiny Internet Interface (TINI) (Agri Vision - WEB enabled KF161 ).

 

image

  • Sign in to reply

Top Comments

  • jasonwier92
    jasonwier92 over 9 years ago +1
    I like this challenge idea. Does it make sound when the pulses are received? I think it would be cool to use keep the chips in place and send pulses to change the digits, then you would only need 6 output…
  • DAB
    DAB over 9 years ago +1
    Looks like a great place to start. Having the chips on sockets enables you to do a lot of easy circuit modification. Look forward to seeing how this project evolves. DAB
  • gpolder
    gpolder over 9 years ago in reply to mads391i +1
    Hey mads391i What do you mean with how much current it draws, the complete counter, or just one nixie tube? Be aware that you also need a high voltage to get the nixie burning. I'm currently traveling…
Parents
  • mcb1
    mcb1 over 9 years ago

    Well done Gerrit.

    First off the block with your intro.

     

    When I saw the application, my first thought is how does someone know what the numbers represent ... they are numbers.

    I'm sure as you progress that will be sorted.

     

    Drawback is that each time you change a digit you will have some counting effect on it.

    I suspect there is a blanking line somewhere that you can manipulate.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago

    Well done Gerrit.

    First off the block with your intro.

     

    When I saw the application, my first thought is how does someone know what the numbers represent ... they are numbers.

    I'm sure as you progress that will be sorted.

     

    Drawback is that each time you change a digit you will have some counting effect on it.

    I suspect there is a blanking line somewhere that you can manipulate.

     

    Mark