Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycled Clock -3D Printing LED diffusers for the panels
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
  • Author Author: carmelito
  • Date Created: 20 May 2017 10:20 AM Date Created
  • Views 1564 views
  • Likes 5 likes
  • Comments 4 comments
  • upcycledclock
  • 3d pritning
  • upcycleit
  • upcycle it
  • intel edison
Related
Recommended

Upcycled Clock -3D Printing LED diffusers for the panels

carmelito
carmelito
20 May 2017

As part of the previous blog post -Upcycled Clock -3D Printing panels , the panels for the clock were printed in wood filament and stained , it was then time to design and  3D Printing LED diffuser's to go with the panels as you see in the picture below. After getting the right nozzle clog sorted out, I designed the LED diffuser's using fusion 360 and dual 3D printed the parts, with the bottom layer printed with 1.75mm transparent PLA and the top layer with regular colored Hatchbox PLA filament.

image

The M is the picture above will act as a diffuser to signify if I have an unread email in my gmail inbox image ,and Home diffuser will light up red if  the temperature/gas sensor values are too high.

 

For combining the two STL files that is bottom which is for the transparent filament and the top, I am using combine STL  feature in Slic3r to dual print. And here are some slicer setting I am using with the Flashforge creator pro

Nozzel temperature – 210 C

Bed temperature – 55 C

Extrusion speed 50 mm/s

First Layer height – 0.3mm

Layer height – 0.2 mm

Infill – 20%

 

 

{gallery} Dual 3D printing

image

Slic3r setup to dual 3D print

image

3D printing the twitter LED diffuser

image

Here are the other LED diffuser's parts

image

LED diffuser's which slides into the panel holder

 

Here is how the clock should look after I have the panels installed. Hmm by the looks of it, I think I can still add another panel between i and ii .

image

 

Now, since I am headed to Bay Area MakerFaire tomorrow, I thought, I will use the similar concept to 3D print myself a custom batch image ..

image

Makerfaire robot svg imported in CAD was taken from - http://makerfaire.com/ website.

  • Sign in to reply
Parents
  • DAB
    DAB over 9 years ago

    Nice update.

     

    I have found the diffuser screens in old LCD displays make a great light diffuser and you could probably 3D print directly onto it.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Nice update.

     

    I have found the diffuser screens in old LCD displays make a great light diffuser and you could probably 3D print directly onto it.

     

    DAB