Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Accessing hardware on the Edison?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 5 subscribers
  • Views 3123 views
  • Users 0 members are here
Related

Accessing hardware on the Edison?

Workshopshed
Workshopshed over 9 years ago

I'm wondering about accessing the GPIO of the Edison in high-level languages such as Python or Node.

 

So far I've found MRAA but wondered if there are other options?

 

https://github.com/intel-iot-devkit/mraa

  • Sign in to reply
  • Cancel

Top Replies

  • jasonwier92
    jasonwier92 over 9 years ago +3
    MRAA should be the way to go. Looks like they have Python interface. Check out this link: Getting Started With Intel Edison - Python Programming - All I cannot wait to play with Python and Node on the…
  • e14 Contributor
    e14 Contributor over 9 years ago +2
    If you can access the gpio through the standard linux filesystem method it should be possible to write out the bash commands in Python using os.popen e.g. import os p = os.popen("echo 1 > /sys/class/gpio…
  • mcb1
    mcb1 over 9 years ago in reply to konstantinoskonstas +2
    I'm learning as I go. I've always said I'm more a hardware guy that pokes and prods at software. I was hoping to get a head start on you guys/gals ...
Parents
  • jasonwier92
    jasonwier92 over 9 years ago

    MRAA should be the way to go.  Looks like they have Python interface.

     

    Check out this link:

    Getting Started With Intel Edison - Python Programming - All

     

    I cannot wait to play with Python and Node on the Edison. Plans are to make that an early write up.

     

    I was wondering if Firmata would work or how does the Arduino and Atom systems communicate?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to jasonwier92

    This article suggests you'd need to be root to run things that access MRAA

     

    https://communities.intel.com/thread/60492

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    There's an article here that is worth reading (the second part) if you want to detect pin changes.

    https://www.linux.com/learn/intro-to-Linux/2017/3/intel-edison-linux-maker-machine-matchbox

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to mcb1

    So a little more playing

     

    It seems that under /usr/bin there is mraa-gpio which is happy to run from the command line.

    The options are.

    root@edison:/usr/bin# mraa-gpio
    Invalid command, options are:
    list              List pins
    set pin level     Set pin to level (0/1)
    setraw pin level  Set pin to level (0/1) via mmap (if available)
    get pin           Get pin level
    getraw pin        Get pin level via mmap (if available)
    monitor pin       Monitor pin level changes
    version           Get mraa version and board name
    root@edison:/usr/bin#

     

    mraa-gpio version gives you

    Version v1.0.0 on Intel Edison

     

    while list

    root@edison:/usr/bin# mraa-gpio list

    00       J17-1: GPIO PWM
    01       J17-2:
    02       J17-3:
    03       J17-4:
    04       J17-5: GPIO
    05       J17-6:
    06       J17-7: GPIO I2C
    07       J17-8: GPIO I2C
    08       J17-9: GPIO I2C
    09      J17-10: GPIO SPI
    10      J17-11: GPIO SPI
    11      J17-12: GPIO SPI
    12      J17-13:
    13      J17-14: GPIO
    14       J18-1: GPIO PWM
    15       J18-2: GPIO
    16       J18-3:
    17       J18-4:
    18       J18-5:
    19       J18-6: GPIO I2C
    20       J18-7: GPIO PWM
    21       J18-8: GPIO PWM
    22       J18-9:
    23      J18-10: GPIO SPI
    24      J18-11: GPIO SPI
    25      J18-12: GPIO
    26      J18-13: GPIO UART
    27      J18-14:
    28       J19-1:
    29       J19-2:
    30       J19-3:
    31       J19-4: GPIO
    32       J19-5: GPIO
    33       J19-6: GPIO
    34       J19-7:
    35       J19-8: GPIO UART
    36       J19-9: GPIO
    37      J19-10: GPIO
    38      J19-11: GPIO
    39      J19-12: GPIO
    40      J19-13: GPIO
    41      J19-14: GPIO
    42       J20-1:
    43       J20-2:
    44       J20-3:
    45       J20-4: GPIO
    46       J20-5: GPIO
    47       J20-6: GPIO
    48       J20-7: GPIO
    49       J20-8: GPIO
    50       J20-9: GPIO
    51      J20-10: GPIO
    52      J20-11: GPIO
    53      J20-12: GPIO
    54      J20-13: GPIO
    55      J20-14: GPIO

     

     

    I tried setting GPIO 48 (pin 7 on the Arduino shield) and it wouldn't work.

     

    If I used the echo command it worked, and using mraa-gpio get 48, it gave the current state (0 or 1) in response to the echo commands.

     

    So I'm a little puzzled ... more digging is required.

     

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 9 years ago in reply to mcb1

    So a little more playing

     

    It seems that under /usr/bin there is mraa-gpio which is happy to run from the command line.

    The options are.

    root@edison:/usr/bin# mraa-gpio
    Invalid command, options are:
    list              List pins
    set pin level     Set pin to level (0/1)
    setraw pin level  Set pin to level (0/1) via mmap (if available)
    get pin           Get pin level
    getraw pin        Get pin level via mmap (if available)
    monitor pin       Monitor pin level changes
    version           Get mraa version and board name
    root@edison:/usr/bin#

     

    mraa-gpio version gives you

    Version v1.0.0 on Intel Edison

     

    while list

    root@edison:/usr/bin# mraa-gpio list

    00       J17-1: GPIO PWM
    01       J17-2:
    02       J17-3:
    03       J17-4:
    04       J17-5: GPIO
    05       J17-6:
    06       J17-7: GPIO I2C
    07       J17-8: GPIO I2C
    08       J17-9: GPIO I2C
    09      J17-10: GPIO SPI
    10      J17-11: GPIO SPI
    11      J17-12: GPIO SPI
    12      J17-13:
    13      J17-14: GPIO
    14       J18-1: GPIO PWM
    15       J18-2: GPIO
    16       J18-3:
    17       J18-4:
    18       J18-5:
    19       J18-6: GPIO I2C
    20       J18-7: GPIO PWM
    21       J18-8: GPIO PWM
    22       J18-9:
    23      J18-10: GPIO SPI
    24      J18-11: GPIO SPI
    25      J18-12: GPIO
    26      J18-13: GPIO UART
    27      J18-14:
    28       J19-1:
    29       J19-2:
    30       J19-3:
    31       J19-4: GPIO
    32       J19-5: GPIO
    33       J19-6: GPIO
    34       J19-7:
    35       J19-8: GPIO UART
    36       J19-9: GPIO
    37      J19-10: GPIO
    38      J19-11: GPIO
    39      J19-12: GPIO
    40      J19-13: GPIO
    41      J19-14: GPIO
    42       J20-1:
    43       J20-2:
    44       J20-3:
    45       J20-4: GPIO
    46       J20-5: GPIO
    47       J20-6: GPIO
    48       J20-7: GPIO
    49       J20-8: GPIO
    50       J20-9: GPIO
    51      J20-10: GPIO
    52      J20-11: GPIO
    53      J20-12: GPIO
    54      J20-13: GPIO
    55      J20-14: GPIO

     

     

    I tried setting GPIO 48 (pin 7 on the Arduino shield) and it wouldn't work.

     

    If I used the echo command it worked, and using mraa-gpio get 48, it gave the current state (0 or 1) in response to the echo commands.

     

    So I'm a little puzzled ... more digging is required.

     

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to mcb1

    A little digging and this table shows that the mraa number and the GPIO number (and then the Arduino) are not the same.

    mraa: Intel Edison

     

    It seems mraa 33 is GPIO 48 and it works BUT.

    You can use either the echo or the mraa-gpio to set the pin or change it,

    BUT if you read the pin with get or getraw, you get a write error.

     

    root@edison:/sys/class/gpio/gpio48# /usr/bin/mraa-gpio getraw 33
    Pin 33 = 0
    root@edison:/sys/class/gpio/gpio48# echo 1 > value
    -sh: echo: write error: Operation not permitted
    root@edison:/sys/class/gpio/gpio48# /usr/bin/mraa-gpio set 33 1
    root@edison:/sys/class/gpio/gpio48# echo 0 > value
    root@edison:/sys/class/gpio/gpio48# /usr/bin/mraa-gpio getraw 33
    Pin 33 = 0
    root@edison:/sys/class/gpio/gpio48# echo 0 > value
    -sh: echo: write error: Operation not permitted
    root@edison:/sys/class/gpio/gpio48#

     

    Seems strange that a read (get) will lock out changing it but you can set it with one method and change it with the other ???

     

     

    mark