Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Accessing hardware on the Edison?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 5 subscribers
  • Views 3132 views
  • Users 0 members are here
Related

Accessing hardware on the Edison?

Workshopshed
Workshopshed over 9 years ago

I'm wondering about accessing the GPIO of the Edison in high-level languages such as Python or Node.

 

So far I've found MRAA but wondered if there are other options?

 

https://github.com/intel-iot-devkit/mraa

  • Sign in to reply
  • Cancel

Top Replies

  • jasonwier92
    jasonwier92 over 9 years ago +3
    MRAA should be the way to go. Looks like they have Python interface. Check out this link: Getting Started With Intel Edison - Python Programming - All I cannot wait to play with Python and Node on the…
  • e14 Contributor
    e14 Contributor over 9 years ago +2
    If you can access the gpio through the standard linux filesystem method it should be possible to write out the bash commands in Python using os.popen e.g. import os p = os.popen("echo 1 > /sys/class/gpio…
  • mcb1
    mcb1 over 9 years ago in reply to konstantinoskonstas +2
    I'm learning as I go. I've always said I'm more a hardware guy that pokes and prods at software. I was hoping to get a head start on you guys/gals ...
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    I just spotted UPM, runs on top of MRAA and provides a further abstraction so you can programme with LEDs and Light Sensors rather than working at the Pin level

     

    https://github.com/intel-iot-devkit/upm

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Following our conversation yesterday ...

    I did some searching and it turns out that the version of mraa-gpio is not the latest.

     

    From here https://github.com/intel-iot-devkit/mraa

     

    https://github.com/intel-iot-devkit/mraa#installing-on-intel-32bit-yocto-based-opkg-imageInstalling on Intel 32bit Yocto based opkg image

    See the section below on compiling or use our repository to install on a glibc based yocto poky image that supports opkg.

    Adding this repository is as simple as and you'll have the latest stable tagged build of mraa installed!

    echo "src mraa-upm http://iotdk.intel.com/repos/3.5/intelgalactic-dev/opkg/i586" > /etc/opkg/mraa-upm.conf

    opkg update

    opkg install mraa

     

    it took a few minutes

    root@Edison_2:~# echo "src mraa-upm http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586" > /etc/opkg/mraa-upm.conf
    root@Edison_2:~# opkg update
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586//Packages.
    Updated list of available packages in /var/lib/opkg/iotkit.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/all/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-all.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/core2-32/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-core2-32.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/edison/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-edison.
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586/Packages.
    Updated list of available packages in /var/lib/opkg/mraa-upm.
    root@Edison_2:~# opkg install mraa
    Upgrading mraa from 1.0.0-r0 to 1.5.1 on root.
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586/mraa_1.5.1_i586.ipk.
    Removing package mraa-dev from root...
    Removing package mraa-doc from root...
    Removing obsolete file /usr/lib/libmraa.so.1.0.0.
    Configuring mraa.
    root@Edison_2:~# /usr/bin/mraa-gpio version
    Version v1.5.1 on Intel Edison
    root@Edison_2:~#

     

     

    and now I have version 1.5.1

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Following our conversation yesterday ...

    I did some searching and it turns out that the version of mraa-gpio is not the latest.

     

    From here https://github.com/intel-iot-devkit/mraa

     

    https://github.com/intel-iot-devkit/mraa#installing-on-intel-32bit-yocto-based-opkg-imageInstalling on Intel 32bit Yocto based opkg image

    See the section below on compiling or use our repository to install on a glibc based yocto poky image that supports opkg.

    Adding this repository is as simple as and you'll have the latest stable tagged build of mraa installed!

    echo "src mraa-upm http://iotdk.intel.com/repos/3.5/intelgalactic-dev/opkg/i586" > /etc/opkg/mraa-upm.conf

    opkg update

    opkg install mraa

     

    it took a few minutes

    root@Edison_2:~# echo "src mraa-upm http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586" > /etc/opkg/mraa-upm.conf
    root@Edison_2:~# opkg update
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586//Packages.
    Updated list of available packages in /var/lib/opkg/iotkit.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/all/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-all.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/core2-32/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-core2-32.
    Downloading http://iotdk.intel.com/repos/3.5/iotdk/edison/edison/Packages.
    Updated list of available packages in /var/lib/opkg/iotdk-edison.
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586/Packages.
    Updated list of available packages in /var/lib/opkg/mraa-upm.
    root@Edison_2:~# opkg install mraa
    Upgrading mraa from 1.0.0-r0 to 1.5.1 on root.
    Downloading http://iotdk.intel.com/repos/3.5/intelgalactic/opkg/i586/mraa_1.5.1_i586.ipk.
    Removing package mraa-dev from root...
    Removing package mraa-doc from root...
    Removing obsolete file /usr/lib/libmraa.so.1.0.0.
    Configuring mraa.
    root@Edison_2:~# /usr/bin/mraa-gpio version
    Version v1.5.1 on Intel Edison
    root@Edison_2:~#

     

     

    and now I have version 1.5.1

     

     

    Mark