Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Node-Red Reading output values
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 3 subscribers
  • Views 897 views
  • Users 0 members are here
Related

Node-Red Reading output values

jasonwier92
jasonwier92 over 9 years ago

Okay, as I am testing, I am noticing that you cannot read the status of an output node. take the following examples:  this controls the relay just fine, sometimes it is a little touchy, but for the most part it works.  But then I monitor the same input triggered on rising and falling edges and I get no output.  I think it is because it is already setup as an output. With Node or Python, you can see what state the output pin is in and that is what I would like to do. I could do it with an output from the WS or MQTT message or the function and even store the state and on a new connection dump out all the values. Problem is when Node-red restarts the states are un-known. The one idea I had was to store this the state in a persistent data storage, like a database.  Only issue I see with that is it could get stale. Maybe I changed it via a command line.  I think it is best to ask the pin what state it is in.

 

To the ones running Node-Red for their project, what do you all think?

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +1
    Not sure if this helps. https://flows.nodered.org/node/node-red-contrib-influxdb Seems writing to a database might be the only way to keep it after a restart. Ran across this which outlines lots of uses…
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Perhaps an inject at startup node could trigger a function that reads the outputs via an external process?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 9 years ago

    Perhaps an inject at startup node could trigger a function that reads the outputs via an external process?