Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Connecting to the Edison over USB
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 5 subscribers
  • Views 2404 views
  • Users 0 members are here
  • network
  • usb
Related

Connecting to the Edison over USB

Workshopshed
Workshopshed over 9 years ago

I've been using Wifi to connect to the Edison but I've also spotted that the Yokto distribution provides the facility to connect using Network over USB. This can be useful as I've used it on other boards such as the BeagleBone Blue.

 

https://software.intel.com/en-us/connecting-to-intel-edison-board-using-ethernet-over-usb

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1 +2
    If you only connect the Edison via USB and don't turn on its Wifi then: The PC to be able to connect to the Edison over one network (a virtual one over USB) The PC to be able to connect to the Internet…
  • jasonwier92
    jasonwier92 over 9 years ago +1
    This is what you use to setup your Edison originally to flash.
  • Workshopshed
    Workshopshed over 9 years ago in reply to jasonwier92 +1
    I thought that was done using magic
Parents
  • jofas
    jofas over 9 years ago

    I was using the usb network connection to ssh into my Edison - got pretty tiring though because I kept having to reboot the Edison every time I made a code change. It could be useful for some applications but keep in mind that you would need to set up the computer as a router. Before I set up wifi on my Edison, I tried to ping from the Edison to external networks through the USB network connection but the Edison couldn't reach them. It also couldn't use DNS even though the nameservers were set up properly. Of course it's possible I was just doing something wrong image.

     

    But this is a good example of what I like about this device - it has lots of different ways of doing things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to jofas

    >I tried to ping from the Edison to external networks through the USB network connection

    I'd not expect that to work unless you'd done some kind of clever routing or sharing on your PC

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    I'd not expect that to work unless you'd done some kind of clever routing or sharing on your PC

    If you have a "USB Network connection" and it's connected to your network, then there should be no reason it won't get out.

    The only limits would be if your router rules stop you.

     

    DNS is tied to being able to reach the DNS server.

    In many setups this is external to your place and usually at the ISP.

    Since the Edison couldn't get out (couldn't ping external) then it's not likely to work.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1

    If you only connect the Edison via USB and don't turn on its Wifi then:

     

    • The PC to be able to connect to the Edison over one network (a virtual one over USB)
    • The PC to be able to connect to the Internet over its other network connector (wifi or hard wired)
    • The Edison would not necessarily be able to connect to the Internet

     

    That is because these are 2 separate networks so your PC would need to be configured to route the network traffic as it is acting as an intermediary between the Edison and Internet.

    internet connection sharing ics

     

    How to enable IP Forwarding in Linux - MDLog:/sysadmin

    Windows 7 Internet connection Sharing (ICS) Host Computer Setup

    https://support.apple.com/kb/PH18704?locale=en_US

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1

    If you only connect the Edison via USB and don't turn on its Wifi then:

     

    • The PC to be able to connect to the Edison over one network (a virtual one over USB)
    • The PC to be able to connect to the Internet over its other network connector (wifi or hard wired)
    • The Edison would not necessarily be able to connect to the Internet

     

    That is because these are 2 separate networks so your PC would need to be configured to route the network traffic as it is acting as an intermediary between the Edison and Internet.

    internet connection sharing ics

     

    How to enable IP Forwarding in Linux - MDLog:/sysadmin

    Windows 7 Internet connection Sharing (ICS) Host Computer Setup

    https://support.apple.com/kb/PH18704?locale=en_US

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Ah yes a shared Network over USB.

     

    I was assumming that it was a USB dongle ...