Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Documents Upcycle it Design Challenge: The Kit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: jwatson
  • Date Created: 9 Jan 2017 3:36 PM Date Created
  • Last Updated Last Updated: 1 Aug 2017 4:28 PM
  • Views 6959 views
  • Likes 13 likes
  • Comments 35 comments
Related
Recommended

Upcycle it Design Challenge: The Kit

image
Upcycle it Design Challenge
About this ChallengeThe KitThe PrizesIntro VideoWhat is Upcycling Video
Unboxing VideoThe JudgesExample ApplicationTerms and ConditionsThe Challengers

 

The 15 official Challengers for the "Upcycle it" Design Challenge will receive for FREE the following kit from our sponsor, IntelRegistered. (The kit is worth about $260.)

 

The lucky 15 will then embark on building an inspiring and inventive project that will upcycle an obsolete item, computer, or appliance that they would otherwise have discarded, and make it into something useful, with greater functionality and value. (NOTE: Even if you aren't an official Challenger, you can still participate in the challenge as long as you comply with the main terms and conditions and integrate the IntelRegistered Edison in your design.)

 

For the official Challengers, if you complete your project by the deadline and write at least 10 blog posts, you’ll also be in the running for some awesome prizes, including a Keithley DMM7510 Digital MultimeterKeithley DMM7510 Digital Multimeter worth almost $4,000.

 

The Kit Buy Kit*Buy Kit*

IntelRegistered Edison for Arduino

The IntelRegistered Edison Board for Arduino is a development platform that allows for rapid prototyping of “Internet of Things” (IoT) and wearable computing products. It supports Arduino Sketches, Linux, Wi-Fi, and Bluetooth. The board is compatible with Arduino Uno's I/O except it that it has 4 PWM instead of 6 PWM. Its 20 digital input/output pins include 4 pins as PWM outputs. It also has 6 analog inputs, one UART (Rx/Tx), one I2C, an ICSP 6-pin header (SPI), a Micro USB device connector, a dedicated standard size USB host Type-A connector, a Micro USB device, an SD card connector and a DC power jack (7 to 15 VDC input).

image
Buy NowBuy Now

IntelRegistered Edison Breakout Board

Slightly larger than the IntelRegistered Edison module itself, the IntelRegistered Edison Breakout Board (also called the "mini" breakout board) is designed to expose the native 1.8 V I/O of the IntelRegistered Edison module. The board consists of a power supply, battery charger, USB OTG power switch, UART to USB bridge, USB OTG port, and an I/O header. It has a 0.1 inch grid I/O array of through-hole solder points. The DC power supply jack accepts a 7 to 15 VDC input.

image
Buy NowBuy Now

Arduino Protoshield R3

The Arduino Protoshield R3 makes it easy to design custom circuits for the Upcycle it Design Challenge. You can solder parts to the prototyping area, or use it with a small solderless breadboard to quickly test circuit ideas. Features include: Arduino 1.0 pin outs, a large 0.1inch prototyping area, Reset button, 14-pin SMD footprint (50mils pitch), 20-pin through hole footprint (100mils pitch), SPI header, and easy-to-solder ground/5V rails.

image
Buy NowBuy Now

Seeed Studio Grove Start Kit for Arduino

Seeed Studio's Grove Starter Kit is a handy collection of components for rapid prototyping, based on the Arduino-compatible, Grove plugable-component system. Besides the base shield, the kit includes a rotary angle sensor, RGB Backlight LCD, sound sensor, button, light sensor, touch sensor, temperature sensor, LEDs, relay, buzzer, servo, and more.

image
Buy NowBuy NowBuy Now

*Available in North America, UK & Ireland

Triad Magnetics WSX120-2000WSX120-2000 AC/DC Power Supply

To power the IntelRegistered Edison from an external source, the Upcycle it kit includes theTriad Magnetics WSX120-2000WSX120-2000 AC/DC Power Supply, which accepts a 90 to 264VAC input and outputs 12 VDC at 2A. It has a changeable head so it can be used anywhere in the world.

image
Buy NowBuy Now

Molex Cable Assembly

To connect the IntelRegistered Edison for Arduino or Breakout Boards to your computer, the kit includes a USB-A to Micro USB-B 2-meter long cable assembly

image
Buy NowBuy Now

 

Join in this Challenge and challenge the challengers at any time to be in with a chance to win the prizes. Just blog in the Upcycle it space (tagging your blogs with 'upcycle it').

  • design challenge
  • design_challenge
  • upcycleit
  • upcycle
  • upcycle it design challenge: the kit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • fvan
    fvan over 9 years ago +5
    Found this article on CharlesGantt 's blog: http://www.themakersworkbench.com/articles/end-life-notice-issued-intel-edison-galileo-and-joule-development-boards End Of Life Notice Issued For Intel Edison…
  • mcb1
    mcb1 over 9 years ago in reply to jasonwier92 +4
    Does this make you judge and jury? Not at all ... I'm sure third party vendors are very good at their business. However the third party boards made just for the EDISON will not fit anything else, and because…
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago +4
    With due respect to the people that we have been communicating over the last months. I find it hard to express my feelings. The least I can say is that after the so many efforts to overcome the difficulties…
Parents
  • jkutzsch
    jkutzsch over 9 years ago

    2 questions.

     

    First, how do we get a bit more info on the Seed Studio Grove Start Kit for Arduino?  The "and more" is intriguing but when I click the picture I get another mini-picture.  And it will let me order it, but under data sheets it says:  Sorry, no product results found.

     

    Second, is it best to write up a Draft application and update it over time to submit near the due date, or can you write up an application and then update it later if so inclined and still within the time constraints out lined?  I have been offline writing a draft because some nights my internet is flaky and have had it the entire application fail due to drop in service.  :-(

     

    Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to jkutzsch

    I have to say I don't enjoy navigating the Grove website, for some reason a lot of their stuff never actually shows up on my screen, could be my system though.  But I did find this http://www.seeedstudio.com/document/Grove%20Starter%20Kit.pdf for info in regards to that Starter Kit.  Looks very interesting!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jkutzsch
    jkutzsch over 9 years ago in reply to jkutzsch

    I have to say I don't enjoy navigating the Grove website, for some reason a lot of their stuff never actually shows up on my screen, could be my system though.  But I did find this http://www.seeedstudio.com/document/Grove%20Starter%20Kit.pdf for info in regards to that Starter Kit.  Looks very interesting!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 9 years ago in reply to jkutzsch

    Note that the contents of the starter kits change from time to time.

     

    There are different versions of the shield as well.

    Base Shield V2 - Seeed Wiki

     

    There is the Grove System Wiki at:

    Grove System - Seeed Wiki

    if you've not already found it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to beacon_dave

    Looking at the wiki, seems a more updated source of information for the Starter Kit can be found there as well!  http://wiki.seeed.cc/Grove_Starter_Kit_v3/