• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Project: ferris farm post 9
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
  • Author Author: shanesissons
  • Date Created: 21 Aug 2015 1:52 AM Date Created
  • Views 989 views
  • Likes 1 like
  • Comments 6 comments
  • mechanical_farm
Related
Recommended

Project: ferris farm post 9

shanesissons
shanesissons
21 Aug 2015








{gallery} post 9

image

image

image

image

image

image

image

image

image

image

image

image

image

image

Parts have started to arrive !!

 

I have now started a dry run building the design so far i have

installed the PSU

installed the fans

1st coat of varnish on the wood

nailed and glued the sides and back

installed the legs

test fit the mounts for the dev boards

soldering and crimping wires and connectors

sizing up where the parts that have not arrived will go

 

PSU

 

the power for this unit will come from a pc power supply that has been adapted

i will be using the 3.3,5 and 12v lines from the PSU

 

Fans

 

I went with 2 5v fans that were repurposed from an old laptop cooling stand

in front of the fans are 3 layers of mesh this is to stop insects from entering the unit and also to restrict air flow to a lower amount

 

Varnish

 

After a long discussion with myself i decided to go with a varnish on the unit instead of a paint to keep the look of the OSB

the top of the unit also has a stain on as well this was a test to see what looked the best and decided just to keep the top stained

 

Board mount

 

i have used 3 pcb spacers to mount the board on a scrap piece of wood to test the idea and it worked out really well and this is how i will be mounting the board inside the unit

 

Cables

 

I have started to solder the connectors onto the cables ready for the boards to arrive that way i can solder them straight onto the boards and save some time as well

 

Lighting

 

for the lighting i am testing out using red green and blue LEDs i will be usign a total of 60 LEDs 20 of each colour i will have these mounted but connect them up so many at a time to get the best amount of light

 

still to be updated when parts arrive

rotation

moisture sensor and my crazy way of connecting them to the board through 2 axis of rotation

watering system

lighting

silver lining (mylar)

  • Sign in to reply

Top Comments

  • shanesissons
    shanesissons over 11 years ago in reply to balearicdynamics +1
    The legs of the unit are from a bed frame they are bolted through the wood and are very sturdy basically they are now one with the unit They will withstand alot of weight approx 10 stone per leg so I'm…
Parents
  • DAB
    DAB over 11 years ago

    It looks like you are off to a good start.

     

    I will be awaiting to see this build progress.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    It looks like you are off to a good start.

     

    I will be awaiting to see this build progress.

     

    DAB