Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Forum Mechanical Design Assistance???
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 9 subscribers
  • Views 7528 views
  • Users 0 members are here
  • vertical_farming
Related

Mechanical Design Assistance???

RWReynolds
RWReynolds over 11 years ago

Hey everyone,

 

I'm not a mechanical engineer by any stretch on anyone's imagination. I have one mechanical design issue that I'm not sure how to approach. I kind of know the theory, but I have no idea how to approach it practically.

 

Here's the problem...

 

I have a load, my cultivator unit, that will be about 3' - 4' tall, maybe 12" to 18" in diameter and weigh between 20 and 40 lbs. The whole thing will be mounted on a lazy susan style turntable. The plan is to have a gear or pulley at the bottom that will be used with a hight torque stepper motor, and chain or belt, to rotate the cultivator. I'm using a stepper motor because they are pretty efficient and can be controlled very easily at very slow speeds. I want the rotation speed to be maybe 3 to 4 revolutions per day. A stepper would work well for this I think.

 

I have no idea how to properly size the motor. I see them speced at anywhere from 10s of oz-in to 1000s of oz-inches of torque. I get the concept of torque being rotational force. And that required torque has to do with acceleration time up to the desired RPM. But I have no idea how to relate this to my requirements.

 

I'm a 'puter software with some dangerous electronics knowledge guy! HELP!!! And feel free to tell me this just a stupid idea and I should be using a washing machine motor or something if that's the case.

 

For reference, here's a drawing of the rig. Note the drive at the bottom right. Please excuse the misspelled labeling. I haven't gotten around to correcting it yet. lol...

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to RWReynolds +2
    RWReynolds It looks like your design is coming together. Two comments. The stepper I linked to, Terry made this comment. This means your pulse number might be lower. (half) With the geared output you already…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jw0752 +2
    Well, I received my 390mm dia lazy-susan a while back (image attached) but it'll sit in a corner some more yet. Reading lots that I hadn't been aware of e.g "inertia-matching" it seems direct-coupling…
  • clem57
    clem57 over 11 years ago +1
    Same here RWReynolds , but try this calculator for gear reduction to decrease speed Mechanical Gear Reduction Calculator C Edit: How about placing LED's around and turning on/off the set you want? Just…
Parents
  • saturnv
    saturnv over 11 years ago

    Rick, the relationship for rotations, or revolutions is gear ratio. For example, if you want 4 rotations of your cultivator per day that means you want ONE rotation every SIX hours, 1/2 rotation every 3 hours or 1/4 rotation every 1.5 hours. Normally you would want a gear ratio between your cultivator base size and your motors pulley size. However, since you're going to use stepper motors,  all you should need to do software-wise is make use of timing parameters to step the turntable once every 6 hours. Using wait, if/the, for, or pause commands or some other variable to reference the passing of time should work for you. For example is you want it to turn 1/4 turn, have it 'sleep for 5400 seconds (3600 secs/hr * 1.5 hrs=5400 seconds). Do that 16 times via an "if' or "while' type statements and your turntable will rotate 4 times in a 24 hour period. It's all about the math!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to saturnv

    Thanks for the info Michael...

     

    I think I have it worked out now. The control application will just be a simple state machine based on "the big loop". Reading sensors, performing control functions and logging them, via the radio, back to the central control/monitor system. I think control functions and reading the sensors should be very lightweight. There's no sensor that needs to be read more than once a second, and that's probably overkill. As the EZR32WG has some very low power modes available I plan to have it sleep most of the time and wake up only periodically to run the loop. The central control/monitor will have the ability to wake the crowing area system up at any time and instruct it to read sensors and/or perform control functions.

     

    I'll have to workout all the timing and pulse count once I have the MCU in hand and the rotator is completed. So far my calculations go like this... My stepper motor is geared and requires 4096 pulses per revolution. There is about a 10:1 ration between the timing gear, at the turntable, and timing pulley on the stepper motor. That gives me about 41,000 pulses per revolution at the turntable. If I want 4 revolutions per day so that's 164,000 pulses per day. That works out to about 2 pulses per second. So I could just pulse it a couple of times on each wake up cycle. Since the motor is geared it doesn't require power to remain stationary. We'll see.

     

    Right now I'm waiting on the final parts for the turntable and on the E14 kit. It's all just theory right now. lol...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RWReynolds
    RWReynolds over 11 years ago in reply to saturnv

    Thanks for the info Michael...

     

    I think I have it worked out now. The control application will just be a simple state machine based on "the big loop". Reading sensors, performing control functions and logging them, via the radio, back to the central control/monitor system. I think control functions and reading the sensors should be very lightweight. There's no sensor that needs to be read more than once a second, and that's probably overkill. As the EZR32WG has some very low power modes available I plan to have it sleep most of the time and wake up only periodically to run the loop. The central control/monitor will have the ability to wake the crowing area system up at any time and instruct it to read sensors and/or perform control functions.

     

    I'll have to workout all the timing and pulse count once I have the MCU in hand and the rotator is completed. So far my calculations go like this... My stepper motor is geared and requires 4096 pulses per revolution. There is about a 10:1 ration between the timing gear, at the turntable, and timing pulley on the stepper motor. That gives me about 41,000 pulses per revolution at the turntable. If I want 4 revolutions per day so that's 164,000 pulses per day. That works out to about 2 pulses per second. So I could just pulse it a couple of times on each wake up cycle. Since the motor is geared it doesn't require power to remain stationary. We'll see.

     

    Right now I'm waiting on the final parts for the turntable and on the E14 kit. It's all just theory right now. lol...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to RWReynolds

    RWReynolds

    It looks like your design is coming together.

     

    Two comments.

    The stepper I linked to, Terry made this comment.

    image

    This means your pulse number might be lower. (half)

    With the geared output you already have increased the step angle by 64, so you don't require 8 steps ...

    The output angle per pulse is close to 0.178 deg.

     

    balearicdynamics Enrico's idea for the tensioner is a good one.

    You could mount your stepper and drive wheel on plate that pivots at one end, and has a spring pulling it onto the disc.

    If the length was long, it would allow for a few millimeters vertical movement at the drive cog.

    If you ensure the belt is wider than the base, you could add a disc onto the top and bottom of the drive cog to ensures it stays in contact with the belt.

     

    This would allow for any wobble your large disc has.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to mcb1

    Thanks for the info mcb1.

     

    I will take into account the info on the steps per revolution. On one of the sites where I researched the motor it did say 4096. I will have it connected soon to a Raspberry Pi for testing. Then I can work out the exact pulse count and timing required.

     

    I was planning to mount the motor in such a fashion as to allow for some spring tensioning against the timing gear. I just have to work out the mount now.

     

    Cheers,

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to RWReynolds

    Fist post here. I hope it's ok to continue on an old thread - there are some similarities to my current project.

     

    It's a long time since I attempted any angular motion calculations - so please forgive any obvious mistakes...I have ignored friction below on the assumption it will be negligible compared to torque/power required for acceleration (not sure if that is wise though).

     

    I'd like to use a stepper (or steppers if needed) to rotate a plywood disk (with a person standing on top) of 1200 mm dia 30° in 1.25 secs. The timing belt drive disk will be 1160 mm dia as the centre of a 1200/1160/1200 mm sandwich with a lazy susan on the bottom. I plan to use something like the AccelStepper library (not sure if providing a link to that is ok?) to do:

    1. from rest provide constant acceleration for 0.5 secs
    2. constant angular velocity for 0.25 secs
    3. const decelerate for 0.5 secs to rest

    I calculated the approximate moment of inertia (plywood + person as 100 kg point load on perimeter of disc) as 39.16kgm2

     

    Torque/Power Calculation:

    Say, use Accelstepper Library to apply the above:

    (i) constant acceleration, α, (from 0 rad/s) for 10° to maximum ω rad/s. Say time taken = 0.5 secs

    (ii) zero acceleration for 10° to 20°. Say time taken = 0.25 secs

    (iii) constant deceleration , α,  from 20° to 30° for 10° (from  ω rad/s to 0 rad/s). Say time taken = 0.5 secs

     

    i.e. total time taken is 1.25 secs for 30° start-to-stop

     

    Considering only item (i) for now:

    Angular Displacement, θ = 10° (or  0.1746 rads)

     

    For rotational motion with constant Angular Acceleration:

    θ = (1/2)(ω0 + ω)t

    since ω0 = 0 rad/s

    0.1746 = 0.5 (0 + ω) 0.5 -> ω = 0.1746 / 0.25 -> ω = 0.6984 rad/s

     

    α = (ω - ω0)/t -> α = (0.6984 - 0)/0.5 -> α = 1.3968 rad.sec-2

     

    Torque required to produce this stated radial acceleration:

    τ = Iα -> τ = 39.16 x 1.3968 Nm -> τ =  54.7 Nm (Max)

     

    Force required to produce this Torque:

    τ = Fd so F = τ / d

    "d" for the disk with the glued on timing belt is = 1160mm/2 = 0.58m

    therefore

    F = τ / d -> F = 54.7 / 0.58 -> F = 94.31 N

     

    Work done by torque τ is W = τ x θ

     

    Power, P = d/dt(W) = d/dt( τ x θ ) = τ x dθ/dt

     

    since ω = dθ/dt

     

    Power = τ x ω

     

    Power = 54.7 x 0.6984 -> Power = 38.2 Watts (Max)

     

    Question(s):

    I have a rough idea how a stepper works but i'm not really sure how to specify a particular stepper/gearing ratio to "make this happen" - any ideas along that route would be most appreciated (based on quoted power alone I have a feeling I may need 2 x Nema 42!!).

     

    Other:

    of related interest - using an 80MHz processor (compared to a 16MHz Arduino Uno) increases the Accelstepper acceleration 5 fold e.g. https://www.youtube.com/watch?v=Hsl3dbRPLTw

    ...that e.g. used a bipolar nema 34 at 1.8°/step (200steps/rev)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor

    Hi Andrew,

    Your person standing on the turntable makes any specific calculation of the torques involved very difficult. The structure of the human body will absorb the movement and only follow a 1.5 second rotation in an elastic manner. To smooth out the rotation I would consider 15 degrees of acceleration and 15 degrees of deceleration. This will slightly improve the amount of torque needed and should improve the overall feel of the rotation to the subject. Foot position of the subject on the disk should not affect overall torque but an imbalance of weight distribution may make friction in the bearings a factor that needs to be considered. Foot position may also affect the amount of elasticity in the bones and muscles of the body and hence change the dynamics of the rotation. By over engineering the problem you should be able to make it work.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jw0752

    Much appreciated John - food for thought. I guess the proof of the pudding is...that it wobbles image. Much experimenting & various poses required - neither is the 1.5 secs set in stone.

     

    I had imagined the 100Kg load / position as the over-engineered extreme (I should have mentioned that though).

     

    "15 degrees of acceleration and 15 degrees of deceleration"

     

    I'd prefer something approaching a sinusoid (i.e. zero, slight +ve, large +ve, slight +ve, zero, slight -ve , large -ve, slight -ve, zero) for the acceleration profile but I haven't looked in detail whether that can be approximated by a series of steps through the AccelStepper library yet.

     

    To be honest I have practically zero mechanical design experience and i'm probably hoping for further comment re how to identify a suitable stepper and how to size the pulley and belt pitch gearing relationship...

     

    Thanks,

    Andrew.

     

    Edit:

     

    Having reviewed the "trapezoidal velocity profile" produced by the the positive accel pulse / zero accel / negative accel pulse i'm no longer sure the sinusoid accel profile I had referred to would be any better than this:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor

    As jw0752 said the postion could affect the friction.

     

    As a cheap source you may wish to consider using automotive components.

    Either the rear or front hub turned on its side, would easily cater for uneven loading while retaining the same friction.

     

    Depending on what option you choose the drive axle could be retained to allow different options to drive it.

     

     

    Looks like an exciting project.

    Good luck

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor

    Hi Andrew,

    The reason I suggested a steadily accelerating and decelerating program is that for any time frame it will have the lowest dv/dt. Any time spent at constant velocity is a waste and only creates the need for higher torques and higher accelerations at the beginning and ends of the cycle.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to mcb1

    I'll keep that in mind Mark - at the minute I have one eye on keeping the solution mobile (and weight down) so will try the lazy susan and some roller bearings around the perimeter first.

     

    Understood John - while that will keep torque down i'm equally concerned about the effect (on the  person) of the sudden change from +ve accel to -ve accel (not mitigated by the period of zero accel). Of course, the fact the shorter periods of accel/decel must be harsher may offset the benefit I refer to...perhaps a short period of zero accel will help.

     

    We'll see!

      

    Thanks,

    Andrew.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jw0752

    Well, I received my 390mm dia lazy-susan a while back (image attached) but it'll sit in a corner some more yet.

     

    Reading lots that I hadn't been aware of e.g "inertia-matching" it seems direct-coupling of gearhead/stepper to the turntable may be preferable (neither had I been fully aware of the reduction in reflected load inertia by the square of the gearbox ratio).

     

    While a direct coupling scenario does work around some complexity (belt-drive redundancy / no requirement for circular ply) I can't say that the lazy-susan bearing is the most accurate "circle" i've ever come across (the bearing is a little sticky at a point to rotate by hand).

     

    Perhaps the accuracy that would be required via a direct coupling from the gearhead output to the underside of the plywood make this newly conceived contrivance impractical?

     

    If someone where to comment on this point it would be useful. However, if the idea where seen as potentially practical then any hint to the nature (by example) of a gearhead shaft to underside of plywood "coupler" would be appreciated as I have very little idea what that could be.

     

    Andrew.

     

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi John - I see you are still in touch with the thread image

     

    I had initially included the following link (in my post above) as an example of what rate of change of acceleration could "look like" wrt the the human body (jelly) but had then deleted it.

     

    In case you missed it i'm sure you'll find the re-instated link interesting https://www.youtube.com/watch?v=X4X_EUxqKEo&feature=relmfu

     

    Andrew.

     

    Edit:

    for the record, I currently understand step changes in d/dt(Acceleration) to be referred to as "jerk".