Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Arduino Oscilloscope with Processing.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 44 subscribers
  • Views 2476 views
  • Users 0 members are here
  • portable
  • challange
  • build_challenge
  • ben_heck
  • arduino
Related

Arduino Oscilloscope with Processing.

e14 Contributor
e14 Contributor over 11 years ago

Hi, I think this would be a highly useful build for those viewers on a budget. Not all of us have the ability to buy a oscilloscope so I think this would be replicated by a lot of people. It would run a processing sketch that would display a few different channels in different colors like red, green, or blue. And it wouldn't be big, it would be somewhat a compact package with an arduino and anything else that would make it work.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +1
    Hi Jordan! If you're flexible on hardware, there is a simple analog signal viewer here that uses a Raspberry Pi and XMOS board, so still fairly cheap. It's not really an oscilloscope (none of these projects…
Parents
  • clem57
    clem57 over 11 years ago

    I have to agree with @Michael Kellett, but how about a Raspberry Pi connected to a BitScope Micro for under $200? image

     

    Comments?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to clem57

    For under $200 you can get a small oscilloscope.

    Still expensive in my opinion, but it's an oscilloscope nonetheless.

     

    Example:

    Portable Mini Nano Arm DSO201 Pocket Sized Handheld Digital Storage Oscilloscope | eBay

     

    There is also the XprotoLab Portable which Ben featured in one of his episodes.

    This one cost around $100

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to toxxn

    Thanks for some more info, but do you have the url for the xprotoLab portable

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    XprotoLab is $50 or so...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57

    Thats Tiny Maaan! but explainable for the price.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to toxxn

    That isn't a proper scope, the spec is very poor, only 1Ms/second - so the maximum frequency of signal you can reasonably look at is 100kHz. Even simple micro based devices like Arduinos have 16MHz clocks so you couldn't use it to work on them.

    Far better buy a second hand scope (Ebay ?) for the same money.

    The XprotoLab is faster sampling (but still only 2Ms/s but the display is tiny - I can't see it being much use.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to michaelkellett

    The Xprotolab is a DIY Kit.

    Whether or not its of much use, you still get the credit in building your own Oscilloscope.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to toxxn

    how accurate is it though?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to e14 Contributor

    Not sure to be honest, it has been some time since I last watched the episode Ben built it in.

    According to Michael Kellett as mentioned above, it might not be of much use due to its small screen and whatnot.

    With the Xprotolab being a DIY kit, it might be a novelty more than anything. I will do a little more research into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to toxxn

    OK, thanks Cory

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to e14 Contributor

    Okay so I read a few reviews and quite a few people were saying the xprotolab was very accurate. Upon looking more into it I also learned a few more things about it. As previously mentioned I thought it to be a DIY kit, however it seems to be ready right out of the box. I think I mistook it for being DIY because Ben made a custom case and whatnot for it in his episode making it simply customizable rather than DIY. However you can plug this little scope directly into a breadboard or integrate it directly into a project making it very handy since its a DIP package. It also seems to be more than just a scope, its an ATXMEGA32A4U Development Board, Logic Analyzer, Mixed Signal Oscilloscope, and an Arbitrary Waveform Generator all in one tiny little package complete with its Micro USB and OLED display (Which can be changed to be black on white or white on black display). One person also mentioned that there was a dual voltmeter function as well.

     

    Here are some specifications I found:

    Dimensions: 1.615" x 1.01"

    Features:

    • ATXMEGA32A4U Development Board
      • ATXMEGA32A4U 36KB Flash, 4KB SRAM, 1KB EEPROM
      • Graphic OLED display 0.96", 128x64 pixels
      • PDI interface
      • 4 tactile switches
      • USB connectivity
    • Logic Analyzer
      • 8 Digital Inputs, 3.3V level
      • Maximum sampling rate: 2MSPS
      • Frequency counter: 12Mhz
      • Protocol Sniffer: UART, I2C, SPI
      • Internal pull up or pull down.
      • Buffer size: 256
    • Mixed Signal Oscilloscope
      • 2 Analog Inputs
      • Maximum Sampling rate: 2MSPS
      • Analog Bandwidth: 200kHz
      • Resolution: 8bits
      • Input Impedance: 1MΩ
      • Buffer size per channel: 256
      • Input Voltage Range: -14V to +20V
    • Arbitrary Waveform Generator
      • 1 Analog Output
      • Maximum conversion rate: 1MSPS
      • Analog Bandwidth: 44.1kHz
      • Resolution: 8bits
      • Output current > +/- 7mA
      • Buffer size: 256
      • Output Voltage: +/- 2V

     

     

    The reviews I read make this one seem pretty useful especially for its size and considering the functionality it has to offer.

    Here are a couple of sites I looked at:

    https://www.sparkfun.com/products/11643

    http://tronixstuff.com/2011/02/13/the-worlds-smallest-oscilloscope/

     

    I think I may end up picking one up myself after looking into this a little further, especially since I found it cheaper than I first saw it at.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to toxxn

    You might want to compare it with this:

     

    Digilent Inc. - Digital Design Engineer's Source

     

    The Digilent Analog Discovery is dead cheap to students ($99) and offers much better performance but perhaps not quite as accessible for hacking (and needs a PC to work).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago in reply to toxxn

    You might want to compare it with this:

     

    Digilent Inc. - Digital Design Engineer's Source

     

    The Digilent Analog Discovery is dead cheap to students ($99) and offers much better performance but perhaps not quite as accessible for hacking (and needs a PC to work).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • toxxn
    toxxn over 11 years ago in reply to michaelkellett

    With the DAD not being portable and the price tag being $279, I don't see it being a  viable option, at least not for me.

    It looks to be a nice piece of equipment however and I do think it would be well worth the price IF I were a student, however I graduated some time ago.