Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Ben's Home-Brew Solder Reflow Oven 2.0 Episode -- Episode 116
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 17 Jan 2014 3:24 PM Date Created
  • Last Updated Last Updated: 10 Jan 2014 8:24 AM
  • Views 7276 views
  • Likes 4 likes
  • Comments 39 comments
Related
Recommended

Ben's Home-Brew Solder Reflow Oven 2.0 Episode -- Episode 116

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Materials
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Ben's fed-up with the difficulty of soldering surface-mount components by hand and builds a new reflow oven to keep in his shop. He transforms an inexpensive toaster over into a vital tool for electronics engineers and tinkerers. In this updated oven, he uses two thermal couples to ensure even heat distribution and effective reflow.
  • 116:
  • reflow
  • ben's
  • solder
  • episode
  • 2.0
  • oven
  • ben_heck
  • heck
  • ben
  • tbhs_ep
  • home-brew
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • colecago
    colecago over 12 years ago in reply to mazzmn +1
    I'm not sure, but I bet most IC sensors wouldn't work well inside an oven, too hot. As for the Thermocouple, you don't need the translation IC, you could just use an Op-amp and math if you know the specs…
  • Sabrina
    Sabrina over 12 years ago in reply to e14 Contributor +1
    Hi- You can see the details available for this show on Ben's blog- Episode 116 Project Files
  • bigdog1
    bigdog1 over 11 years ago in reply to clem57 +1
    thank you.
  • matas1
    matas1 over 12 years ago in reply to colecago

    Well, I have a RasPi but I really don't want to use an SD card, as they've proven unreliable (except for the most expensive ones). I would like to put it into an enclosure and have it in fire and forget manner, once I've done everything I need on it. Most likely I'll not be the only one using it, moving it around, loaning it to friends, etc. and I want to minimise the risk of anything going awry. RasPi without SD card would be the single solution to my problem... Is there such a thing?

     

    I would require ethernet shield only to configure wireless connection (or something like that, don't have that concept worked out in my head yet.) I don't want to reprogram arduino everytime a friend asks me to lend him the oven so he can connect to his own wireless.

    One of the ideas I came across is connecting arduino via serial port to TL-WR703N wireless router

    One is using Spark and cloud.

    and so on...

     

    I don't know...Its been occupying my mind for a week now, making me losing sleep because of all the possibilities image

    I'm lost...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colecago
    colecago over 12 years ago in reply to matas1

    I believe the SPI I was using for those sensors was bit-banged, so it was kind of slow.  I wouldn't recommend putting all of those things on a SPI bus with an Arduino.  The Arduino is a pretty limited device.

     

    Maybe look into using a Raspberry Pi instead, they have a TFT touch screen that fits on it, it already has ethernet, and there are a lot of tutorials on SPI sensors and I/O control with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • matas1
    matas1 over 12 years ago in reply to benheck

    Hi,

    I'm new at this but i love to learn new stuff.....I would like to make this, but beside just copying your thing, i'd like to add network access and a web server where i could set the values, and monitor progress...(timer, current temp, etc...)

    What are the limits of the SPI ?

    will i run into a problem if i grab a tft touch screen, ethernet shield, wifi shield, and those two sensors?

    if yes, is there some way to avoid it? other MCU? 1-way type sensors?

    what are the memory restrictions? i'd like to avoid SD cards if possible.

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colecago
    colecago over 12 years ago in reply to sb72104

    You might be better off foregoing the max31855, they take a little time to read and are expensive.  There are other thermocouple cards out there that output an analog signal and still do cold junction compensation and such and are a much cheaper.  I'll look on Monday as I'm using some in another project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sb72104
    sb72104 over 12 years ago in reply to Ironaxe

    I'm working on a Schematic for a board that includes the max31855's, the avr processor, power supply and connectors for the lcd and ssr "all inclusive".  it's kinda hard when I work 60+ hours a week but I'm getting there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Ironaxe
    Ironaxe over 12 years ago

    I would really love to see real Schematics/BOM´s for this kind of Projects.

    So any Hobbyist can build one for himself. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sb72104
    sb72104 over 12 years ago in reply to colecago

    I guess I need to find a good Arduino tutorial.  I have never messed with one. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    Not sure what Solid State relay was used exactly, they tend to be expensive, I think that was his ebay comment to try there if you can't find a cheap one elsewhere.  This is probably comparable to what we used

    SSR http://www.newark.com/opto-22/240d10/ssr-panel-mount-280vac-32vdc-10a/dp/96F1061

     

    Here is the thermocouple stuff

    Thermocouple reader http://www.adafruit.com/products/269

    Thermocouples Ready-Made Insulated Thermocouples, Models 5TC-GG, 5TC-TT  (5TC-GG-K-30-36)

     

    and for LCD we used a generic 16x2 character display he had lying around the shop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • messi
    messi over 12 years ago

    Hi Ben

    nice video but there things which could be improved.

    1.) Use a convection oven. It will improve the soldering process a lot.

    2.) To get a more accurate solder profile, you have to connect the thermocouplers to the PCB board.

    Otherwise you will measure the air temperature, which will rise much faster than the PCB temperature

    3.) Use a program which shows you the temperature curve against a optimal solder profile.

    4.) Always run a dummy test first. This will heat up the oven. It can be critical when you have to reach a solder phase in a certain time.

     

    Cheers. J 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Sabrina

    Like Stephen is mentioning: There is only the program-file for the Arduino(?).

    What I need is the BOM, so I know which components Ben has used for this mod.

    In the movie there is a hint to look at ebay for the thermocouple interfaces, but which are used here?

    The SolidState used? etc...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>