element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Smart Drive motor as a motor 'and' as a generator?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 45 replies
  • Answers 1 answer
  • Subscribers 34 subscribers
  • Views 10634 views
  • Users 0 members are here
  • drive
  • smart
  • dc
  • brushless
  • motor
  • generators
Related

Smart Drive motor as a motor 'and' as a generator?

e14 Contributor
e14 Contributor over 12 years ago

Hi

I am working on a project where I want to use a Smart Drive Motor (Found in Fisher and Paykel washing machines, and also in LG and Samsung machines) as a motor, and then as a generator.  The problem I am having is getting the motor to work.  It needs a motor controller, but I haven't found anything in a post or anywhere that provides a list of parts and schematic. I am hoping to have the capabiltiy within the system to switch between a motr and a generator.

Given my level of capability I would really like a start to end project description.

 

Does anyone know of such a description or is anyone able to help me out with building this project?

 

Thanks

 

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colecago +1
    Hi I have drawn up the schematic as I see it at this point. Points to note are that the motor is in a 3-phase star configuration. I have also drawn in a relay to allow to switch between the motor and generator…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett +1
    Hi Michael, Due to me still being a newbie in this area, I can only offer up the info I have gleaned from the internet. I think the reason this is not a simple stepper is because of the arrangement of…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
  • colecago
    0 colecago over 12 years ago

    What do you want the generator to do?  Charge a battery or something?

     

    Basically look for a 4Q motor drive that can do regeneration.  Regeneration/regen/regen braking basically dumps the energy back onto the input line

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    At this stage I actually want the generator to do as little as light some bulbs.  I am working on prototyping a new type of transmission system, instead of a gearbox.   So I want to run the motor and then switch it over to a generator.  As mentioned in the original post I would really like to get a full description of what I need to set this up, because, whilst I am learning as quickly as I can, this is outside of my realm of expertise, so specifics and details are what I need.  I am not even sure what a 4Q is.

     

    Cheers

     

    Si

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    Sorry, had some bad ideas here.

     

    I think you might be able to accomplish this with an h bridge used in a non standard way. I'll look into more tomorrow and post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    It is sort of like an electric car, except that I anticipate that I would run the motor up to a set speed, and then switch over (relay?) to the generator mode and keep it that way as the input energy (wind turbine or similar) would then keep the generator turning, via the mechanical transmission, which is what I am trying to demonstrate.

     

    I look forward to your further comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    One big question first, what size and type of motor? That will matter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago

    I believe our interlocutor is referring  to a BLDC motor:

     

    InstaSPINTm-BLDC Solution - INSTASPIN-BLDC - TI Software Folder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to D_Hersey

    Is that the controller you are using?  Wow, that thing can support up to like a 6.6HP motor.

     

    I think you might have a problem with a controller that smart if it doesn't allow the motor to freewheel, it probably does regen braking and everything already, so breaking out your own load braking might be difficult.

     

    If using a large brushless motor like that can support, I suggest using a 3phase bridge and a motor contactor to output to your regen load.  Basically you'll want to disable the drive, not stop it or brake it, to allow the system to freewheel, then on the output of the 3phase bridge turn on the contactor to put the current through your load.

     

    You won't want to run the drive while diverting the current to your regen load though, otherwise you'll just power it from your motor drive.

     

    I'll draw up a diagram in a bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago

    Examples of a 3 phase bridge

    VS-26MT80 - VISHAY FORMERLY I.R. VS-26MT80 - RECTIFIER, 3 PHASE, 800V, 25A, D-63 | Newark element14 US

    and contactor

    120-901 - WHITE RODGERS 120-901 - CONTACTOR, SPST-NO, 12VDC, 100A, BRACKET | Newark element14 US

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago

    Losses are of great concern in regenerative braking, so sometimes they use synchronous rectifiers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago

    That contactor could be overkill depending on your regen brake load. You might be able to get away with a smaller relay or mosfet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>