element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Smart Drive motor as a motor 'and' as a generator?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 45 replies
  • Answers 1 answer
  • Subscribers 34 subscribers
  • Views 10643 views
  • Users 0 members are here
  • drive
  • smart
  • dc
  • brushless
  • motor
  • generators
Related

Smart Drive motor as a motor 'and' as a generator?

e14 Contributor
e14 Contributor over 12 years ago

Hi

I am working on a project where I want to use a Smart Drive Motor (Found in Fisher and Paykel washing machines, and also in LG and Samsung machines) as a motor, and then as a generator.  The problem I am having is getting the motor to work.  It needs a motor controller, but I haven't found anything in a post or anywhere that provides a list of parts and schematic. I am hoping to have the capabiltiy within the system to switch between a motr and a generator.

Given my level of capability I would really like a start to end project description.

 

Does anyone know of such a description or is anyone able to help me out with building this project?

 

Thanks

 

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colecago +1
    Hi I have drawn up the schematic as I see it at this point. Points to note are that the motor is in a 3-phase star configuration. I have also drawn in a relay to allow to switch between the motor and generator…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett +1
    Hi Michael, Due to me still being a newbie in this area, I can only offer up the info I have gleaned from the internet. I think the reason this is not a simple stepper is because of the arrangement of…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
Parents
  • colecago
    0 colecago over 12 years ago

    That contactor could be overkill depending on your regen brake load. You might be able to get away with a smaller relay or mosfet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    I have drawn up the schematic as I see it at this point.  Points to note are that the motor is in a 3-phase star configuration.  I have also drawn in a relay to allow to switch between the motor and generator wiring.  The hall sensors from the motor to the motor controller will also have a switch to disconnect them so that in generator mode the controller does not receive spurious signals.

     

    image

    I have also attached a drawing of the wiring of the motor as it is configured at the moment in regard to the coils. 

     

    image

     

    I would like to know what controller I would need to be able to run this.  (And perhaps it is the one in the link above suggested by Don, but this does seem like it manages more power than I have), and any additional detail with how to install control the controller would also be appreciated.

     

    Look forward to your comments.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    What is the motor rated at for current, power, voltage, etc?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    The info I have on the motor is as follows.

     

    Electric Supply

    Operating Voltage 220/240 V AC 50Hz

    Maximum Current 2.8 amps

     

    Motor

    Electronically commutated direct drive 3 Phase brushless DC Motor.

    Motor resistance

                                  Per Winding                    Phase to Phase

    Phase 1                    1.3 ohms @ 20degC          2.6 ohms @ 20 degC

    Phases 2 to 4            6.1 ohms @ 20 degC         12.2 ohms @ 20 degC

    Phases 5 and 6          16 ohms @ 20 degC          32 ohms @ 20 degC

     

     

    Below is a link that has the info on the motor.  It is the manual for the washing machine it comes from.  I also have a pdf that describes the same motor in relation to its use as a generator.  It doesn't seem to be available online anymore and I can't see where I attach files within the post, only images and links.  I can email it if it would help.

     

    Anyway, I hope the link to the motor manual helps. 

     

    http://www.eserviceinfo.com/downloadsm/60779/Fisher%20&%20Paykel_Several%20-%20MW%20GW%20etc.html

     

    I appreciate the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    I haven't time to go into all the details of this motor but it is seriously weird - quite possible just perfect for a washing machine but absolutely NOT your standard BLDC. For a traction/regen application you need a motor intended for the purpose where all the phases are the same - otherwise you will need to design a controller completely on your own ( there isn't a lot of stuff on the web to help you.).  Get  a normal BLDC motor and then you can use all the kits and design stuff (loads of it) on the web.

     

    I'm also worried by your earlier post where you refer to the wind turbine - are you hoping to keep the vehicle moving by extracting energy from it's passage through the air ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    I haven't time to go into all the details of this motor but it is seriously weird - quite possible just perfect for a washing machine but absolutely NOT your standard BLDC. For a traction/regen application you need a motor intended for the purpose where all the phases are the same - otherwise you will need to design a controller completely on your own ( there isn't a lot of stuff on the web to help you.).  Get  a normal BLDC motor and then you can use all the kits and design stuff (loads of it) on the web.

     

    I'm also worried by your earlier post where you refer to the wind turbine - are you hoping to keep the vehicle moving by extracting energy from it's passage through the air ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Hi Michael

    Thanks for your comments.  I am discovering that this is not an easy motor to run as a motor.  Fairly easy to run as a generator though. 

    Perhaps if I explain my scenario some more you will see why I want to stick with it.

    I am using this generator because of its shape and size.  I am building a demonstration model of a new transmission system that I have invented.  I want to be able to prove the invention works so I can move forward in seeking investors and going towards commercialisation.  I have already built the transmission system to fit this generator, and as I have tolerances of 3 mm in some places, I am sure you can appreciate that swapping the motor/generator at this stage is not an option I wish to consider.  At the time I chose the generator, I had not anticipated the difficulty involved in running it as a motor. 

    You needn't worry about me wanting to put a wind turbine on a car to power it. 'I ain't that daft'.  :-)

    The turbine reference is because that is what the transmission system is likely to be suited to.  The car comment was in relation to another comment about the motor swapping between motor and generator, as in a hybrid car.  But this is not going on a car.

    I do have an article that outlines much of what is needed, but they do not stipulate the motor controller needed, just an indication of the sort of controller I should use.  As mentioned before, this is not an area of technology I am very familiar with so I do not want to buy the wrong equipment and either find it is unsuitable, or underrated. 

     

    I look forward to any other info you can add to the discussion..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    I guess I don't understand why it needs a separate generator mode when most of the drives you will run it with can do regeneration.  If you need the separate mode just to prove it's regenerating energy, just put an current meter in series with the phases (or the input bus) and show the direction of current changed.

     

    Edit: I was assuming you were running the motor and then switching to generator mode to brake it, if that is not the case, then using the regen braking of a motor drive might not directly fit the application for you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    I was not aware that the driver could handle the regen mode, hence why I was looking to 'externally' manage generation. 

    What I need to do is start the unit as a motor and run it until it syncs with the energy input (wind turbine or surrogate), then I turn off the motor and it will run as a generator, continuing to spin, and generate power, thereby demonstrating its function as a generator.  If I can show that the generator is, in fact, generating power (or works under load) then this proves my concept, and I can move on.

     

    Does that make it clearer and does that help you decide if I can use the regen mode of a drive, or should I stick with my original plan which was to disconnect the 'motor' externally and switch to a generator mode.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Are you able to tell me how to load a pdf in this forum, because then I could load up the article I have, and perhaps you and others can review this and then suggest suitable parts?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    Here are some brushless drives that are 230VAC and take hall effect inputs. They do regen.  Not sure how well they'd do with your motor if it has strange windings.  You could always talk to their apps engineer and he might be able to help you out

     

    PML Series

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Hi

    Thanks for the link.  I have sent them an email with some of my data, so hopefully they can suggest something.

    In the meantime, I hope there might be a cheaper suggestion. 

    Thanks again.