element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Smart Drive motor as a motor 'and' as a generator?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 45 replies
  • Answers 1 answer
  • Subscribers 34 subscribers
  • Views 9092 views
  • Users 0 members are here
  • drive
  • smart
  • dc
  • brushless
  • motor
  • generators
Related

Smart Drive motor as a motor 'and' as a generator?

Former Member
Former Member over 11 years ago

Hi

I am working on a project where I want to use a Smart Drive Motor (Found in Fisher and Paykel washing machines, and also in LG and Samsung machines) as a motor, and then as a generator.  The problem I am having is getting the motor to work.  It needs a motor controller, but I haven't found anything in a post or anywhere that provides a list of parts and schematic. I am hoping to have the capabiltiy within the system to switch between a motr and a generator.

Given my level of capability I would really like a start to end project description.

 

Does anyone know of such a description or is anyone able to help me out with building this project?

 

Thanks

 

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago in reply to colecago +1
    Hi I have drawn up the schematic as I see it at this point. Points to note are that the motor is in a 3-phase star configuration. I have also drawn in a relay to allow to switch between the motor and generator…
  • Former Member
    Former Member over 11 years ago in reply to michaelkellett +1
    Hi Michael, Due to me still being a newbie in this area, I can only offer up the info I have gleaned from the internet. I think the reason this is not a simple stepper is because of the arrangement of…
  • Former Member
    Former Member over 11 years ago in reply to Former Member +1
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    I was thinking of using a four-phase stepper as resolver.  I read an article on this topic years and years ago and cannot find it.  A four-phase step motor sequence uses two signals (bipolar, unipolar is just a winding trick) that are ninety degrees out-of-phase.  The RF community refers to these as quadrature signals.  They use them for detection at much higher rates, which they can because they are not using moving parts.  These are square waves if we are full stepping. They are sinuate if we are micro-stepping. 

     

    The author connected the two coils to a resistor, on the order of the nominal coil resistance, if recall serves.  He also shunted them with back-to-back Zeners to clamp any spikes.  He used a comparator circuit to suss the signum of a step signal if he received one.  This interrupted the processor.  He had an image of the next anticipated step in memory.  If the signal conformed to this, he new he had taken another step, updated his count and image.  If not, he knew a backward step had been taken, decremented his step, and inverted his image of the next step and toggled his direction flag.  If recall serves.  I don't remember how he set up his initial configuration, or if he had to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    I was thinking of using a four-phase stepper as resolver.  I read an article on this topic years and years ago and cannot find it.  A four-phase step motor sequence uses two signals (bipolar, unipolar is just a winding trick) that are ninety degrees out-of-phase.  The RF community refers to these as quadrature signals.  They use them for detection at much higher rates, which they can because they are not using moving parts.  These are square waves if we are full stepping. They are sinuate if we are micro-stepping. 

     

    The author connected the two coils to a resistor, on the order of the nominal coil resistance, if recall serves.  He also shunted them with back-to-back Zeners to clamp any spikes.  He used a comparator circuit to suss the signum of a step signal if he received one.  This interrupted the processor.  He had an image of the next anticipated step in memory.  If the signal conformed to this, he new he had taken another step, updated his count and image.  If not, he knew a backward step had been taken, decremented his step, and inverted his image of the next step and toggled his direction flag.  If recall serves.  I don't remember how he set up his initial configuration, or if he had to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to D_Hersey

    Thanks Don,

    Is the method you suggested going to be possible with the motor I have already selected?  As mentioned it is too late to change to another motor/generator system as everything is built around the smart drive specs.