element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Smart Drive motor as a motor 'and' as a generator?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 45 replies
  • Answers 1 answer
  • Subscribers 34 subscribers
  • Views 10517 views
  • Users 0 members are here
  • drive
  • smart
  • dc
  • brushless
  • motor
  • generators
Related

Smart Drive motor as a motor 'and' as a generator?

e14 Contributor
e14 Contributor over 12 years ago

Hi

I am working on a project where I want to use a Smart Drive Motor (Found in Fisher and Paykel washing machines, and also in LG and Samsung machines) as a motor, and then as a generator.  The problem I am having is getting the motor to work.  It needs a motor controller, but I haven't found anything in a post or anywhere that provides a list of parts and schematic. I am hoping to have the capabiltiy within the system to switch between a motr and a generator.

Given my level of capability I would really like a start to end project description.

 

Does anyone know of such a description or is anyone able to help me out with building this project?

 

Thanks

 

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colecago +1
    Hi I have drawn up the schematic as I see it at this point. Points to note are that the motor is in a 3-phase star configuration. I have also drawn in a relay to allow to switch between the motor and generator…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett +1
    Hi Michael, Due to me still being a newbie in this area, I can only offer up the info I have gleaned from the internet. I think the reason this is not a simple stepper is because of the arrangement of…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    You can look to see what the competition has to offer, industrial drives aren't cheap that I've seen, and being at 230vac kind of puts you in that arena, if it was low voltage dc, you could use Chinese scooter controls.

     

    Look at kb electronics and dart controls, they were our competitors.

     

    One nice thing about the American Controls one is the voltage doubler, you can run a 230 drive on 120.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Ok Thanks.  Can you please advise on the specifics of what features I need to have with such a unit?  This is part of why I started to this discussion in the first place.  I don't really know what I am looking for, and I really don't want to buy the wrong item and have my dollars converted to smoke, quite literally, or to have a motor that doesn't turn.

     

    I want to run it on 24V DC. 

    It has Hall sensors.

     

    Not so sure about Amps, or the regenerative load part of the control.  Or whether I should stick with my initial plan to switch it over to generator mode with relays and disconnect the drive completely.

    All and any guidance in this regard would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    Oh, so low voltage input and output?  I actually worked on a 24V brushless design while I was there, but it hasn't made it to market it yet as the customer dropped out.

     

    I'm not sure how well that will turn the motor, but it looks like from that article the person was using 36V, so maybe 24V will work, it will definitely have less torque than running it off the line.  Look into 24 or 36V scooter or bike controllers, something like this

    24V 500W Brushless E Bike Scooter Controller with Hall | eBay

     

    Also, I wouldn't run this off a power supply, they can't handle regen current (most of them), you'll have to run it off a battery for the best result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to colecago

    Thanks for that.  I have found a ebike company in the city where I live so I will take the motor to them and get an opinion.  And try and get a unit from them for super cheap.  I'll keep you posted.

     

    Thanks to everyone for the interesting discussions and help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi there, did u sort this out in the end? Ive made a prototype 24volt starter generator for a 1300cc engine using a f&p motor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<