element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Schematic
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 147 subscribers
  • Views 3280 views
  • Users 0 members are here
Related

Schematic

idontunderstand
idontunderstand over 7 years ago

im 71 years old and am experimenting with electronics. However as much as I try and study I am getting bogged down with schematics. I’m ok with simple circuits but as they grow I lose all direction. Can someone please colour code a large schematic so I can see where positive and negative are in conjunction with the components. I realise for your community this is obvious but for me quite confusing. I have watched countless videos on schematics and am being told you can build circuits just by following a schematic. However not for me.

many thanks

ROGER

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 7 years ago +5
    Roger, The key to understanding electronics is to study the basic rules or laws to which all electronics must follow. These laws (Ohm's law to start with) help you better understand the flow of electricity…
  • ralphjy
    ralphjy over 7 years ago +5
    Hi Roger, Element14 has an excellent series on basic electronics called the Learning Circuit. Have you looked at that? The Learning Circuit It really helps to understand the basic circuit elements before…
  • shabaz
    shabaz over 7 years ago +4
    Hi Roger, In conjunction with all the other excellent techniques mentioned, familiarity over time will make you recognise portions because they will look like patterns you've seen before. Unless it is…
  • shabaz
    shabaz over 7 years ago in reply to idontunderstand +4
    Is there an example of the type of color-code you mean? I've tried in the past to color-code some wires, but I've only found it usable for very small circuits, such as this one: It can sometimes look fine…
  • ralphjy
    ralphjy over 7 years ago in reply to idontunderstand +4
    Hi Roger, I think part of the problem is understanding precisely what you are asking for. I know that might sound strange. I'm not sure what you mean by "where positive ends and negative starts". I think…
  • luislabmo
    luislabmo over 7 years ago +4
    Hello Roger, I think these links may be very, very useful for you: How to Read a Schematic - Sparkfun Skill Builder: Reading Circuit Diagrams - Make Luis
  • DAB
    DAB over 7 years ago +4
    Hi Roger, I am slightly younger than yourself. A good way to approach complex schematics is to create a block diagram view and then look at each section as it relates to the next block. This approach gives…
  • makerkaren
    makerkaren over 7 years ago +4
    Not sure if this will help. This is the circuit diagram from the TLC episode that just came out where I made a mask with a spinning pinwheel on it. It's a small motor controller that uses a pressure sensitive…
  • rachaelp
    rachaelp over 7 years ago +3
    Hi Roger, When you first start with electronics things which some people think are trivially obvious are not as a newbie, don't feel disheartened by this, it'll get easier with time, the key thing is to…
  • genebren
    genebren over 7 years ago in reply to idontunderstand +3
    Hi Roger, I really do understand your frustration, but schematics can represent circuits that are very dynamic. What might be positive at one instance may become negative in another. Then, there are relative…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Roger,

     

    In conjunction with all the other excellent techniques mentioned, familiarity over time will make you recognise portions because they will look like patterns you've seen before.

    Unless it is a very poor quality schematic, most people will try to draw their schematics in some well-known styles.

    This web link 101-200 electronic circuits is quite good, it has lots of small circuits to gain a quick appreciation of what types of circuits will achieve certain tasks.

    There is also 1-100 electronic circuits and 100 IC circuits and 50 555 circuits, they are all useful.

    So, for example, here are some random snippets from there:

     

     

    image

    At a glance, it is possible to tell this is a 'H-bridge' circuit, due to the shape looking like a H. It is used to switch power in either direction. It could have been drawn totally different, but people don't do that - they try to draw it in this style. It becomes an easy pattern to recognise in a larger circuit. Also without any labels, by convention it is possible to guess that the top line is a positive supply rail, and the lower is 0V. This convention wouldn't be assumed when constructing the circuit (since then precision about it is required), but it can be initially assumed when trying to guess what a schematic does.

     

    image

    Even though this is just part of a circuit, it is instantly recognizable as something that will pulse and flash LEDs in a sequence. This is because the 555 is a well-known chip for generating a single or stream of pulses, and the 4017 is well-known to convert an input pulse stream into ten outputs in sequence.

     

     

    image

    The circuit above can be assumed to be some sort of amplifier, with two stages, since that's a normal use of a transistor. It look designed for amplifying AC signals, since there are capacitors on the input and output that would block DC.

     

    Anyway, these are just some examples, there are many more sub-circuits like these to explore.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Hi Roger,

     

    In conjunction with all the other excellent techniques mentioned, familiarity over time will make you recognise portions because they will look like patterns you've seen before.

    Unless it is a very poor quality schematic, most people will try to draw their schematics in some well-known styles.

    This web link 101-200 electronic circuits is quite good, it has lots of small circuits to gain a quick appreciation of what types of circuits will achieve certain tasks.

    There is also 1-100 electronic circuits and 100 IC circuits and 50 555 circuits, they are all useful.

    So, for example, here are some random snippets from there:

     

     

    image

    At a glance, it is possible to tell this is a 'H-bridge' circuit, due to the shape looking like a H. It is used to switch power in either direction. It could have been drawn totally different, but people don't do that - they try to draw it in this style. It becomes an easy pattern to recognise in a larger circuit. Also without any labels, by convention it is possible to guess that the top line is a positive supply rail, and the lower is 0V. This convention wouldn't be assumed when constructing the circuit (since then precision about it is required), but it can be initially assumed when trying to guess what a schematic does.

     

    image

    Even though this is just part of a circuit, it is instantly recognizable as something that will pulse and flash LEDs in a sequence. This is because the 555 is a well-known chip for generating a single or stream of pulses, and the 4017 is well-known to convert an input pulse stream into ten outputs in sequence.

     

     

    image

    The circuit above can be assumed to be some sort of amplifier, with two stages, since that's a normal use of a transistor. It look designed for amplifying AC signals, since there are capacitors on the input and output that would block DC.

     

    Anyway, these are just some examples, there are many more sub-circuits like these to explore.

    • Cancel
    • Vote Up +4 Vote Down