element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Schematic
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 147 subscribers
  • Views 3280 views
  • Users 0 members are here
Related

Schematic

idontunderstand
idontunderstand over 7 years ago

im 71 years old and am experimenting with electronics. However as much as I try and study I am getting bogged down with schematics. I’m ok with simple circuits but as they grow I lose all direction. Can someone please colour code a large schematic so I can see where positive and negative are in conjunction with the components. I realise for your community this is obvious but for me quite confusing. I have watched countless videos on schematics and am being told you can build circuits just by following a schematic. However not for me.

many thanks

ROGER

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 7 years ago +5
    Roger, The key to understanding electronics is to study the basic rules or laws to which all electronics must follow. These laws (Ohm's law to start with) help you better understand the flow of electricity…
  • ralphjy
    ralphjy over 7 years ago +5
    Hi Roger, Element14 has an excellent series on basic electronics called the Learning Circuit. Have you looked at that? The Learning Circuit It really helps to understand the basic circuit elements before…
  • shabaz
    shabaz over 7 years ago +4
    Hi Roger, In conjunction with all the other excellent techniques mentioned, familiarity over time will make you recognise portions because they will look like patterns you've seen before. Unless it is…
  • shabaz
    shabaz over 7 years ago in reply to idontunderstand +4
    Is there an example of the type of color-code you mean? I've tried in the past to color-code some wires, but I've only found it usable for very small circuits, such as this one: It can sometimes look fine…
  • ralphjy
    ralphjy over 7 years ago in reply to idontunderstand +4
    Hi Roger, I think part of the problem is understanding precisely what you are asking for. I know that might sound strange. I'm not sure what you mean by "where positive ends and negative starts". I think…
  • luislabmo
    luislabmo over 7 years ago +4
    Hello Roger, I think these links may be very, very useful for you: How to Read a Schematic - Sparkfun Skill Builder: Reading Circuit Diagrams - Make Luis
  • DAB
    DAB over 7 years ago +4
    Hi Roger, I am slightly younger than yourself. A good way to approach complex schematics is to create a block diagram view and then look at each section as it relates to the next block. This approach gives…
  • makerkaren
    makerkaren over 7 years ago +4
    Not sure if this will help. This is the circuit diagram from the TLC episode that just came out where I made a mask with a spinning pinwheel on it. It's a small motor controller that uses a pressure sensitive…
  • rachaelp
    rachaelp over 7 years ago +3
    Hi Roger, When you first start with electronics things which some people think are trivially obvious are not as a newbie, don't feel disheartened by this, it'll get easier with time, the key thing is to…
  • genebren
    genebren over 7 years ago in reply to idontunderstand +3
    Hi Roger, I really do understand your frustration, but schematics can represent circuits that are very dynamic. What might be positive at one instance may become negative in another. Then, there are relative…
Parents
  • idontunderstand
    idontunderstand over 7 years ago

    Ralph

    it appears no matter how many times I say it that no one is understanding that I really struggle understanding schematic drawings. I have watched many many schematic turorials and still don’t get it. I have also watched The Learning Circuit tutorials and still don’t get it.  I’m ok with basic schematics and can build simple one dimensional circuits but get confused when the circuits get larger. I can’t get my head around where positive ends and negative starts. I know this is really simple to you and must be frustrating that I don’t get it but that is how it is.

    If only someone would be kind enough to colour code a schematic drawing to help me understand.

     

    Many thanks

     

    Roger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • idontunderstand
    idontunderstand over 7 years ago

    Ralph

    it appears no matter how many times I say it that no one is understanding that I really struggle understanding schematic drawings. I have watched many many schematic turorials and still don’t get it. I have also watched The Learning Circuit tutorials and still don’t get it.  I’m ok with basic schematics and can build simple one dimensional circuits but get confused when the circuits get larger. I can’t get my head around where positive ends and negative starts. I know this is really simple to you and must be frustrating that I don’t get it but that is how it is.

    If only someone would be kind enough to colour code a schematic drawing to help me understand.

     

    Many thanks

     

    Roger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to idontunderstand

    Is there an example of the type of color-code you mean?

    I've tried in the past to color-code some wires, but I've only found it usable for very small circuits, such as this one:

    image

    It can sometimes look fine, but although there are three black lines at the bottom, they are actually separate wires that are not electrically connected, they are connected to MOSFETs. So the color code can get confusing too if done in this way (and there are not enough easy-to-identify shades for most circuits, to have one shade per net).

    This circuit uses red to indicate positive, and the three black lines are 'kind of' negative, but they are all different negatives. The left black line is a permanent negative, and the other two are switched negatives. It would be hard to convey this meaning with separate colors, but can be explained in a text explanation of the circuit, or perhaps by recognizing the pattern of two MOSFETs and resistor as shown.

     

    I prefer when circuit diagrams look like this; here the section is identified, it is clear that it is the power supply sub-circuit that is part of a larger circuit, because it has its own box and title, within a larger schematic sheet. Do you mean this dashed box ought to be shaded in a single color, so that the sub-circuit is identified by color?

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to idontunderstand

    Hi Roger,

     

    I think part of the problem is understanding precisely what you are asking for.  I know that might sound strange.  I'm not sure what you mean by "where positive ends and negative starts".  I think that we might be struggling with how to color code a schematic for you.

     

    I'm going to be offline for a while, but if you can explain exactly what you need,  I'm sure someone could help.  It really would be good if you could provide an example of a schematic you don't understand as a starting point.  And indicate how you would want color coding applied to that schematic.

     

    Ralph

    • Cancel
    • Vote Up +4 Vote Down