element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Schematic
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 147 subscribers
  • Views 3280 views
  • Users 0 members are here
Related

Schematic

idontunderstand
idontunderstand over 7 years ago

im 71 years old and am experimenting with electronics. However as much as I try and study I am getting bogged down with schematics. I’m ok with simple circuits but as they grow I lose all direction. Can someone please colour code a large schematic so I can see where positive and negative are in conjunction with the components. I realise for your community this is obvious but for me quite confusing. I have watched countless videos on schematics and am being told you can build circuits just by following a schematic. However not for me.

many thanks

ROGER

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 7 years ago +5
    Roger, The key to understanding electronics is to study the basic rules or laws to which all electronics must follow. These laws (Ohm's law to start with) help you better understand the flow of electricity…
  • ralphjy
    ralphjy over 7 years ago +5
    Hi Roger, Element14 has an excellent series on basic electronics called the Learning Circuit. Have you looked at that? The Learning Circuit It really helps to understand the basic circuit elements before…
  • shabaz
    shabaz over 7 years ago +4
    Hi Roger, In conjunction with all the other excellent techniques mentioned, familiarity over time will make you recognise portions because they will look like patterns you've seen before. Unless it is…
  • shabaz
    shabaz over 7 years ago in reply to idontunderstand +4
    Is there an example of the type of color-code you mean? I've tried in the past to color-code some wires, but I've only found it usable for very small circuits, such as this one: It can sometimes look fine…
  • ralphjy
    ralphjy over 7 years ago in reply to idontunderstand +4
    Hi Roger, I think part of the problem is understanding precisely what you are asking for. I know that might sound strange. I'm not sure what you mean by "where positive ends and negative starts". I think…
  • luislabmo
    luislabmo over 7 years ago +4
    Hello Roger, I think these links may be very, very useful for you: How to Read a Schematic - Sparkfun Skill Builder: Reading Circuit Diagrams - Make Luis
  • DAB
    DAB over 7 years ago +4
    Hi Roger, I am slightly younger than yourself. A good way to approach complex schematics is to create a block diagram view and then look at each section as it relates to the next block. This approach gives…
  • makerkaren
    makerkaren over 7 years ago +4
    Not sure if this will help. This is the circuit diagram from the TLC episode that just came out where I made a mask with a spinning pinwheel on it. It's a small motor controller that uses a pressure sensitive…
  • rachaelp
    rachaelp over 7 years ago +3
    Hi Roger, When you first start with electronics things which some people think are trivially obvious are not as a newbie, don't feel disheartened by this, it'll get easier with time, the key thing is to…
  • genebren
    genebren over 7 years ago in reply to idontunderstand +3
    Hi Roger, I really do understand your frustration, but schematics can represent circuits that are very dynamic. What might be positive at one instance may become negative in another. Then, there are relative…
Parents
  • idontunderstand
    idontunderstand over 7 years ago

    Karen

    I watched the video with the rotating fan and was intrigued the way you made the connections under the board and for the first time began to get an idea. However the  connection part was sped up so still a little confusing. The schematic you have colour coded is a great help and almost what I need. However I do understand from your drawing the run of the positive and ground runs but what is, and always has been is all the other lines within the schematic that you have not coloured. Which is positive and which goes to ground. I know you will think this is a ridiculous question but I don’t follow the positive and ground runs inside the schematic.

    Im not conversant with the 555 timer so don’t know what each pin does.

    From the base of M1 the - sign is connected to the diode D3 which in turn connects to the positive plane, It appears to me, the novice, that negative is connecting directly to positive the diode D3.

    From R1 to VR1 and to R2 appear to come from the positive plane and stops at D1, but then from VR1 it looks like power goes through D2 and also picked up below D1. I am so confused which is positive and negative. I know you will be thinking I am overthinking it but if you could draw on the flow direction and colour the lines within the schematic to show which is which. Is it that I’m not understanding the way the components operate that is confusing me?  I think i need to be next to someone while the circuit is built from a schematic to help me understand how it is put together.

     

    love your videos.

     

    thanks

     

    Roger

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 7 years ago in reply to idontunderstand

    Hi Roger,

     

    I really do understand your frustration, but schematics can represent circuits that are very dynamic. What might be positive at one instance may become negative in another.  Then, there are relative degrees of positive (represented by number of volts above ground).  A voltage divider may take a 5 volt supply and generate a mid-point that is less than 5 volts, but still more positive than ground (0 Volts).

     

    In your comment above, you zeroed in on one of the more obscure aspects of the circuit, diode D3.  99% of the time the diode does absolutely nothing, it exists to route current back into the power rail when the motor is switch off (de-energizing Q1).  The motor has a magnetic field around it when the motor is driven (Q1 on), when switched off, the magnetic field collapses and generates a large voltage spike that could damage components in the circuit.  Diode D3, routes this current into the power rail.  Why not to ground?  If the diode directed current to ground, it would also short current to ground when the motor was on (not a good thing).  This concept is a little more advanced that beginner electronics, but it is an important lesson.

     

    When I was first learning electronics, I was fascinated by schematics.  I could not understand them in their entirety, but with time and education they became clearer and clearer.  Be patient, time and studying will allow you to understand schematics more fully.

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 7 years ago in reply to idontunderstand

    Hi Roger,

     

    I really do understand your frustration, but schematics can represent circuits that are very dynamic. What might be positive at one instance may become negative in another.  Then, there are relative degrees of positive (represented by number of volts above ground).  A voltage divider may take a 5 volt supply and generate a mid-point that is less than 5 volts, but still more positive than ground (0 Volts).

     

    In your comment above, you zeroed in on one of the more obscure aspects of the circuit, diode D3.  99% of the time the diode does absolutely nothing, it exists to route current back into the power rail when the motor is switch off (de-energizing Q1).  The motor has a magnetic field around it when the motor is driven (Q1 on), when switched off, the magnetic field collapses and generates a large voltage spike that could damage components in the circuit.  Diode D3, routes this current into the power rail.  Why not to ground?  If the diode directed current to ground, it would also short current to ground when the motor was on (not a good thing).  This concept is a little more advanced that beginner electronics, but it is an important lesson.

     

    When I was first learning electronics, I was fascinated by schematics.  I could not understand them in their entirety, but with time and education they became clearer and clearer.  Be patient, time and studying will allow you to understand schematics more fully.

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down