Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents 3D Object Rendering Using an FPGA -- Episode 558
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Jul 2022 2:04 PM Date Created
  • Last Updated Last Updated: 8 Jul 2022 7:24 AM
  • Views 136463 views
  • Likes 8 likes
  • Comments 15 comments

3D Object Rendering Using an FPGA -- Episode 558

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Rendering of 3D models is a computationally expensive task and often slow. With hardware customization and reprogrammable flexibility using FPGAs, highest performance can be achieved. So we are going to build customized hardware on a FPGA Cyclone IV E (DE0 nano board) to render 3D objects into images, and finally, display the rendered images on a monitor over VGA. I have used Verilog for the hardware implementation so that the code can be easily compiled for most FPGAs out there. Happy Rendering!

 

Supplemental Material:

  • Triangle rasterization
  • Download Quartus Prime Lite
  • Rotation Matrix
  • 558_Resources.zip

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Development Kit, Altera Cyclone IV FPGA , DE0-Nano, 2x GPIO Headers, 32MB SDRAM, Accelerometer TERASIC TECHNOLOGIES 1 Buy Now
 

Additional Parts:

Wire Gauge:28AWG

element14 presents

element14 presents  |  About Surbika Rastogi |  Project Videos

  • Rasterization
  • fpga
  • rendering
  • surbika
  • element14 presents
  • verilog
  • friday_release
  • vlsi
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • surbhika
    surbhika over 4 years ago in reply to shabaz +1
    shabaz i am keen to get the complete results too and also going through few boards which facilitates easy integration with micro-controllers... may be that will be a better and optimised step forward.
  • surbhika
    surbhika over 4 years ago in reply to beacon_dave +1
    There was no way to fit more than few triangles in this design. Though there are few little things in terms of floating point representation etc.which can be optimized in the code (which i realized afterwards…
  • surbhika
    surbhika over 4 years ago in reply to cstanton +1
    Indeed. Limited resources lead to optimized designs!
  • flyingbean
    flyingbean over 4 years ago

    Zynq FPGA is a good way for accelerated graphic design since the transition latency between the processor and the acceleration engine could be a bottle neck in a real project with higher speed/resolution. However, pure FPGA logic implementation is a good approach for the sub-module development  without being stopped by the dependencies from the processor side, such as drivers, OS, etc..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to michaelkellett

    Also, I think the project is already more interesting without the Zync processor, and harder for people to replicate or port across if they don't have the same device.

    Also, surbhika wondering, since GPUs are normally very parallel, if (say) FPGA boards eventually become a limit for the design you're implementing, perhaps the architecture can be paralleled across additional FPGA boards in future. That could be an extremely interesting element14 presents video too! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to surbhika

    That board has a Zynq processor which has more on chip logic than the Arty board. It costs a bit more but the price per LUT is probably lower.

    If its a good board for you depends very much on what you are trying to do.

    The Pynq process is a lot further abstracted from the hardware than using Verilog. The Zynq is a Linux application processor with an FPGA bolted on. (I know you can run other software on it but in reality you can only go where the support is.) If you look at the questions on forums and support sites about Zynq boards you'll find a very large proportion are about Linux and how to work around the enormously complex Vivado/Vitis toolset.

    If you want to learn how to make a good GPU, or how to efficiently translate complex maths alogithms into hardware, then stick with Verilog or VHDL, keep away from the Zynq and stick with pure FPGAs.

    As DAB woud say, just my 2c worth.

    Other people will have different opinions.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • surbhika
    surbhika over 4 years ago in reply to michaelkellett

    michaelkellett i was rather pondering to convert it into a hardware accelerated configuration using PYNQ with board such as Farnell 2913033 .

    Do you think it would be a good idea?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to cstanton

    You have the Arty boards in stock:

    Farnell: 2775205 (£117)

    or if you were feeling very generous:

    the Farnell 2760616 (£2202)

    would make a pretty good GPU !

    It has on board HDMI and the FPGA has 840 DSP slices and 2Mbytes of on chip block RAM.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to michaelkellett

    It's easier if the product's in stock at one of our regional stores, www.newark.com, www.farnell.com, https://sg.element14.com / https://au.element14.com / https://cn.element14.com etc.

    Maybe there's something in the Avnet & Tria Boards Community range of products?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to shabaz

    Hello Shabaz,

    My first thought was the Digilent Nexys board but it's out of stock.

    Second thought was Aliexpress, I've bought several FPGA dev boards from there and so far they have all worked !

    Not tried this one but it would be a step up from the Cyclone IV.

    https://www.aliexpress.com/item/32691533741.html?spm=a2g0o.productlist.0.0.24de5b711gu7rM&algo_pvid=d93627fe-f626-4fc5-9772-52be7283b489&algo_exp_id=d93627fe-f626-4fc5-9772-52be7283b489-0&pdp_ext_f=%7B%22sku_id%22%3A%2266513301682%22%7D&pdp_npi=2%40dis%21GBP%21%2177.6%21%21%21%21%21%402100bde316575280936974536e0dd8%2166513301682%21sea

    The free alternative is an unopened (and therefor unused) Arty. (bought for  a project a long time ago by me, won't ever get used now.)

    Both boards have Artix 35 chips (not ideal for this, an Artix 100 as fitted to the Nexys would be better).

    The ALiexpress board has SDRAM, slower but easier to work with, the Arty has much faster DDR3 RAM and more of it, the downside is you need to spend some time wrestling with the MIG and Xilinx's DDRAM interface.

    So, if E14 can arrange to get it from me to surbhika I'm ahppy to post it to them in the UK.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 4 years ago

    Very good walk through of the process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • surbhika
    surbhika over 4 years ago in reply to cstanton

    Indeed. Limited resources lead to optimized designs!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • surbhika
    surbhika over 4 years ago in reply to beacon_dave

    There was no way to fit more than few triangles in this design. Though there are few little things in terms of floating point representation etc.which can be optimized in the code (which i realized afterwards) to fit more triangles. But that complete car model (i showed initially) was almost impossible to even store in ROM let alone rendering it. It's a single clock cycle implementation right now. I wish to build pipeline to allow rendering of just few triangles in a single cycle.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>