Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Tinkering vs Engineering: Can You Build a Laptop from Scratch? -- Episode-640
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 22 Jan 2024 5:16 PM Date Created
  • Last Updated Last Updated: 31 Jan 2024 7:56 PM
  • Views 3057 views
  • Likes 7 likes
  • Comments 17 comments

Tinkering vs Engineering: Can You Build a Laptop from Scratch? -- Episode-640

Clem's latest project takes a deep dive into laptop design, merging various components, such as a BLE keyboard, compute module, mouse, and a universal diagnostic screen into a custom-built laptop. However, the path to success wasn't without its challenges. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Downloads | Bonus Video | Bill of Material | Discussion

The project required a unique power system. For that, Clem opted for multiple 2000mAh LiPo cells, instead of a single large one. To achieve the necessary voltages (3.3V@1A, 5V@2.5A, and 12V@0.5A), Clem faced the complexity of generating multiple voltages from a single-cell source. This involved designing a switching converter, a task he had never done before.. 

image

Troubles arose when attempting to parallelize the step-up converters. Clem's initial approach faced issues with voltage regulation and load-induced voltage drops. The struggle to balance multiple step-up converters led to unexpected challenges, impacting the overall system's stability. Despite successful testing of the charging circuit, integrating the system with an actual computer brought about further complications. 

image

Clem wanted to use a Sudosom module; however, development wasn’t quite complete. This prompted a switch to a Raspberry Pi Compute Module 4. However, the step-up converters failed to deliver sufficient current, causing the voltage to drop and the computer to brown out. Even switching to a CM4 Lite did not resolve the problem. 

image

In a last-ditch effort, Clem used resistors in an effort to control the voltage, but realized that the project demanded more expertise in power supply construction than he currently possessed. The undertaking highlighted the distinction between tinkering and engineering, emphasizing the need for precise measurements and in-depth knowledge in the latter. 

image

Clem's rapid one-month endeavor revealed the importance of a well-planned and fresh design for such complex undertakings. 

Downloads and Links:

  • Download CAD Files and Schematics!

Bonus Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Materials:

Product Name Manufacturer Quantity Buy Kit
MICROCHIP Power Load Distribution Switch IC, Active Low, 1 Output, 5.5 V in, 700 mA, 0.14 ohm, SOIC-8 MICROCHIP 5 Buy Now
MOLEX HDMI Connector, 19 Contacts, Receptacle, PCB Mount, Surface Mount Right Angle MOLEX 2 Buy Now
MIKROELEKTRONIKA Rechargeable Battery, 3.7 V, Lithium Polymer, 2 Ah, JST MIKROELEKTRONIKA 3 Buy Now
BOURNS Power Inductor (SMD), 10 µH, 2.1 A, Shielded, 2.5 A, SRR0745A BOURNS 6 Buy Now
TOREX DC-DC Switching Synchronous Step-Up Regulator, 0.65-6V in, 5V out, 0.5A out, 3MHz, SOT-25, 5Pin TOREX 6 Buy Now
TEXAS INSTRUMENTS DC-DC Switching Boost Step Up Regulator, Adjustable, 2.7V-14Vin, 600 kHz, 2Aout, SOT-23-5 TEXAS INSTRUMENTS 2 Buy Now
MICROCHIP Battery Charger for 1 Cell of Li-Ion, Li-Pol battery, 6V input, 4.2V / 500mA charge, SOT-23-5 MICROCHIP 3 Buy Now
TOUCHSCREEN 10.1 MULTICOMP PRO 1 Buy Now
MOLEX FFC / FPC Board Connector MOLEX 6 Buy Now
 

element14 presents

element14 presents  |  About Clem  |  Project Videos 

  • real engineering vs tinkering
  • DIY electronics learning
  • Lipo cell configurations
  • Power supply challenges
  • Custom laptop design
  • maker vs engineer
  • Project complexities
  • BLE keyboard integration
  • Custom power system design
  • Step-up converter design
  • laptop from scratch
  • Compute Module 4 issues
  • Technical challenges in laptop building
  • Maker community insights
  • Laptop engineering hurdles
  • Circuit troubleshooting
  • Switching converter pitfalls
  • step up power supply
  • friday_release
  • DIY electronics projects
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 2 years ago in reply to baldengineer +1
    Quote from an SMPS book I bought today:
  • gendragonfly
    gendragonfly over 2 years ago in reply to mayermakes +1
    Thank you Clem, for all the great videos & projects! For someone who is learning as they go, you really tend to pick the most challenging projects
Parents
  • baldengineer
    baldengineer over 2 years ago

    You've embarked on an impressive project and made an incredible project.

    However. Regarding your power supply, I took a peek at your KiCad files—just a few critical issues I see right away.

    I am using this converter for an example (so I can use designators.)

    image

    1. For the ceramic output capacitor (C28), you should have a relatively large CV 0805 (imperial) MLCC. A large CV means the highest rated voltage at whatever capacitance you picked. An 0805 has much less DC-Bias effect than a 0603 and is available with higher rated voltages. Since you have the space, I would also use a 0805 on the input (C29) as well.

    image

    2. That tiny ground trace on the capacitor is KILLING the supply. Everything should have a FAT connection to ground. The kind of connection that is tough to solder!

    3. You should not use traces for any of the switching signals! Everything should be a large copper pour. Even though you used larger traces, their inductance is a significant issue. For comparison, here is a partial shot of the board I made for the "How to make a noise-free SMPS" video:

    image

    In this case, I used a through-hole switcher IC (and this is a buck, not a boost--but the principles are the same.) Notice how the ONLY trace I used is for the feedback signal (which I don't think your fixed switchers have.)

    The massive Vout and GND pads at the top are the output filter capacitor. The Vout and SW at the bottom is the inductor. See how I drew massive copper pours for them?

    I would also encourage you to use large pours, NOT TRACES, throughout the distribution of your 5-volt rail.

    For example, here are the 3v3 and 5v rails in the Mega IIe's design:

    image

    (The empty space is GND, which I deleted for this picture.) Only in a few cases did I draw a trace from my fat pours to a chip.

    As a suggestion, I would have laid out the supplies something like this. (Don't copy this exactly. I just did it real quick.)

    image

    Since you have enough room, I would also suggest adding an extra capacitor footprint so you can add a second value.

    Last. I would encourage you to do two things if you're going to move forward with your own SMPS design.

    1) Make the SMPS as standalone boards first. You need to test them in isolation. You'll rarely get them right on the first try. Then you can replicate their design to the larger PCB.

    and the most important

    2)  Please, please, please, verify the operation of your switchers on an oscilloscope! Your DMM is lying to you!! Given how your PCB looks, I would NOT be surprised if your peak-to-peak noise was several volts, meaning you are hitting that poor CM4 with >10 volt transients! It's also possible your supply is oscillating from all of the inductance on the power distribution network (PDN).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • baldengineer
    baldengineer over 2 years ago

    You've embarked on an impressive project and made an incredible project.

    However. Regarding your power supply, I took a peek at your KiCad files—just a few critical issues I see right away.

    I am using this converter for an example (so I can use designators.)

    image

    1. For the ceramic output capacitor (C28), you should have a relatively large CV 0805 (imperial) MLCC. A large CV means the highest rated voltage at whatever capacitance you picked. An 0805 has much less DC-Bias effect than a 0603 and is available with higher rated voltages. Since you have the space, I would also use a 0805 on the input (C29) as well.

    image

    2. That tiny ground trace on the capacitor is KILLING the supply. Everything should have a FAT connection to ground. The kind of connection that is tough to solder!

    3. You should not use traces for any of the switching signals! Everything should be a large copper pour. Even though you used larger traces, their inductance is a significant issue. For comparison, here is a partial shot of the board I made for the "How to make a noise-free SMPS" video:

    image

    In this case, I used a through-hole switcher IC (and this is a buck, not a boost--but the principles are the same.) Notice how the ONLY trace I used is for the feedback signal (which I don't think your fixed switchers have.)

    The massive Vout and GND pads at the top are the output filter capacitor. The Vout and SW at the bottom is the inductor. See how I drew massive copper pours for them?

    I would also encourage you to use large pours, NOT TRACES, throughout the distribution of your 5-volt rail.

    For example, here are the 3v3 and 5v rails in the Mega IIe's design:

    image

    (The empty space is GND, which I deleted for this picture.) Only in a few cases did I draw a trace from my fat pours to a chip.

    As a suggestion, I would have laid out the supplies something like this. (Don't copy this exactly. I just did it real quick.)

    image

    Since you have enough room, I would also suggest adding an extra capacitor footprint so you can add a second value.

    Last. I would encourage you to do two things if you're going to move forward with your own SMPS design.

    1) Make the SMPS as standalone boards first. You need to test them in isolation. You'll rarely get them right on the first try. Then you can replicate their design to the larger PCB.

    and the most important

    2)  Please, please, please, verify the operation of your switchers on an oscilloscope! Your DMM is lying to you!! Given how your PCB looks, I would NOT be surprised if your peak-to-peak noise was several volts, meaning you are hitting that poor CM4 with >10 volt transients! It's also possible your supply is oscillating from all of the inductance on the power distribution network (PDN).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • baldengineer
    baldengineer over 2 years ago in reply to baldengineer

    Oh yeah, the inner and bottom layers should all be ground. And there should be more ground stitching vias than you can count.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to baldengineer

    Quote from an SMPS book I bought today:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to baldengineer

    Also, I meant to say,  "... you made incredible progress," but I wrote "project" twice.

    ¯\_(ツ)_/¯

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to Jan Cumps

    Hah!

    Every time I design an SMPS, I say to myself: "Next time, I'm just using a module."

    Some day I will learn.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 2 years ago in reply to baldengineer

    I was always wondering, why every SMPS has a recommended layout in the datasheet. Isn't this the HW designer's pride to layout on their own? From your Workbench Wednesdays videos I also learned it is not that easy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to baldengineer

    thanks for the info.
    how do you conncet the planes to a net? is it just a pour plane but with the specific net selcted for the pour? or is there a different tool for that job?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to mayermakes

    Copper Pour = Zone.

    Click on a copper layer and then use the Zone tool. When you start to draw it, you can select which net it connects to.

    You could also leave it as "no net" and draw it until you're happy.