Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Twilight Zone Fortune Telling Machine -- Episode 365
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 25 Oct 2018 4:25 PM Date Created
  • Last Updated Last Updated: 26 Oct 2018 7:24 AM
  • Views 9653 views
  • Likes 10 likes
  • Comments 26 comments

Twilight Zone Fortune Telling Machine -- Episode 365

image
Twilight Zone Fortune Telling Machine

element14 Presents  |  AirborneSurfer's VCP Profile |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Matt is a huge fan of the Twilight Zone, so for Halloween, he's decided to build a classic prop from the old series with a modern twist! The original Mystic Seer was a coin-operated fortune telling machine created for the 1960 episode "Nick of Time". Will this new, electronic fortune teller actually predict the future?

 

Supplemental Content:

 

Project: Serling [OUTTAKES] (and an Apple rant)

 

Adobe InDesign Files For Project Serling

 

Bash Shell Script For Project Serling

 

The Mystic Seer In Action

 

Bill of Material:

PartQuantityBuy Kit

Raspberry Pi 2 Model B v1.2 Quad Core CPU 1GB RAM 40 GPIO Pins HDMI Port

1Buy Now

Heat Sink Kit For Raspberry Pi

1Buy Now

Toggle Switch On-Off SPST Non Illuminated 10 A Panel Mount

1Buy Now

Mini Thermal Receipt Printer Starter Pack

1Buy Now

DC PLUG TO SCREW TERMINALS MALE 5.5X2.1MM 5PK

1Buy Now

DC JACK TO SCREW TERMINALS FEMALE 5.5X2.1MM 5PK

1Buy Now
AC/DC Power Supply ITE 1 Output 20 W 5 V 4 A 1Buy Now
LED Panel Mount Indicator Amber 12 V 12.7 mm 25 mA 13 cd 1Buy Now
  • mystic seer
  • e14presents_airbornesurfer
  • twilight zone mystic seer
  • raspberry pi fortune teller
  • raspberry pi
  • sharethescare
  • matt eargle
  • twilight zone
  • vcp
  • replica props
  • fortune teller
  • twilight zone props
  • friday_release
  • zoltar machine
  • electronic props
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • andywest
    andywest over 7 years ago in reply to airbornesurfer +3
    The ability to "scan for life forms".
  • mayermakes
    mayermakes over 7 years ago in reply to airbornesurfer +2
    Do the TIME FREEZING STOPWATCH!!
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to DAB +2
    giphy.com/.../iframe
Parents
  • realgeneralgrunt
    realgeneralgrunt over 7 years ago

    As someone who's been wanting to build my own original fortune telling machine, this is beyond helpful. I'm currently designing an original 3d printed figure head. In my build, I plan to use the arcade button press and thermal printer, however I want there to be animated leds and music that plays a little show before the printer prints the fortune. I have NO IDEA how i'm going to do the middle part though. I'm composing a twisted circus waltz and designing the artwork in the meantime. I had the idea of making it like a mix between the Seer and Zoltar from Big. If anyone has any input or ideas or would like to help me out, let me know! Awesome vid though I learned a lot!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to realgeneralgrunt

    Thanks, buddy--that's why we're here! Meanwhile, that sounds like an awesome idea on your end--I'll be stoked to see it (so be sure to ping me) when it's done!

     

    As for the middle part, that's not too terribly difficult to do from the GPIO pins on the Pi. You can write a little script in Python (which, even if you're "not a programmer", should be pretty easy to handle) that can blink the lights. To play the music, you'll need to get one of those USB sound cards and add the command to play the music to the aforementioned script. It wouldn't be too hard to add a couple of lines to my bash script that runs your Python code between the button press and the print.

     

    Check out these other videos to see more of what I'm talking about:

    LEDs from GPIO:

    Project TIROS

    Project Mooninite

     

    Hacking a USB sound card:

    Project TurtlePi

     

    Good luck, and if you need more help, check out the Raspberry Pi and Code Exchange spaces or just ask! Welcome to the Community!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to realgeneralgrunt

    Thanks, buddy--that's why we're here! Meanwhile, that sounds like an awesome idea on your end--I'll be stoked to see it (so be sure to ping me) when it's done!

     

    As for the middle part, that's not too terribly difficult to do from the GPIO pins on the Pi. You can write a little script in Python (which, even if you're "not a programmer", should be pretty easy to handle) that can blink the lights. To play the music, you'll need to get one of those USB sound cards and add the command to play the music to the aforementioned script. It wouldn't be too hard to add a couple of lines to my bash script that runs your Python code between the button press and the print.

     

    Check out these other videos to see more of what I'm talking about:

    LEDs from GPIO:

    Project TIROS

    Project Mooninite

     

    Hacking a USB sound card:

    Project TurtlePi

     

    Good luck, and if you need more help, check out the Raspberry Pi and Code Exchange spaces or just ask! Welcome to the Community!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • realgeneralgrunt
    realgeneralgrunt over 7 years ago in reply to airbornesurfer

    Thanks good sir! Glad you like the idea! I love the size and devil head aspect of the seer, while also the complexity and artistry of the Zoltar machine in Big  so I figure I'd combine the two into one demented chuck e cheese like arcade amusement. I ordered some LEDs with built in resistors, and I pretty much have all the parts I need. I DO have the space for a coin acceptor which I got a while back. I assume I can use that in place of the button to make it more authentic. I am not a programmer by any stretch, so I can use a lot of help on the coding end of things.

     

    image

     

    Heres the 3d printed head I created in Sculptris. My plan is to cut out the eyes and replace them with clear red spheres with the LEDS fed into them. I can't seem to find any red spheres only clear ones unfortunately.

     

    I have a lot of questions, would it be alright if I messaged you? Thanks for the kind words and support by the way, I've been wanting to build one of thee creepy ass things for a few years now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to realgeneralgrunt

    Looks delightfully demented! Drop me a line anytime, but be warned: I'm not always the fastest to respond (especially around deadline time) image

     

    Check out Episode 356: Bank to the Future with Arduino & TI for some info on using a coin acceptor as well!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • realgeneralgrunt
    realgeneralgrunt over 7 years ago in reply to airbornesurfer

    no worries man! I made a thread here with my progress/ greater detail as to what I'm using.

     

    Raspberry Pi, creepy Zoltar Like Fortune Teller help