Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Miniature Multimeter -- Episode 483
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Jan 2021 4:41 PM Date Created
  • Last Updated Last Updated: 29 Jan 2021 8:24 AM
  • Views 5229 views
  • Likes 14 likes
  • Comments 14 comments

DIY Miniature Multimeter -- Episode 483

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Breadboarding is often the start of great projects but measuring on Breadboards is often not so great. The standard multimeter leads don't fit into breadboard holes and alligator clips are needed to connect to the circuit. There must be a better way! Clem designs a tiny Multimeter dedicated to be used with a breadboard! Easy to connect, battery powered and it even has a WI-FI so you can view the readings on your phone!

 

Get the PCB here: https://aisler.net/p/BKDRSPYV

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
BAK Rechargeable Battery, 3.7 V, Lithium Polymer, 370 mAh, Connector BAK 1 Buy Now
MIDAS Graphic OLED, 96 x 16 Pixels, White on Black, 3V, I2C, 33mm x 10mm, -40 °C Midas 1 Buy Now
MCM Wire Kit, Jumper, Copper, 0.6 mm Diameter, 350 Piece MCM 1 Buy Now
FTDI Interface Analog Development Board LC234X, USB to UART Bridge FTDI 1 Buy Now
MICROCHIP Battery Charger for 1 Cell of Li-Ion, Li-Pol battery, 6V input, 4.2V / 500mA charge, SOT-23-5 Microchip 1 Buy Now
MICROCHIP Fixed LDO Voltage Regulator, 2.1V to 6V, 210mV Drop, 3.3V/500mA Out, SOT-223-3 Microchip 1 Buy Now
ESP32-S2-WROOM espressif 1 Buy Now
USB Connector, USB Type C, USB 3.1, Receptacle, 24 Ways, Surface Mount, Right Angle Molex 1 Buy Now
INA219 SOIC TI 1 Buy Now
0,1 Ohm current shunt resistor panasonic 1 Buy Now

 

Additional Parts:

 

Product Name
ESP32-S2-WROOM
Attachments:
MiniMultimeter_Resources.zip
element14 presents
DIY Miniature Multimeter

element14 Presents  |  About Clem  |  Project Videos

  • esp32
  • oled
  • molex
  • measure voltage arduino
  • make a multimeter
  • clem
  • mcm
  • ina219 arduino
  • homemade multimeter
  • battery charger
  • microchip
  • native usb esp32s2
  • esp32 project
  • esp32 multimeter
  • diy multimeter
  • e14presents_mayermakes
  • esp32-s2-wroom
  • breadboard
  • BAK
  • oled arduino
  • esp32-s2
  • rechargeable battery
  • multimeter
  • esp32s2
  • midas
  • friday_release
  • mayermakes
  • ftdi
  • e14p_CMM
  • simple esp32s2 i2c on esp32
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 5 years ago +4
    Here are some interesting question is want to adress: by user Cliff Matthews I don't know why the typical breadboard end-type PCB format wasn't chosen as the base PCB (you could put your 3D plastic contraption…
  • DAB
    DAB over 5 years ago +3
    Nice build Clem. The screen is way too small for someone like me, but sending the data to your phone or computer makes up for that problem. DAB
  • aspork42
    aspork42 over 5 years ago +3
    I love it! I see two different uses - "local" just as you have noted; and "Remote" where these are small enough to deploy out and about; perhaps around a larger machine like the power supply on a 3D printer…
  • kmikemoo
    kmikemoo over 5 years ago

    mayermakes  VERY cool.  Outside my current skill set, but awesome none the less.  Definitely bookmarked for visiting again later.

    On the MODE Resistance in the code, why ADC?  I don't understand why (ReadADC/10).  Wouldn't VR1 = [(Vin/1023) * ReadADC]?  I can understand the rest - although I did need to get out the paper and pen to dust the cobwebs from my brain.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago in reply to davedarko

    the display is primarly compatible with the library but i had to turn it 90 degrees in code and that changes the adressing it seems to wrap in the middle..sometimes but not on all commands.

    also 0,0 is not in a corner but off the screen

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davedarko
    davedarko over 5 years ago

    what's going on with the display? seems like half of it is garbled, the other half is split lines? Wrong library after all or not configured correctly?  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago

    Here are some interesting question is want to adress:
    by user Cliff Matthews

    I don't know why the typical breadboard end-type PCB format wasn't chosen as the base PCB (you could put your 3D plastic contraption around that..). Also, most everyone has a access to an old Android phone, so why u$e an OLED display when there's a much bigger one (with data logging) on the phone? Another thing, I see you chose a Lion battery and charger to isolate the INA219 and ESP from the hobbyist's various power scenario's, but open Lion cells are typically for portable power and pose their own safety risks... why not help the hobbyist by using a DC-DC converter instead for DMM isolation?

     

    shape:

         to make the premise more tangible I chose to make it look similar to my klein mutlimeter /typical multimeters

    android phone:

         It is compatible with any phone I showed in the video that you can access the measurements with any device on the same network. the section where i talk more about viewing on the phone ended up on the cutting      floor, as it was not core to the project.

    battery:

         I choose a lipo first to get myself familiar with designing charge circuits for them and secondly to make this device truly portable. a tiny multimeter will be handy in more situations than just on a breadboard.
         also it avoids power loops that might occur when hocking it up incorrectly. and it does not draw power from your project which might make the measurements unusable or give a fals impression of the projects power      requirements.

     

    Some things I like to improve are:

         Isolation, I like to use tiny isolation transformers to decouble the I2C and Measurment lines.
    The code needs alot of improvement in general

    I'd like to replace the screen with a more standard one that works better with the libraries.
    I'm searching for a better way to plug breadboard wires into the multimeter in a locking fashion, but hassle free... maybe wago terminals?

     

     

    let me know if you have any ideas!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<