Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Hot Plate for SMD Soldering Using Raspberry Pi Pico -- Episode 655
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 23 May 2024 6:32 PM Date Created
  • Last Updated Last Updated: 24 May 2024 9:49 AM
  • Views 14117 views
  • Likes 14 likes
  • Comments 8 comments

DIY Hot Plate for SMD Soldering Using Raspberry Pi Pico -- Episode 655

Does using a soldering iron or a hot air gun come to mind when you think of soldering with surface mount device (SMD) components? In this video Milos explores another way that printed circuit boards (PCBs) can be soldered. The answer? Using a hot plate. A hot plate can be bought as a module by itself, some people have even built their own out of an electric clothes iron (just do not use it for your shirt afterwards!). A hot plate is a great tool for soldering when you have a stencil for your PCB and you are using solder paste, but it can also be useful when you are trying to unsolder some kind of integrated circuit (IC) with many small pins. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Designing the Concept of the Hot Plate 

image 

Note: It is typical that a hot plate must connect to mains voltage, whether that is 110 volts or 220-250 volts. Make sure that if you intend on completing this project yourself, that you are either a sufficiently competent and qualified person to do so, or you are working with someone else that can supervise the project to ensure that it is completed safely. 

Controlling the solid-state relay (SSR) was Milos’ first task, deciding upon a solid-state relay, because it can be controlled with a pulse width modulation (PWM) signal unlike an ordinary relay. For measuring the temperature, he opted to use a negative temperature coefficient (NTC) thermistor, which is essentially a resistor which changes its resistance based on the temperature, allowing it to be read appropriately. 

 image

In the video, Milos introduces us to the fundamental principles of the NTC thermistor, how it reacts to temperature and how to calculate the temperature from the resistance as well as how to calculate the resistance from the ADC reading. If you are interested in more detail about the calculations, here is a great blog that you can learn from: 

 Blog #3: Characterising Thermistors – A Quick Primer, Beta Value & Steinhart-Hart Coefficients

For the project, the final schematic can appear rather simple, connecting all of the component as modules to the Raspberry Pi Pico, except in the case of the NTC thermistor that connects to a voltage divider with a 2k ohm resistor. 

image 

CAD Designing an Enclosure 

No project is complete without a presentable and a suitable enclosure. Milos’ decides to combine materials for convenience and an aesthetic. Choosing two types of material: wood and plastic. Since the hot plate can reach temperatures up to 300 degrees centigrade, the plastic can get too soft from temperatures of 60 degrees centigrade, up to melting at 160 degrees centigrade. Insulating the plastic would be a good choice, separating them as much as possible. To help with the design, Milos first secured the hot plate using standoffs (sized at 40mm) that are connected to wooden planks. These are then connected with 20mm standoffs to a top plywood plate. The plywood used is 4mm thick and can be cut by whichever method you prefer. This is the computer aided design (CAD) model of the whole device. 

image 

For an output display of the state of the hot plate, Milos opts for a simple 16x2 character liquid crystal display (LCD) which will show the intended set and measured temperatures, as well as the mode that the hot plate is currently in, whether it’s idle, heating up, or in an error state. To the right of the LCD goes the rotary encoder with a button that is used for setting the temperature as well as turning the heater on and off. On the side to the right of the enclosure, there is an external USB connector which is handy if you want to track the temperature plots on your computer while the hot plate is working, giving you the opportunity to tweak how it operates. To secure it together it uses M3 sized screws with the solid-state relay secured using M4 screws and nuts. 

 

{gallery}My Gallery Title
image

image

image

Programming the Software Controller 

Now to get the components working it needs to be told what to do, the code for the hot plate created by Milos provides the functionality needed to monitor and control the temperatures and heating. Milos wanted to make it as simple to use as possible to ensure that very little could go wrong, and it gives a great basis to build upon!  

As there are many variables which can affect the temperature of the hot plate, reading the temperature does not need to be incredibly accurate but it should be within a small margin of error. To regulate, a straightforward proportional-integral (PI) controller is employed, featuring supplementary elements like a ramp limiter for the temperature reference. Additionally, safeguards against overshooting and undershooting are integrated into the integral aspect of the controller. 

The output of the proportional-integral controller is the PWM duty cycle which was limited in software to 40% since the hotplate can get up to temperature incredibly quickly. Milos also implemented an automatic shut-down of the heater if the temperature doesn’t rise on the thermistor, while the controller is keeping an above zero duty cycle a set amount of time. This can happen when the thermistor gets somehow disconnected from the hot plate (or when the SSR or the hot plate itself are faulty). This prevents the PI controller from trying to heat up the hot plate perpetually, causing components to burn out or catch on fire.  

Have you moved on from soldering irons and heat guns? Do you repair your electronic devices with a heat plate to ensure an even distribution? Did you make your own hot plate or buy one, and what do you use? Let us know in the comments, or simply share your feelings on this episode. 

Download Files and Related Links

  • Download CAD Files and Code!
  •  Blog #3: Characterising Thermistors – A Quick Primer, Beta Value & Steinhart-Hart Coefficients 
  •  Mastering Oven Control: Precision Resin Curing with DIY Modifications - How Hard Can it Be? -- Episode 616  

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
MULTICOMP PRO MCKSI240D10-LM(070)Solid State Relay, 10 A, 280 VAC, Panel Mount, Screw, Zero Crossing MULTICOMP PRO 1 Buy Now
RASPBERRY-PI RASPBERRY PI PICO H RASPBERRY-PI 1 Buy Now
VISHAY 4N27 VISHAY 1 Buy Now
EATON BUSSMANN NRBG105F3950B1F EATON BUSSMANN 1 Buy Now
DFROBOT Expansion Board, Gravity I2C 16x2 Arduino LCD, DFRduino UNO R3 Board DFROBOT 1 Buy Now
DFROBOT Rotary Encoder Module, Breakout, Fermion, EC11, DFRduino UNO R3 Board DFROBOT 1 Buy Now
SCHURTER 6100.3100 SCHRUTER 1 Buy Now
MULTICOMP PRO MCMRA-1-KKFTCRocker Switch, On-None-Off, SPST, Non Illuminated, Panel Mount, Black MULTICOMP PRO 1 Buy Now
 

Additional Parts:

Passive components like wires, perfboard, resistors
M3 and M4 screws for holding everything together
4mm plywood sheet
PLA or PET-G for printing the enclosure
  • DIY reflow soldering
  • Raspberry Pi Pico project
  • hot plate temperature control
  • hot plate for PCB assembly
  • e14p_Milos
  • PCB soldering tutorial
  • DIY reflow oven alternative
  • soldering safety tips
  • custom soldering station build
  • negative thermal coefficient thermistor
  • DIY hot plate soldering
  • PCB soldering techniques
  • friday_release
  • DIY electronics projects
  • Raspberry Pi soldering project
  • how to solder with a hot plate
  • homemade soldering station
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • guillaume9433
    guillaume9433 over 2 years ago

    Hi, great job!

    however in the video, at 4.50min, at the line of code: meassure_resistance, you enter 4086,
    I think this corresponds to the maximum value of the ADC, shouldn't it be 4096? In the source files there is the same "error". But 4086 instead of 4096 doesn't change much to the final result. where do you buy the hot plate, and for soldering paste, how much should you heat the plate?

    very nice achievement in the end.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • guillaume9433
    guillaume9433 over 2 years ago

    Hi, great job!

    however in the video, at 4.50min, at the line of code: meassure_resistance, you enter 4086,
    I think this corresponds to the maximum value of the ADC, shouldn't it be 4096? In the source files there is the same "error". But 4086 instead of 4096 doesn't change much to the final result. where do you buy the hot plate, and for soldering paste, how much should you heat the plate?

    very nice achievement in the end.