Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Designing a Smarter Workbench: Inside Mark’s 8-Channel Power Monitoring System
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: cstanton
  • Date Created: 1 Jul 2026 3:54 PM Date Created
  • Last Updated Last Updated: 2 Jul 2026 10:46 AM
  • Views 13305 views
  • Likes 6 likes
  • Comments 5 comments

Designing a Smarter Workbench: Inside Mark’s 8-Channel Power Monitoring System

Mark set out to simplify a cluttered workbench full of power adapters by designing a smart 8-channel power distribution and monitoring system built around an ESP32, giving him full control over each output while tracking voltage, current, energy use and even running costs in real time. As he explains, “there must be a better way,” and the result is a custom PCB with integrated current sensing, programmable protection, and an intuitive rotary-driven interface that can automatically shut down channels on overcurrent to protect connected devices. From careful PCB assembly and thermal management to firmware that stores settings and energy data in non-volatile memory, the project highlights both practical challenges and thoughtful engineering decisions, all wrapped up in a compact, 3D-printed enclosure designed for everyday use on the bench.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

As laboratories and desktop workspaces become increasingly complex, so does the demand for reliable, intelligent power distribution. Mark’s custom-built "PowerMon 8" takes a practical problem, too many devices, too many adapters, and transforms it into a tightly integrated system that combines control, monitoring, and protection in a single unit.

“So I decided there must be a better way… not only does it distribute power… it also includes an energy monitor.”

This project goes beyond a simple power strip. It introduces real-time analytics, independent channel control, and programmable safeguards, all driven by an ESP32-based embedded system and supported by a purpose-built PCB.

image

From Clutter to Control: The Motivation Behind PowerMon 8

A scenario that is familiar to many: a workstation crowded with power-hungry devices, each requiring its own adapter and outlet. Maybe they're not all USB-C yet, maybe they're USB-A, perhaps some are still barrel jack. Regardless, you have a lot of power requirements, and so does Mark. Mark’s design consolidates this into a single distribution unit capable of powering and managing eight outputs independently. 

Rather than simply routing power, the device actively monitors consumption and provides feedback, allowing users to understand both instantaneous usage and long-term cost implications.

“I have an office with a whole load of outlet sockets… and each socket is occupied with one of these annoying power adapters.”

image

System Architecture and Hardware Design

At the core of the system is an ESP32 microcontroller, chosen for its versatility and ability to manage multiple inputs, outputs, and communication tasks simultaneously. The hardware is divided into several key functional blocks:

  • Eight independent output channels
  • Dedicated current sensing per channel
  • Switchable outputs via MOSFET stages
  • Dual power regulation (fixed 5V and adjustable rail)
  • User interface via rotary encoder and OLED display

Each output channel is effectively identical, simplifying both PCB design and firmware logic.

“It’s eight of them and they’re all the same… we have our energy monitor… outputs that can be enabled or disabled.”

The bill of materials listed out at the end of this blog reflects careful component selection, including:

  • INA219 current sensors for precise per-channel monitoring
  • Onsemi MOSFETs (FDN340P / FDN335N) for efficient switching
  • LM1084 adjustable regulator for configurable output voltage
  • Precision resistors and capacitors supporting stable measurements

This combination ensures accuracy in measurement while maintaining robustness under varying load conditions.

image

Power Stage and Thermal Considerations

Power handling is a critical aspect of the design. With multiple channels potentially drawing current simultaneously, thermal management becomes essential.

Mark addressed this by designing a custom heatsink solution tailored to the PCB layout.

“I designed my own heat sink… it all depends on how much power you’re going to export.”

Rather than using conventional mounting, thermal adhesive is used to secure the heatsink:

“There is a difference between this one and actual thermal paste… this one does [stick].”

This decision simplifies assembly while still providing effective thermal coupling. However, it introduces a constraint: sufficient curing time is required before applying load.

image

Assembly Challenges and Practical Considerations

Although many surface-mount components were pre-installed, assembly still required careful handling, particularly for fine-pitch soldering.

“That’s why I use a microscope… I instantly see it and I can correct it.”

LED alignment also proved important due to the enclosure design, requiring incremental soldering and verification:

  • Initial single-pin soldering for adjustment
  • Mechanical alignment checks with enclosure lid
  • Final soldering once positioning was confirmed

These steps highlight a recurring theme: mechanical and electrical design must be considered together, especially in compact builds.

image

User Interface and Interaction Design

The system’s interface is deliberately minimal, relying on a single rotary encoder for navigation and configuration. Despite this simplicity, it enables full control over:

  • Channel switching
  • Current limit configuration
  • Energy pricing
  • System monitoring
“Rotate to navigate… press to confirm… depending on what layer in the menu we are in.”

Visual feedback is provided through both an OLED display and LED indicators, with clear colour coding for channel states:

  • Green – active
  • Blue – disabled
  • Red – tripped
“If it’s triggered… it will be rather orange… and I manually have to enable it again.”

image

Firmware: Monitoring, Protection and Control

The firmware ties the entire system together, managing inputs, measurements, and output control in real time. The structure follows a typical embedded pattern:

  • Initialisation in setup()
  • Event-driven loop for interaction
  • Periodic safety checks for protection

A key feature is continuous monitoring of current across all channels, with automatic shutoff when limits are exceeded.

“Whenever that current is exceeded… the output will be disabled immediately.”

A simplified representation of this logic appears in the code:


// Periodic overcurrent check (conceptual)
if (measuredCurrent[channel] > maxCurrent[channel]) {
    disableOutput(channel);
    setChannelState(channel, TRIPPED);
}

The firmware also maintains persistent state using non-volatile memory, ensuring that configuration and energy data survive power cycles.

“We retrieve some parameters from the non-volatile memory… channels that were on or off last time.”

Energy Monitoring and Cost Analysis of Real-World Behaviour and Safety Features

Beyond protection, PowerMon 8 delivers detailed energy insights. Each channel tracks:

  • Voltage
  • Current
  • Power consumption
  • Total energy usage
  • Calculated cost
“I used 0.02 kilowatt hours… which is equal to 1 euro… because I set the unit price very high.”

This enables meaningful evaluation of device efficiency and long-term operational costs, particularly useful for development and testing environments. In practice, the system behaves intelligently under fault conditions. When a current limit is exceeded:

  • Output is immediately disabled
  • Status changes to indicate a fault
  • User must manually reset the channel
“The minute I set the current limit lower… it will detect and it will switch off.”

This manual reset requirement ensures that faults are acknowledged rather than silently ignored.

image

Enclosure Design, Future Improvements and Expansion Possibilities

A custom 3D-printed enclosure brings the project together, ensuring:

  • Secure PCB mounting
  • Correct LED alignment
  • Accessible controls
  • Thermal clearance

The integration of mechanical, thermal, and electrical elements demonstrates a complete product-oriented approach rather than a simple prototype. While already feature-rich, the design naturally opens the door to further enhancements:

  • Remote monitoring via Wi-Fi (leveraging ESP32 capabilities)
  • Data export or logging to external systems
  • Automated channel scheduling
  • Integration with test automation frameworks

Mark encourages modification and iteration, highlighting the project’s adaptability.

“If you’re going to change something please let me know… I’m very curious on what you’re going to change.”

PowerMon 8 aims to be more than an exercise in PCB design, it is a practical tool that addresses everyone's messy workbench. By combining power distribution, monitoring, and protection into a cohesive system, Mark has created something that fits naturally into any serious workspace, and maybe, the non-serious ones too. Give it a go.

Supporting Links and Files

-  Episode 721 Resources - Designing a Smarter Workbench: Inside Mark’s 8-Channel Power Monitoring System  

- ESP32 Library

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
CL31A106KBHNNNE SAMSUNG 8 Buy Now
16PK330MEFC6.3X11 Rubycon 2 Buy Now
C0603C104K3RACTU Yageo 13 Buy Now
TAJB107K006RNJ Kyocera AVX 2 Buy Now
TAJA106K016RNJ Kyocera AVX 1 Buy Now
CC0805KRX7R9BB104 Yageo 4 Buy Now
ES5JB Shandong Jingdao Microelectronics 1 Buy Now
L-934LID Kingbright 8 Buy Now
FDN340P Onsemi 8 Buy Now
FDN335N Onsemi 8 Buy Now
LR2512-22R050F4 TT Electronics 8 Buy Now
MCHP05W4F1200T5E MULTICOMP PRO 1 Buy Now
ERA6ARB103V Panasonic 16 Buy Now
3314J-1-102E BOURNS 1 Buy Now
0805W8F1001T5E Panasonic 8 Buy Now
MC0805S8F4701T5E MULTICOMP PRO 2 Buy Now
MCHP05W4F1501T5E MULTICOMP PRO 3 Buy Now
MC0805S8F5101T5E MULTICOMP PRO 3 Buy Now
MCWR08X3301FTL MULTICOMP PRO 2 Buy Now
MCTF0805BTC1002 MULTICOMP PRO 2 Buy Now
EC11E09244AQ ALPSALPINE 1 Buy Now
LM1084IS-ADJ-TP TECH PUBLIC 1 Buy Now
KLDX-0202-A Kycon 9 Buy Now
INA219AIDR TI 8 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
ESP32 Doit Devkit 1
Display SSD1351 OLEd color
PCB
AMS1084CM-5.0 or lm1084/lm1085 AMS 1

  • yageo
  • samsung
  • power consumption tracking
  • Energy Monitoring System
  • e14presents_mdonners
  • Maker Electronics Tutorial
  • esp32 power monitor
  • power control system
  • electronics workbench upgrade
  • diy electronics build
  • kyocera avx
  • rubycon
  • current sensing ina219
  • energy cost monitoring
  • multi channel power supply
  • rotary encoder interface
  • smart power distribution
  • embedded systems project
  • custom PCB project
  • overcurrent protection circuit
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
  • Attila Tőkés
    Attila Tőkés 4 months ago

    Nice project, donnersm ! Clap

    It happens that I'm in the process of building a 12V distribution board quite similar to yours.

    Mine is aimed more for routers / modems / switches / SBC-s, has 4 output channels, and is based on the W55RP20-EVB-Pico (for LAN connectivity).

    image
    It also has current sensing (slightly different architecture than yours) and dual power input for redundancy.

    Currently, I'm waiting for the PCB and components to arrive. Once the board is assembled and tested, I will post a detailed project description here at E14.

    Until then, more details here: https://maker.wiznet.io/attitokes/contest/smart%2Dups%2Dmonitor%2Dhome%2Dlab%2Dpower%2Ddistribution%2Dboard/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • donnersm
    donnersm 4 months ago

    IF anyone needs the step file or have the 3d housing in a different file format...right click on the parts in the lower left to export, using this read and export only link
    https://cad.onshape.com/documents/d45ffa528a9e779c59ce97db/w/8aef10a4f96da7f8cc9b7566/e/b34cd258bd513b36bc292a4b?renderMode=0&uiState=6a47b56d31edf2f9d58e5027

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Qbit
    Qbit 4 months ago

    Great project, Mark! An 8-channel power monitoring system is exactly what a smart workbench needs—especially when you're juggling multiple prototypes and want to track real-time power consumption across different devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 4 months ago

    Nice useful build.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • donnersm
    donnersm 4 months ago

    If you have any questions, feel free to ask. I'll do my best to answer all.