Products
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
WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum Microcontroller Dev Boards: What features do you like to have (or to add?)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 114 subscribers
  • Views 8076 views
  • Users 0 members are here
  • pcb
  • microcontroller
  • arduino
  • pi pico
Related

Microcontroller Dev Boards: What features do you like to have (or to add?)

baldengineer
baldengineer over 3 years ago

image

A couple of weeks ago, I bribed shabaz (with coffee) to send me one of his Pi PIco Eurocards. As the name implies, these are a development board for the Pi Pico / RP2040. In the past, another friend sent me one of his all-in-one microcontroller development boards (pictured above). And I have designed a few boards that had development features on them. Besides those, boards like Adafruit's Feathers or even the iconic Arduino Uno could be considered dev boards. Last, historically, microcontroller manufacturers had elaborate evaluation platforms for their chips.

All of these points made me wonder: what are the features YOU want to see in a microcontroller development board?

image

If we use shabaz's Eurocard, some notable features are:

  • Headers for changing power source (external / Pi Pico / Programmer)
  • Integrated programmer/debugger (RP2040-based Xiao, in this case)
  • Prototype areas for through-hole and surface mount parts
  • SD Card
  • Button
  • LED
  • (and many more)

In addition to features, what tricks or tips have people learned when making a board like this one?

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +8
    I just want to point out one feature, which is really nicely done on both of those boards. The markings of connectors and everything else in silkscreen. Pin numbers or signal labels in readable size, also…
  • michaelkellett
    michaelkellett over 3 years ago +7
    Keep it simple. Power supply input, on board regulator and clock. Break out every pin. Serial port, debug programming port. 0.1" headers are good and cheap but sometimesd take up too much room…
  • mayermakes
    mayermakes over 3 years ago +6
    i don't really have requests in stuff that should be on the board, I prefer to have zero clutter or parts that I don't really use in the project present to avoid conflicts and confusion on my part. also…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    Keep it simple.

    Power supply input, on board regulator and clock.

    Break out every pin.

    Serial port, debug programming port.

    0.1" headers are good and cheap but sometimesd take up too much room.

    Some mounting holes so the board can be fixed to box or other boards.

    I've been using my little display board as a general purpose micro board recently (where others might use a Pico or an Arduino).

    image

    The display board is the one in the vice. It doesn't have much more than the absolute basics (it has power siwtches for the displays and a possible back light.) The serial interface doesn't use an RS232 drive chip but works at logic level.

    The thing it's connected to is a multiplexer and DC bias injector for an LCR meter. (I'll blog about it when it's working a bit more.)

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago

    Keep it simple.

    Power supply input, on board regulator and clock.

    Break out every pin.

    Serial port, debug programming port.

    0.1" headers are good and cheap but sometimesd take up too much room.

    Some mounting holes so the board can be fixed to box or other boards.

    I've been using my little display board as a general purpose micro board recently (where others might use a Pico or an Arduino).

    image

    The display board is the one in the vice. It doesn't have much more than the absolute basics (it has power siwtches for the displays and a possible back light.) The serial interface doesn't use an RS232 drive chip but works at logic level.

    The thing it's connected to is a multiplexer and DC bias injector for an LCR meter. (I'll blog about it when it's working a bit more.)

    MK

    • Cancel
    • Vote Up +7 Vote Down