WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
WBW Episodes Capacitor Replacement on a Commodore 64 - A Lesson in Through-Hole Soldering -- Workbench Wednesdays 04
  • Episodes
  • Blog
  • Forum
  • Quiz
  • Files
  • Members
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Matt
  • Date Created: 19 Dec 2018 3:40 AM Date Created
  • Last Updated Last Updated: 13 Mar 2019 8:24 AM
  • Views 2951 views
  • Likes 6 likes
  • Comments 2 comments
Related
Recommended

Capacitor Replacement on a Commodore 64 - A Lesson in Through-Hole Soldering -- Workbench Wednesdays 04

image
Capacitor Replacement on a Commodore 64 - A Lesson in Through-Hole Soldering

WorkBench Wednesdays |  Bald Engineer: James Lewis' VCP Profile |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Need to rework through-hole components? Check out this Weller WX-Series soldering gear. It includes a 120 Watt de-soldering iron (WXDP120), 65 Watt (WXP65) iron, and a larger 120 Watt (WXP120) iron. James re-caps a Commodore 64 with the help of this WXR3 soldering system. It takes no time to remove components like capacitors and swap them in with modern replacements. As a bonus, he ends the video by re-working a Raspberry Pi to have a socket header instead of pins!

WX3 Pump On/Off Delay

In the video, James mentions the WXR3 has a user-configurable pump delay-off and delay-on time setting. His suggestion was to automate the desoldering process. An additional reason for the pump-on delay is to prevent clogging the WXDP 120. A delay-off time of a few seconds ensures that all of the molten solder is sucked into the glass tube before the pump shuts off. Without the delay-off, solder could become trapped in the tool leading to a clogged condition.

 

 

Supplemental Material:

 

  • Picking aluminum polymer electrolytic capacitors for the C64

 

Bill of Material:

 

Part
Weller Soldering Tools

WXR3001N Station Bundle (WXR3, WXP65, WXDP120, etc.)

Weller1Buy NowBuy Now

WXR3 Base Station

Weller1Buy NowBuy Now
WXP65 - 65W IronWeller1Buy NowBuy Now
WXP120WXP120 - 120W IronWeller1Buy NowBuy Now
WXDP120 - 120W De-Soldering ToolWeller1Buy NowBuy Now
ZERO SMOG EL FilterWeller1Buy NowBuy Now
Soldering Supplies
De-Soldering Wick 484-2 (0.05")American Beauty1Buy NowBuy Now
No Clean Flux PenKester1Buy NowBuy Now
SnPb Solder 0.02" Rosen Core (SPC22130)Duratool1Buy NowBuy Now
IPA Wipes (8421-WX25)MG Chemicals1Buy NowBuy Now
Other Tools Used
Handheld DMM (72-7780)Tenma1Buy NowBuy Now
PCB HolderPanavise1Buy NowBuy Now
5 Piece Plier Set (1PK-5015)Duratool1Buy NowBuy Now
4 Piece ABS Magnetic Storage Trays (D03162)Duratool1Buy NowBuy Now
Components
GPIO Socket Strip [SSW-120-01-F-D]Samtec1Buy NowBuy Now
Raspberry Pi 3 B+Raspberry-Pi1Buy NowBuy Now
C64 Capacitors - Partial List
100nF Radial Ceramic Replacements (Decoupling) [K104K15X7RF5TH5]Vishay50Buy NowBuy Now
10uF 25V Polymer Electorlytics (Decoupling) [A758BG106M1EAAE070]KEMET25Buy NowBuy Now
Bulk Capacitor #1 (16V) [A750MS477M1EAAE015]KEMET1Buy NowBuy Now
Bulk Capacitor #2 (12V) [A750MS477M1EAAE015]KEMET1Buy NowBuy Now
Bulk Capacitor #3 (5V) [RNL1C222MDS1]Nichicon1Buy NowBuy Now
Bulk Capacitor #4 [A750EK107M1CAAE018]KEMET1Buy NowBuy Now

 

 

Additional Parts:

 

Product Name

Thermal Paste

  • weller
  • e14presents_baldengineer
  • wxr3
  • wxdp120
  • workbenchwednesday
  • desoldering
  • soldering
  • wxp120
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 7 years ago +4
    Concerns about bending the polymer's leads came up in the YouTube comments. Here's a detailed response with pictures. by spreading the capacitor leads wide like that will stress the rubber seal and it…
  • DAB
    DAB over 7 years ago +2
    Using the right tool always makes the job easier. You did a good job pointing out the maintenance issues with de-soldering tools. This issues is often over looked and can cause many problems. Tool maintenance…
  • baldengineer
    baldengineer over 7 years ago

    Concerns about bending the polymer's leads came up in the YouTube comments. Here's a detailed response with pictures.

    by spreading the capacitor leads wide like that will stress the rubber seal and it will leak years sooner than a buying a proper axial capacitor that fits there.

    The capacitors used are polymer aluminum. These are a solid device with no electrolyte (or other liquid) to leak out.

     

    Here is the construction diagram for the A750, one of the capacitors used.

     

    image

    It even goes to the extent to make sure users realize the polymer layer is solid, not liquid. If you open the KEMET A750 family datasheet in Acrobat, there is also a 3D model on the first page. I did make a mistake in my original YT reply when I said there was no seal. In fact, polymers DO use a rubber seal, but for the opposite reason, that traditional wet-electrolytics do. With a conventional electrolytic, the goal is to keep moisture inside of the can while still allowing hydrogen gas that builds up from the dielectric regrowing, to escape. In the case of aluminum polymers, the seal is there to keep moisture OUT. The polymer material is PEDOT which is hygroscopic. When it comes in contact with moisture, it oxidizes. That oxidation increases the polymer layer's ESR (and affects the lifetime of the capacitor.)

     

    Second did you compare the ripple current specifications of the old caps?

    The ESR of the new caps are orders of magnitude less than traditional electrolytics. Which means, they have orders of magnitude more ripple current carrying capability. The polymer aluminum capacitors here have ESRs in the range of 18 milliohms. In terms of rated ripple current, the A750 polymer can handle 3 Amps, while a modern traditional wet-style of the same CV only has a ripple capability of 85 mA! Absolutely no reason for concern there.

     

    I've used them before, and polymer caps are wrapped just like a regular electrolytic cap.

    Canned capacitors are wound, not wrapped. image

     

    But if they have a solid core then they are surrounded with a electrolytic liquid.

    That is incorrect. There are two types of polymer aluminum cans. Solid and Hybrid. The most popular are solid. (Hybrid is only available from one vendor.) In solid polymer aluminum can caps, there is no liquid.

    The hybrid varient does, however, include both the polymer and an electrolyte. That construction allows more of the dielectric layer to come in contact with the cathode foil through the added electrolyte, which increases effective capacitance. The additional ions available on the electrolyte also allow for the dielectric to re-grown when exposed to higher voltages. However, hybrids have a cost premium over solids.

     

    Only ceramic caps are a solid material without an electrolytic liquid.

    Again, this is incorrect. I've already pointed out multiple times that polymer aluminum cans are solid. Additionally, tantalum-MnO2, tantalum-polymer, niobium-MnO2, niobium-polymer, film (PEN, PET, PPS, PP), and aluminum polymer chip capacitors are all solid capacitors with no electrolyte. (There are, however, variants which may include one. For example, tantalum slugs in a rhobidum-based electrolyte for high-temperature applications.)

     

     

    What caps did you use, I would like to look them up.

    They are included in the show notes, which was available in the description link (and the table above.) Additionally, I strongly recommend watching my video The Learning Circuit 40: Learning About Polymer Capacitors. You might also find these articles I wrote in my previous career helpful.

     

    1. How can material selection improve capacitor reliability.

    2. Self-healing capacitors can fix themselves.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    Using the right tool always makes the job easier.

     

    You did a good job pointing out the maintenance issues with de-soldering tools. This issues is often over looked and can cause many problems. Tool maintenance is important, do it after every use.

     

    DAB