WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Digilent Analog Discovery 2 Review -- Workbench Wednesdays 18
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Matt
  • Date Created: 11 Dec 2019 12:54 AM Date Created
  • Last Updated Last Updated: 18 Dec 2019 8:24 AM
  • Views 6606 views
  • Likes 7 likes
  • Comments 9 comments
Related
Recommended

Digilent Analog Discovery 2 Review -- Workbench Wednesdays 18

image
Digilent Analog Discovery Review

element14 Presents  |  Bald Engineer: James Lewis' VCP Profile |  Workbench Wednesdays

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Analog Discovery 2 combines all the equipment found on a typical electronics workbench into one small package. It packs an oscilloscope, logic analyzer, power supplies, spectrum analyzer, and so much more. As impressive as the hardware is, the Analog Discovery 2’s software, called Waveforms, is fantastic as well. You can configure it for any measurement situation, and it has extensive scripting capability. See if you should be considering adding the Analog Discovery 2 to your electronics workbench. If you there are measurement tools you want to know more about, follow the link to the full series on Workbench Wednesday’s Instrument Basics.

 

The Analog Discovery 2 combines all the equipment found on a typical electronics workbench into one small package. It packs an oscilloscope, logic analyzer, power supplies, spectrum analyzer, and so much more. As impressive as the hardware is, the Analog Discovery 2’s software, called Waveforms, is fantastic as well! You can configure it for any measurement situation, and it has extensive scripting capability. If you there are measurement tools you want to know more about, check out the links below from the full series on Workbench Wednesday’s Instrument Basics.

 

Supplemental Content:

 

  • Expanding your Test and Measurement Workbench Beyond the Lab with the Analog Discovery 2
  • New Product Release - Analog Discovery 2 Pro Bundle
  • Analog Discovery 2 + LabView Home Bundle - Review by iamashwin99
  • Analog Discovery 2 + LabView Home Bundle - Review by s2000gt
  • Analog Discovery 2 + LabView Home Bundle - Review by jpnbino
  • Analog Discovery 2 + LabView Home Bundle - Review by jdlui
  • Analog Discovery 2 + LabView Home Bundle - Review by rusgray
  • Analog Discovery 2 is now Compatible with Raspberry Pi 4

 

Bill of Material:

 

Product NameManufacturerQuantityBuy KitBuy Kit
[Base] Analog Discovery 2 USB Oscilloscope, 2 Analogue, 30 MHz, 100 MSPSDigilent1Buy NowBuy Now
[Bundle] Development Kit, Analog Discovery 2 Pro Bundle, 30MHz Oscilloscope, 12MHz Waveform GeneratorDigilent1Buy NowBuy Now
Add-On Board, Impedance Analyzer For Analog Discovery, 2-Wire InterfaceDigilent1Buy NowBuy Now
ADAPTOR BOARD, BNC, ANALOG DISCOVERYDigilent1Buy NowBuy Now
  • fpga based measurements
  • e14presents_baldengineer
  • usb scope
  • workbench wednesday
  • digilent
  • all-in-one measurements
  • analog discovery 2
  • usb measurements
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 6 years ago in reply to scottsto +3
    Hi scottsto , interesting question. As my main electronics hobby, I also repair old consoles and computers. That said, I haven't used my Analog Discovery 2 yet for those repairs. However, I am working…
  • koudelad
    koudelad over 6 years ago +2
    Thanks for putting a spotlight on this tool, James. I love my Analog Discovery 2! I have used it many times for debugging I2C communication (I haven't used the scripting possibility, neither). When evaluating…
  • jpnbino
    jpnbino over 6 years ago in reply to koudelad +2
    I haven't used the scripting possibility Hi David, I have used it. You can dowload the attached script on my RoadTest ( the link is in the suplemental content section in this page).
  • baldengineer
    baldengineer over 6 years ago in reply to scottsto

    Hi scottsto, interesting question. As my main electronics hobby, I also repair old consoles and computers. That said, I haven't used my Analog Discovery 2 yet for those repairs. However, I am working on a ZX81-related problem and just designed some PCBs to act as interposers to the Z80 and ULA, so I could connect a Logic Analyzer. (I was thinking of the digital channels on my oscilloscope at the time, but now I'm thinking about AD2 because I really do like the Waveforms software.)

     

    That said, the documentation for the AD2 says it is compatible with 1.8-3.3 LVCMOS and 5V tolerant. Which means, the logic level is probably set around 1.17 volts, which is the lowest level for 1.8V logic. 1.17 is well below TTL's 2.0 volt level and well above the 0.4 volt for input-low. For reference, here is a chart from this TI application note on Logic Families.

    image

     

    In reality, I have rarely run into digital systems that were so marginal that they relied on the limits of the logic families. So I think the AD2 should be fine in logic mode. The nice thing about such a device is that if you suspect a digtial line is giving you problems, it is a quick re-connection to see the analog behavior.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottsto
    scottsto over 6 years ago

    In the video it is said that it is for 3.3v CMOS but is 5v tolerant. I mostly work on older electronics which are 5v TTL or 5v CMOS. (For example old video game console or pinball PCBs.) Is this logic analyser still a good choice? Are there any problems when using it on 5v devices? My ancient HP Agilent Keysight died, and I want to get something light, new and modern.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jpnbino
    jpnbino over 6 years ago in reply to koudelad
    I haven't used the scripting possibility

    Hi David,

     

    I have used it. You can dowload the attached script on my RoadTest ( the link is in the suplemental content section in this page).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 6 years ago

    Thanks for putting a spotlight on this tool, James. I love my Analog Discovery 2!

     

    I have used it many times for debugging I2C communication (I haven't used the scripting possibility, neither). When evaluating a new I2C sensor, I connect it to the AD2, use the internal power supply and run a protocol analyzer on data and clock pins. Quick and easy. Also the GUI on a PC is much more responsive than doing the same using knobs and buttons on a traditional oscilloscope.

     

    I wish I had something like this when I was a student.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    Good test report.

     

    I had looked at the device, but decided not to buy it.

     

    If I need a simple system like this in the future, I will reconsider.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • celcius1
    celcius1 over 6 years ago in reply to baldengineer

    Actually baldengineer I would love to do this but I dont have over $400 (Australian) to spend on the pro kit, otherwise I would happily order a kit and design and print an all in one case, not to mention I'm after an oscilloscope kit, as i'm currently designing a Multi Zone Amp Board for Volumio as in my Day job I do Multi Zone Audio systems for some of my clients and having to use a RPi per zone and Hi-fi HAT is annoying, My normal Job I do is I design and deploy, Security, Communication and AV systems for clients in the Domestic and Commercial sectors, but work volumes are low at the moment so unfortunately income has been tight.

     

    I could already envisage a design, using a 5V 3A Mean well supply in the case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 6 years ago

    From YouTube, Mohammad wrote:

    Very useful instrument. I worked on a CAN bus for Automotives and needed to demonstrate the voltage quality as well as the digital messages on both CANL and CANH signals. Our Keysight oscilloscopes needed a differential probe to show both CANL and CANH. My Analog Discovery (AD )was able to show both signals on the 2 scope channels as well as the CAN messages on the logic analyzer

    The differential analog inputs are something I very much glossed over in the video. Typically oscilloscopes are ground-referenced. As Mohammad mentions, this might mean you need to use a differential probe for some measurements. For example, if a signal-under-test itself is differential like for his CAN bus. Another case is measuring the voltage across a component like a resistor or a transistor. With a traditional passive probe or oscilloscope input, one side of the measurement would need to be grounded.

     

    However, with differential input, no such reference is needed. Care does need to be taken to make sure the common-mode voltage is still within the measurement capability. So, for example, if you measured a current sense resistor on the high-side of a +12 volt rail, you have about 12 volts of common-mode in that measurement even though the difference (or differential) would probably be on the order of 100 millivolts or so.

     

    In the case of the Analog Discovery 2, it appears the differential inputs can handle up to 50 volts of common mode. Maybe it is 100 volts? I'm not sure how to interpret the specifications. To be safe, I would recommend less than 50 volts. How do you know how much common-mode a signal has? One quick method is to measure each side of the desired component referenced to ground. In other words, measure point-A to ground and point-B to ground. Add the two voltages together and then divide by two.

     

    Long story short, I should have made a bigger point about what "differential inputs" mean. Maybe single-ended vs differential measuerments is somethign we can cover in the future.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 6 years ago in reply to celcius1

    Interesting Idea celcius1. It would make a portable all-in-one bench.

     

    Hmmm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • celcius1
    celcius1 over 6 years ago

    Due to ease of taking it apart, its hard to resist taking it out of its shell and making a custom all in one case with RPi 4 and Touchscreen