Acoustics
  • Challenges & Projects
  • Project14
  • Acoustics
  • More
  • Cancel
Acoustics
Documents Project14 | Acoustics: Build Projects that Involve Infrasound, Audible Sound, Ultrasound, Amplifiers, and More!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Acoustics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Jan 2020 6:24 PM Date Created
  • Last Updated Last Updated: 29 Jan 2020 10:37 PM
  • Views 13570 views
  • Likes 16 likes
  • Comments 39 comments
Related
Recommended

Project14 | Acoustics: Build Projects that Involve Infrasound, Audible Sound, Ultrasound, Amplifiers, and More!

image

Acoustics

Enter Your Electronics & Design Project for a chance to win an $200 Shopping cart of product!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

In the Comments Below Let Us Know Your Ideas for Projects Around Acoustics!

 

The theme this month is Acoustics and it comes from an idea from neuromodulator.  This competition is an opportunity to do projects around sound and can involve projects that involve infrasound, audible sound, ultrasound, amplifiers, piezoelectric material, spectrum analyzers, and more!  Acoustics (from the Greek word akoustos which means "heard") is the science of how sound is produced, transmitted, controlled, and the effects of sound. Acoustics play a huge role in music, especially when it comes to musical scales and instruments.  Concert halls and auditoriums take into account the relationship between space and the listener with a good acoustic design taking into account issues such as reverberation time; sound absorption of finished material; echoes; acoustic shadows; sound intimacy, texture, and blend; as well as external noise.  Architectural modifications can be made to improve sound such as adding orchestral shells, canopies, and undulating or angled ceilings and walls. image

 

Your project can be anything involving sound or using a transducer for converting one form of energy into another. In an electroacoustic context, a transducer converts sound energy into electrical energy (or vice versa). Your project can involve electroacoustic transducers that convert a sound wave to some form of electric signal such as loudspeakers, microphones, particle velocity sensors, hydrophones and sonar projectors. The most widely used transduction principles are electromagnetism, electrostatics and piezoelectricity.

image

 

An ordinary acoustic guitar generates sound entirely through vibration.  If you pluck a string, it vibrates back and forth, transmitting sound energy into the hollow wooden body of the guitar, making it resonate and amplifying the sound. An electric guitar produces sound through electromagnetism, electromagnetic induction to be precise.  The metal strings of an electric guitar act as dynamos: producing electricity when you move them. Under the strings, you will find electricity-generating devices called pickups. Each pickup consists of one or more magnets with hundreds or thousands of coils around them. The magnets generate a magnetic field that passes up through the strings making them partially magnetized and when they vibrate, they make a very small electric current flow through the wire pickup coils. The pickups are hooked up to an electrical circuit and amplifier, boosting the small electric current and sending it to a loudspeaker, usually an "amp" which consists of the amplifier and loudspeaker in a simple unit.

image

 

Transducers in most common loudspeakers, including woofers and tweeters, are electromagnetic devices that generate waves using a suspended diaphragm driven by an electromagnetic voice coil, sending off pressure waves. Electret microphones and condenser microphones employ electrostatics—as the sound wave strikes the microphone's diaphragm, it moves and induces a voltage change. The ultrasonic systems used in medical ultrasonography employ piezoelectric transducers. These are made from special ceramics in which mechanical vibrations and electrical fields are interlinked through a property of the material itself.

 

Pythagoras, often described as the first pure mathematician, is credited with making one of the first discoveries around sound in the sixth century BC.  In what is now known as the law of strings, he noted the relationship between the length of a vibrating string and the tone that it produces. He noticed that these vibrating strings produced harmonious tones when the lengths of strings are whole numbers, something that could be extended to other instruments.  Pythagoras himself was a fine musician who played the lyre.  He enjoyed using music as a means to help those who were ill.

 

The modern study of sound is said to have originated from Galileo Galilee, whose interest in sound is said to have been inspired by his father who was a mathematician, musician, and a composer of some repute. He elevated sound to a science by studying vibrations and the correlation between frequency and the source of sound.  In the Discorsi  Galileo thought out the vibrating complexion of sounds, and asserted that the pitch was correlated with the number of vibrations. He was unable to count them, so he did not use the word “frequency,” but spoke of the “number of vibrations in the same time.”image

image

 

Acoustics is the study of all mechanical waves in gases, liquids, and solids and encompasses the topic of vibrations, sound, ultrasound, and infrasound. The audio range of the spectrum is between 20 Hz and 20,000 Hz.  This range is important because its frequencies can be detected by the human ear.

 

Very low frequency, beyond what our ears can hear refers to infrasound while anything operating at very high frequency is ultrasound.  The ultrasound range is commonly used for medical diagnostics such as sonograms.  An ultrasound scan uses high-frequency sound waves to create images of the inside of the body. A pregnancy ultrasound is a test that uses high-frequency sound waves to image a developing baby as well as the mother's reproductive organs. An ultrasound, also called a sonogram, can help monitor normal fetal development and screen for any potential problems.  Ultrasound scans, or sonography, are safe because they use sound waves or echoes to make an image, instead of radiation. Ultrasound scans are used to evaluate fetal development, and they can detect problems in the liver, heart, kidney, or abdomen. They may also assist in performing certain types of biopsy.  Animals such as dogs, birds, and bats can hear ultrasound. The high pitched ultrasound used by bats in echolocation is perfect for navigating at night because these noises are easily reflected back to the bats by objects in the environment:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Anything under the 20 Hz range is known known as the infrasonic range.  Sources of infrasound in nature include volcanoes, avalanches, earthquakes and meteorites.  Early studies of infrasound of hurricanes offer some hope of deciphering the infrasound signature of an approaching hurricane. Monitoring of infrasound seems to be one of the best ways for detecting atmospheric nuclear tests.  A number of animals produce and use sounds in the infrasonic range.   Animals such as elephants, whales, and hippopotamus use infrasound  to communicate over long distances.  Infrasound frequencies travel well through objects instead of being reflected so its good for long distance communication.  because they travel well through objects instead of being reflected. The rumbling vocalizations of elephants have been measured at frequencies as low as 14 Hz, detectable at a range of 10 km.

 

Analytic instruments such as the spectrum analyzer facilitate visualization and measurement of acoustic signals and their properties. The spectrogram produced by such an instrument is a graphical display of the time varying pressure level and frequency profiles which give a specific acoustic signal its defining character.

 

Episode 227: The Ben Heck Show’s Felix Hacks a Guitar Episode

 

image

 

Your Chance to Win

 

Be Original
Stick to the Theme
  • You could come up with a clever name that make's your project memorable!
    • This project is your baby! Part of the fun of bringing something new into the world is coming up with a name.
  • Your project could introduce something new or that is not commercially available or affordable!
  • If you have an idea for a project that doesn't fit the current theme then submit your idea in the comments section of the monthly poll.
List the Steps
Submit Video Proof
  • Provide the steps you took to complete your project (text, video, or images).
    • This could be a step by step how-to-guide, vlog, schematics, coding, napkin drawings, voice narration, or whatever you think will be useful!
  • If it doesn't work that's fine, this is more about the journey than the end product.
  • A short video is all that is required but you can shoot as much video as you like.
  • You are encouraged to be creative and have as much fun as possible!

 

Your Project Examples

 

Acoustics
Homemade Electric Guitar Tube Amp on a PCB
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
Your Prizes

 

One Grand Prize Winner Wins a $200 Shopping Cart!Three First Place Winners Win a $100 Shopping Cart
  • One Grand Prize Winner Wins a $200 Shopping Cart!
  • 3 First Place Winners a $100 Shopping Cart!
imageimage

 

 

 

Your Project, Your Ideas!

 

About Project14
Directions

Every month you'll have a new poll where you'll get to decide an upcoming project competition, based on your interests, that will take place a couple of months in advance. Themes are broad in scope so that everyone can participate regardless of skill set.

 

What are Monthly Themes?

  • Every month (around the 14th of each month) a new theme will be posted on Project14.
  • Submit your ideas (proposals) for your projects to get feedback from the rest of the community.
  • Submit a project entry in the Theme space once you start working on it.

 

What are Monthly Theme Polls?

  • Every month (around the 14th of each month) there is a project theme poll.
  • Vote on which project competition you want to see for the following upcoming theme.
    • The themes voted on during the previous poll decided the upcoming theme.
    • If you submit an idea for a theme that is not used then it can still be used in a future poll.
  • Themes comments and ideas from the comments section of the project theme poll.

Step 1: Log in or register on element14, it's easy and free.

Step 2: Post in the comments section below to begin a discussion on your idea. Videos, pictures and text are all welcomed forms of submission.

Step 3: Submit a blog post of your progress on your project by the end of the month.  You are free to submit as many blog entries as you like until the beginning of the next theme.

 

Be sure to include video proof of your project!

 

Visit: Acoustics  or tag your project blog AcousticsCH

 

You have until March 16th End of Day to submit your completed project!

 

A jury consisting of your peers will judge project submissions!

 

In the Comments Below Let Us Know Your Ideas for Projects Around Acoustics!

  • pickup coils
  • electroacoustic
  • ultrasound
  • acoustic
  • acoustic electric
  • electromagnetism
  • mechanical wave
  • spectrum analyzer
  • electromagnetic
  • pressure waves
  • loudspeaker
  • reverberation time
  • piezoelectric material
  • piezo electric
  • piezo transducer
  • infrasound
  • sonar projectors
  • audible sound
  • amplifiers
  • sound
  • electromagnetic induction
  • pickup
  • law of strings
  • acousticsch
  • pythagoras
  • hydrophones
  • external noise
  • acoustic engineering
  • tweeter
  • electret microphones
  • spectrogram
  • sound intimacy
  • galileo
  • magnets
  • vibration
  • microphones
  • particle velocity sensors
  • speaker
  • frequency
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • easyejl
    easyejl over 6 years ago +9
    I think i have one. I'm pondering using light AI along with it. What it will be is an automatic dog bark stopping system. It will listen for the frequency + pattern of a dog barking, and then use a piezo…
  • dubbie
    dubbie over 6 years ago +9
    I might have a go at a scanned ultrasonic radar which technically should be SADAR or maybe AADAR. Rather than mechanically rotate the ultrasonic transmitter, just keep it static and use multiple receivers…
  • dougw
    dougw over 6 years ago in reply to easyejl +8
    Cool idea. I once tried hooking up a high power tweeter to an ultrasonic tone coming from a power amp - to keep dogs off the lawn. It didn't do anything cool like detect dogs barking - it was just manually…
Parents
  • cypresstwist
    cypresstwist over 6 years ago

    I always wanted my own scream machine. So here's my project in its infancy:

     

    Audio project: Agony Box

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cypresstwist
    cypresstwist over 6 years ago

    I always wanted my own scream machine. So here's my project in its infancy:

     

    Audio project: Agony Box

    • Cancel
    • Vote Up +4 Vote Down