• Products and Partners
    Products and Partners
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
Project14
  • Challenges & Projects
  • More
Project14
Member Updates Time and Space Prize
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 3 Jul 2024 9:00 PM Date Created
  • Views 2746 views
  • Likes 16 likes
  • Comments 13 comments
  • SLG4DVKGSD
  • Time and Space
  • SLG47004V
  • greenpak
  • ADAU1467
  • SLG47004V-SKT
  • AnalogPAK
  • renesas
  • analog devices
  • LCTR1002
  • EVAL-ADAU1467Z
  • SLG47004V-EVB
  • sigmadsp
  • SLG47004
Related
Recommended

Time and Space Prize

shabaz
shabaz
3 Jul 2024

Thanks to the judges and element14, I was able to obtain some bits and pieces that I may not ordinarily have purchased. I took the opportunity to try some new things. This blog post just contains some photos, in case they are of interest.

First off are some items that will allow experimentation with a Renesas GreenPAK part SLG47004V.

image

The diagram here shows what’s inside the SLG47004V chip; it contains analog functions such as op-amps and comparators, plus digital functions such as configurable combinatorial logic, flip-flops, and even a digital pattern generator. I don’t know much more about it currently.

image

Here’s a close-up of the SLG47004V-EVB board which is mostly blank apart from the single SLG47004V chip installed at the center.

image

The SLG4DVKGSD board is used to program it:

image

Both the eval board and the programmer board are quite low-cost, which makes it attractive for experimenting. However, the chip is QFN sized : ( so I figured it was worth getting the SLG47004V-SKT board that contains a QFN socket broken out to pin headers. It comes with 20 SLG47004V chips, i.e. plenty for a lot of experimentation (each chip is reprogrammable).

image

I also wanted to experiment further with audio DSP, and I selected an Analog Devices DSP board, EVAL-ADAU1467Z. It comes with a separate USB interface board.

image

The ADAU1467 is one of the more powerful DSPs in the range.

image

These types of DSP chips are extremely easy to use and it doesn’t have to cost a lot; see the following blog post:  Wave Miner: A Pi-controlled Digital Signal Processor 


Close-up of the evaluation board:

image

Underside:

image

The USB interface board is extremely useful (it can be purchased separately as EVAL-ADUSB2EBZ), but unfortunately, it’s pricey. However, it is possible to work around it and use a Pi partially, but that’s nowhere near as convenient.

image

Finally, I also chose an LCTR1002 50-ohm SMA RF terminator and some GC005-LF prototyping boards.

image

Thanks for reading.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 2 years ago in reply to balajivan1995 +1
    Things like Echo Dot (at least the early versions; I've not checked the recent models) use tiny MEMs microphones, and at least the Echo Dot 2 uses analog output ones, connected to an ADC (TI TLV320ADC3101…
Parents
  • shabaz
    shabaz over 2 years ago

    I installed the software needed for the GreenPAK device, which is called (awful name) Go Configure Software Hub. Upon startup, it was possible to select the chip, and then a 'GreenPAK Designer' window appears with a center black area for schematics.

    For a first project I just clicked on the right-side pane list of internal components to choose an op amp. Them I selected some external components (resistors and voltage sources) using the left side pane. Very straightforward. Wires are added by clicking on any two nodes (only valid connections will be formed).

    Then, I clicked on Debug, a simulation pane appeared on the right, and then it was possible to right-click on nodes to add probes.

    image

    When the simulation was run from the simulation pane, charts with the probe outputs appeared. The bottom blue trace is the op amp output. 

    image

    Interesting how the output wasn't correct for the first approx 2 msec. Probably that's the chip initializing itself (maybe). I'm guessing.

    So far I've only used the software, and have not tried to connect to the board.

    Anyway, this is really neat. I need to explore this more. There are examples online, that do more sophisticated stuff such as reading rotary encoders and generating adjustable sine-waves. 

    The incredible thing is the low cost. These chips are about $2 in single quantity, yet house several op-amps, electronically controlled resistors, oscillators, logic and so on. They are also low-power (can operate from coin cells).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 2 years ago

    I installed the software needed for the GreenPAK device, which is called (awful name) Go Configure Software Hub. Upon startup, it was possible to select the chip, and then a 'GreenPAK Designer' window appears with a center black area for schematics.

    For a first project I just clicked on the right-side pane list of internal components to choose an op amp. Them I selected some external components (resistors and voltage sources) using the left side pane. Very straightforward. Wires are added by clicking on any two nodes (only valid connections will be formed).

    Then, I clicked on Debug, a simulation pane appeared on the right, and then it was possible to right-click on nodes to add probes.

    image

    When the simulation was run from the simulation pane, charts with the probe outputs appeared. The bottom blue trace is the op amp output. 

    image

    Interesting how the output wasn't correct for the first approx 2 msec. Probably that's the chip initializing itself (maybe). I'm guessing.

    So far I've only used the software, and have not tried to connect to the board.

    Anyway, this is really neat. I need to explore this more. There are examples online, that do more sophisticated stuff such as reading rotary encoders and generating adjustable sine-waves. 

    The incredible thing is the low cost. These chips are about $2 in single quantity, yet house several op-amps, electronically controlled resistors, oscillators, logic and so on. They are also low-power (can operate from coin cells).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 2 years ago in reply to shabaz

    I've looked at GreenPAK stuff from time to time but not in the last couple of years since Renesas bought them. This chip looks quite fun - I don't have anywhere for it to go right now but I couldn't resist buying the kit and the adaptor !

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to michaelkellett

    Awesome! These do seem to be intriguing/fun things. Looking forward to exploring a bit more with them hopefully at the weekend.