Crazy Arduino Automations
  • Challenges & Projects
  • Project14
  • Crazy Arduino Automations
  • More
  • Cancel
Crazy Arduino Automations
Crazy Arduino Automations Forum Arduino Day 2023 Giveaway: Win an Arduino Board for Your Crazy Arduino Automation Project Proposal!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Crazy Arduino Automations to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 43 subscribers
  • Views 9016 views
  • Users 0 members are here
  • arduino nano
  • crazyarduinoautomationch
  • arduinoday2023
  • arduinoday23
Related

Arduino Day 2023 Giveaway: Win an Arduino Board for Your Crazy Arduino Automation Project Proposal!

tariq.ahmad
tariq.ahmad over 3 years ago

In the Comments Below:   Let Us Know What Crazy Arduino Automation You Would Do with One of These Boards!

In a honor of Arduino Day we are giving away some really cool Arduino Boards.   Let us know a crazy arduino automation project that you want to use with one of these boards.  We have 4 Nicla Sense ME boards, 4 Arduino Nanos, a Nano 33 IoT Board, Portenta H7 board, a TinyML Kit, a couple of MKR 1010 boards, and a Limited Edition Uno Board to giveaway.    Simply comment below with your Crazy Arduino Automation project idea for a chance to win one of these you boards.

Here are the Arduino products that we are giving away:

image image
4 x Nicla Sense ME Boards Nano 33 IoT Board

The Nicla Sense ME is a tiny, low-power tool that sets a new standard for intelligent sensing solutions. With the simplicity of integration and scalability of the Arduino ecosystem, the board combines four state-of-the-art sensors from Bosch Sensortec:

  • BHI260AP motion sensor system with integrated AI
  • BMM150 magnetometer
  • BMP390 pressure sensor
  • BME688 4-in-1 gas sensor with AI and integrated high-linearity, as well as high-accuracy pressure, humidity and temperature sensors. 

Arduino Nano 33 IoT is a small, robust and powerful board with Wi-Fi and Bluetooth connectivity combined with its low power architecture makes it a practical and cost effective solution. It is fully compatible with the Arduino IoT Cloud and supports full TLS secure transport.

The ATECC608A cryptochip stores the cryptographic keys in hardware, offering a very high level of security for this class of products. The integration with the Arduino IoT Cloud offers also a very efficient way of setting up online dashboards with little coding and minimal effort. It is an easiest and cheapest point of entry to enhance existing devices (and creating new ones) to be part of the IoT and designing pico-network applications. T

The Wi-Fi and Bluetooth® connectivity is performed with a module from u-box, the NINA-W10, a low power chipset operating in the 2.4GHz range. It is perfect for simple vibration alarm systems, pedometers, relative positioning of robots.

Buy Now Buy Now
image image

Portenta H7 Board

Arduino Tiny Machine Learning Kit

Portenta H7 module simultaneously runs high level code along with real time tasks. Its two asymmetric cores can simultaneously run high level code such as protocol stacks, machine learning or even interpreted languages like MicroPython or Javascript along with low-level real time tasks.

PH7's main processor is a dual core unit made of a Cortex® M7 running at 480MHz and a Cortex® M4 running at 240MHz. Two cores communicate via remote procedure call mechanism that allows calling functions on other processor seamlessly. The on-board wireless module allows to simultaneously manage Wi-Fi and Bluetooth connectivity. Bluetooth interface supports Bluetooth Classic and BLE. 

The Portenta H7 follows Arduino MKR form factor but is enhanced with Portenta family 80 pin high-density connector. The board comes with STM32H747 dual-core processor with graphics engine, 8MB SDRAM, 16MB NOR flash, 10/100 Ethernet Phy, USB HS, NXP SE050C2 Crypto, Wi-Fi/BT module, ceramic antenna, DisplayPort over USB-C.

The Tiny Machine Learning Kit, combined with the exciting TinyML Applications and Deploying TinyML on Microcontrollers courses that are part of the Tiny Machine Learning (TinyML) specialization from EdX will equip you with all the tools you need to bring your ML visions to life!

The kit consists of a powerful board equipped with a microcontroller and a wide variety of sensors (Arduino Nano 33 BLE Sense*). The board can sense movement, acceleration, rotation, barometric pressure, sounds, gestures, proximity, color, and light intensity. The kit also includes a camera module (OV7675) and custom Arduino shield to make it easy to attach your components and create your very own unique TinyML project. You will be able to explore practical ML use cases using classical algorithms as well as deep neural networks powered by TensorFlow Lite Micro. The possibilities are limited only by your imagination!

“The Future of Machine Learning is Tiny and Bright. We’re excited to see what you’ll do!”
Prof. Vijay Janapa Reddi, Harvard University and Pete Warden, Google

Buy Now Buy Now
image image
Arduino Uno Mini 4 x  Arduino Nanos

The world's favorite development board has gone mini. Everything in this version of the Arduino UNO is unique. Black and gold, finishing, elegant design and packaging, all delivered to the highest standard. A little jewel to celebrate the Arduino community and what we’ve been doing together for all these years.

Each item is unique and numbered on the PCB, and includes a hand-signed letter from the founders. It’s a limited edition, so get while it’s in stock!

The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328 (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one.

Buy Now

Buy Now
image
2 x Arduino MKR 1010 Boards

Ever wanted an automated house? Or a smart garden? Well, now it’s easy with the Arduino IoT Cloud compatible boards. It means: you can connect devices, visualize data, control and share your projects from anywhere in the world. Whether you’re a beginner or a pro, we have a wide range of plans to make sure you get the features you need.

The Arduino MKR WiFi 1010 is the easiest point of entry to basic IoT and pico-network application design. Whether you are looking at building a sensor network connected to your office or home router, orif you want to create a Bluetooth® Low Energy device sending data to a cellphone, the MKR WiFi 1010 is your one-stop-solution for many of the basic IoT application scenarios.

Buy Now

T&C Arduino Day 2023 Giveaway

  • Sign in to reply
  • Cancel

Top Replies

  • JWx
    JWx over 3 years ago in reply to Gough Lui +3
    maybe put it behind glass with "In case of emergency - break glass" sign...
  • Gough Lui
    Gough Lui over 3 years ago +2
    The Arduino Uno Mini is certainly cute and perhaps a bit too pretty to be actually used in any serious project. Perhaps it can be the centerpiece for an LED sequencer to light up a picture frame containing…
  • colporteur
    colporteur over 3 years ago +2
    Putting the farm animals out to pasture On a 12x12 piece of plywood, I am constructing a farm scene for an HO scale model train layout. The scene is of a farm yard fenced-in enclosure that has pigs…
Parents
  • JWx
    JWx over 3 years ago

    And another one - it would be interesting to check power-saving capabilities of Nano 33 IoT Board vs. standard ESP module... In theory it would be no better (it includes NINA-W102 wifi-module that is ESP32 based) but who knows - maybe it is better optimized than one would think

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to JWx

    and this one would be "Efficient, battery powered Arduino based wi-fi sensor"  as project idea

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 3 years ago in reply to JWx

    and this one would be "Efficient, battery powered Arduino based wi-fi sensor"  as project idea