DIY Test Equipment
  • Challenges & Projects
  • Project14
  • DIY Test Equipment
  • More
  • Cancel
DIY Test Equipment
Blog Portable addressable led strip tester
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Equipment to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: den_olli
  • Date Created: 8 Sep 2017 12:19 PM Date Created
  • Views 2886 views
  • Likes 2 likes
  • Comments 15 comments
  • diytestequipch
Related
Recommended

Portable addressable led strip tester

den_olli
den_olli
8 Sep 2017

in the office building I work we have DIY addressable led strips surrounding every floor of the building to make it glow at night. It's a part of my job to maintain this setup and unfortunately the setup breaks down a lot.

 

We we got a defect then I have to open up the sealing and get the 3m long led bar out and take it to the warehouse to test the led strip. I have already bought a wireless soldering iron so I can do small repairs without taking the led strip out of the sealing, but I still need to get it out if I want to connect it to the test unit.

 

It would really be great if I would have sort of a portable addressable led strip tester, that can run the following tests

- put all led's to red

- put all led's to green

- put all led's to blue

- put all led's to white

- slow nightrider mode 1 led at a time

- put all led's to black (off)

 

this would save me a lot of time and I guess it would be a great tool for everyone that uses addressable led strips in there projects

I'm trying to figure out a way to make such tester, but the main problem I have is how to deliver enough power for the 3 meter long led strip?

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +3
    You can buy low cost commercial controllers for ws2812 or whatever led type you have or make your own... https://learn.adafruit.com/adafruit-neopixel-uberguide/arduino-library
  • shabaz
    shabaz over 9 years ago in reply to den_olli +3
    Hi Olivier, How frequently is there a failure? And how long could it take to fix the failure, if you had a test tool? Even if it takes just 30 minutes to fix, this is very expensive, considering the aliexpress…
  • gadget.iom
    gadget.iom over 9 years ago +2
    Do you know what make/model the LED strips are? How may LED's need testing by the unit?
Parents
  • mcb1
    mcb1 over 9 years ago

    It sounds very much that the system was not designed to be easily serviced (sadly a common problem)

     

    I'm trying to figure out a way to make such tester, but the main problem I have is how to deliver enough power for the 3 meter long led strip?

    The strip shown above seems to be 144 LED/metre and are the addressable type.

     

    If they are 144/m then one site said it was 43.2 W/m which is 8.64A at 5v.

    This means a single 3m length uses 25.92 Amps.

     

    Having two strips off the same supply is likely to cause issues when they are on white and full brightness.

     

    You'd also need to verify that there are connectors at various points.

    Looking at your picture it seems that there are power and the connection back to the controller.

     

     

    If you can confirm the number of LEDs per metre and the type (some more sharp photos will help), then we might be able to suggest a controller.

    I am suspicious of the power, and curious to know the wiring running back to the controller as I see three wires along with the DC connector.

    The Data and earth are okay but the 5v is only likely to start pulling power from other sections, which may make things worse.

     

     

    Do you have records of the cause each month, or more correctly what has fixed the apparent problem.

    If the LED strips aren't being replaced, then it's either connections, controller or the power supplies.

     

    If the strip isn't the issue, then it sounds like you need a portable strip to prove the rest of the system is working before removing the strips from the ceiling.

    WS21812 strips should work even if you don't connect the rest of them after that strip.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to mcb1

    mcb1 wrote:

     

    It sounds very much that the system was not designed to be easily serviced (sadly a common problem)

     

    It is probably a fire hazard too. From the photo, I can't believe those wires are anything other than low-temperature flammable hobby grade stuff, with a 26A-capable supply connected. Probably unfused too, so prossibility of flames when (I won't even say 'if') a short occurs. It is extreme incompetence to fit such a huge amount of aliexpress sourced lighting into a building.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to shabaz

    It appears the power supply is here.

    RS-150-MEAN WELL Switching Power Supply Manufacturer

     

    It has a hiccup type overload system, but that doesn't help the wiring issues.

    I also struggle with the connectors that are shown in the photo.

    26A is a lot to expect form the style used, unless they feed the DC from both ends.

     

    As we know breaking the sections up into smaller size is a better option, esecially when the LED concentration is so high.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • den_olli
    den_olli over 9 years ago in reply to mcb1

    I don't know a lot about the custom controller, but I know that the power of the strips is via 1,5mm wires instead of the default wires an that it's connected to a few places on the strip.

    And to be honest, I'm also not convinced that there design is save. I want to make it better and safer, but then I need to be able to proof first that it isn't safe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • den_olli
    den_olli over 9 years ago in reply to mcb1

    I don't know a lot about the custom controller, but I know that the power of the strips is via 1,5mm wires instead of the default wires an that it's connected to a few places on the strip.

    And to be honest, I'm also not convinced that there design is save. I want to make it better and safer, but then I need to be able to proof first that it isn't safe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to den_olli

    but then I need to be able to proof first that it isn't safe

    In that vein then, are you able to take detailed photos of the connections (ie not the actual controller details).

     

    We can offer some advice, and points for futher testing that would allow you to put together a report to your management.

     

    I have no actual issue with the LED's but I do think the way they manage the DC load could be improved to make it safer, reliable and much easier to manage.

     

     

     

    Mark