DIY Test Equipment
  • Challenges & Projects
  • Project14
  • DIY Test Equipment
  • More
  • Cancel
DIY Test Equipment

Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Equipment to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Raspberry PI - Ohmmeter

    sherbieny
    sherbieny
    An Ohmmeter device using Raspberry PI 2B with ADS1015 as ADC https://github.com/Sherbieny/Ohmmeter-Pihttp://fritzing.org/projects/pi-ohmmeterSetupItems needed:PC or LaptopRaspberry Pi (I used model 2B)ADS1015 12bit ADC converter (if you use 1115...
    • 23 Sep 2017
  • DIY Wired & WiFi (2.4Ghz & 5 Ghz) Analyzer

    dgshue
    dgshue
    I started this post as a Wifi Analyzer... but the more I got into it the more it became a complete handheld network analyzer for wireless as well as wired for performing basic network functions such as speed tests and pings, on up to measuring signal...
    • 14 Sep 2017
  • Raspberry pi web interface computer on and off system

    dasherman
    dasherman
    Hi i resently got an idea after learning about freenas interface web based I learned that freenas lets you to turn off your computer form the web so i was thinking is it possible to turn the comouter on by the web interface so i tryed to solve this p...
    • 11 Sep 2017
  • Portable addressable led strip tester

    den_olli
    den_olli
    in the office building I work we have DIY addressable led strips surrounding every floor of the building to make it glow at night. It's a part of my job to maintain this setup and unfortunately the setup breaks down a lot. We we got a defect the...
    • 8 Sep 2017
  • Raspberry Pi Universal Scope/Meter

    masonjones
    masonjones
    How about building a Raspberry Pi universal multimeter and oscilloscope. You could use the bitscope mod and if you can create a application you can make a multimeter app to measure voltage, resistance and current (Or even a LCR function)
    • 7 Sep 2017
  • Project14's DIY Test Equipment: DIY Constant Current Load

    ipv1
    ipv1
    This is my submission to the Element14 Project14 DIY The problemI have recently been doing extensive experimentation with recycled batteries as well as voltage regulators and line control circuits. The customary approach requires a programmable ...
    • 3 Sep 2017
  • Elevator test unit

    popupideas
    popupideas
    one diy test unit I want to build is a g-force accelerometer tested for elevators. Prefer a Bluetooth enabled box you put inside an elevator that when it is sent up it will record the travel speed, acceleration, start and stoppong force. It bit I had...
    • 27 Aug 2017
  • Multi-Ref Mk. II

    hlipka
    hlipka
    The Multi-Ref is not a test device as such, but the tool I use to test my test equipment. I got the idea for this from the user [matseng] as the Dangerousprototypes.com forum, and found it very useful.MrRef, as it was called, is just two coin cells p...
    • 22 Aug 2017
  • Building a Fluxgate Magnetometer based Current Probe

    shabaz
    shabaz
    IntroductionCurrent measurement can be really awkward when working with circuits. Voltage measurements are (usually) straightforward, but when it comes to current measurements the story is different. One typical approach is to insert a known resistan...
    • 22 Aug 2017
  • Arduino oscilloscope - DIY entry device

    idanre1
    idanre1
    The Software The Hardware The probe - Try 1 (not that good, please review try 2) The probe - Try 2 Summary Proof of work  The big problem with being a maker newbie, is that you have to have equipment.When I started, I bought solderin...
    • 21 Aug 2017
  • Vintage 555 - A general-purpose button debouncer

    balearicdynamics
    balearicdynamics
    Too many button clicksButtons and tactile switches are frequently used in many projects involving micro controllers; one of the most frequent issue is related to unwanted multiple transitions when the button is pressed once.Tactile switches as well a...
    • 12 Aug 2017
  • DIY Test Equipment: Ears and Tears 2020 (A Logic Probe)

    koudelad
    koudelad
    IntroductionWhen I saw Jon's The ByEar 2000, I remembered a Cypress' video showing a construction of an analog alarm and posted that as an comment under his blog post.PSoCs usually have many integrated analog and digital peripherals, so I tho...
    • 6 Aug 2017
  • DIY Test Equipment: The Di-o-Matic, a Simple Diode Tester [Arduino]

    jc2048
    jc2048
    I really should be doing other things, but I can't resist doing another quick piece of DIY Test Equipment. Again I'mgoing to post it here in my blog. I haven't worked it up into a polished piece of equipment - it isn't even reallyfini...
    • 5 Aug 2017
  • USB Programmable (electronic DC load) Test Equipment

    Jan Cumps
    Jan Cumps
    peteroakes, jc2048 and I are designing a programmable electronic load, here on element14: Programmable Electronic LoadWe'll never make it in time for the DIY Test Equipment initiative (we may have a first prototype In the Year 2525). But it can h...
    • 30 Jul 2017
  • Mini Logic Probe with display

    Workshopshed
    Workshopshed
    I was planning to make a super simple logic probe but Jon beat me to it with his comparator based logic probe. So I've prototyped a microcontroller based one. Microcontroller based logic probe with displayMy project has just two modules, an ...
    • 26 Jul 2017
  • TLE94112 Interactive Testing Platform

    balearicdynamics
    balearicdynamics
    Introduction The Project Planning the Design Testing motors Control I/O DC/DC Regulator Design in practice The Testing Platform The Software Software Design 1. Main Sketch Main loop() structure Motors running status block Seri...
    • 26 Jul 2017
  • DIY Test Equipment: Mini Air Jet

    rsc
    rsc
    I work with small thermocouples and Hot-Wire/Hot-Film devices in my lab.  To test and calibrate these devices requires some crazy equipment sometimes.Try to imagine blowing air on a thermocouple that's in a chain of thermocouples 1mm apart witho...
    • 21 Jul 2017
  • Help in Finding Rotational Speed of Different Types of Electric Motors (Submition attempt #2)

    swankybarbecue4
    swankybarbecue4
    Just understood what the prize is haha. In that case, this could benefit me with the documentation of the different max speeds of all electric motors in my inventory. I could then select the most appropriate motor for a certain application. &nbs...
    • 18 Jul 2017
  • Simple 8-bit Computer (Finding Unknown Components)

    swankybarbecue4
    swankybarbecue4
    I have recently begun the construction of an 8-bit computer based around an Intel 8088 CPU. I believe that I have all necessary components for the build, but I am still not too sure. A handful of ICs (including what appears to be the clock IC) have l...
    • 18 Jul 2017
  • Cyclops-1000: An Electronic Eye for Rotational Speed Measurement

    shabaz
    shabaz
      Introduction How does it work? Working with the Microcontroller Building the Circuit PCB Version Final Test and Assembly How does the Software work? Summary Parts List August 2019 Update - Revision 2 Code Background Revision 2 Algorithm B...
    • 14 Jul 2017