• Products and Partners
    Products and Partners
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
Electromagnetism
  • Challenges & Projects
  • Project14
  • Electromagnetism
  • More
  • Cancel
Electromagnetism
Blog 3000A clamp table and amplifier update #2
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electromagnetism to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 15 Apr 2019 8:11 PM Date Created
  • Views 1365 views
  • Likes 6 likes
  • Comments 4 comments
  • clamp adapter table
  • electromagnetismch
  • flir cm55
  • current amplifier
  • impedance measurements
  • clamp meter
Related
Recommended

3000A clamp table and amplifier update #2

three-phase
three-phase
15 Apr 2019

I have done some more work today on the current amplifier and found that I did not have the input turned up to a high enough voltage to obtain the full 1A output, so I have now repeated the test and monitored the heat output from the amplifier.

 

image

This is still just within the nominal operating temperature specified for the op-amp, but it was still climbing slowly when turned off. When switched back down to a 0.5A output, the temperature does start to drop away quite rapidly.

 

With this completed, I decided to do a few quick tests with a 20 turn coil and a CM55 current clamp as shown below.

 

{gallery} CM55 current clamp tests

image

10A reading expected on clamp meter

image

20A reading expected on clamp meter

image

Clamp meter taken beyond frequency specification

The first two tests show the clamp meter with the expected readings for a 50Hz input into the 20 turn coil. The frequency was then raised in the third picture and you can see that the current reading drops right off. For a Rogowski style clamp, the CM55 actually has quite a poor bandwidth.

 

My next stage with the current amplifier will be to try and figure out a way of measuring the input and output of the coils with the equipment I have, to see if there is any frequency drop off across the coil.

 

I have collected some impedance data for each of the coils I have wound using an LCR meter.

 

image

imageimage

The data shows the increasing impedance of the coil as the frequency is increased. This may give issues with being able to reach the full output current using the existing amplifier design.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +3
    Hi Donald, This is a great project, a nice challenge. I was wondering, (these ideas may have flaws..): if the coil could be possible with copper blanks per turn (e.g. like these ) with the centre punched…
  • genebren
    genebren over 7 years ago +3
    Donald, Another great update. It does appear that the clamp is rolling off at higher frequencies. Looking at the specification for the clamp, the AC frequency range is listed as 45 - 500Hz, so 5KHz is…
  • three-phase
    three-phase over 7 years ago in reply to shabaz +1
    That is an interesting alternative to manufacturing a coil, depending on the size of the copper, each joint is going to have be either soldered or brazed, there will also need to be insulation between…
Parents
  • three-phase
    three-phase over 7 years ago

    Many thanks Gene. I did go and check the frequency response of the CM55 myself and it did surprise me how low it was. The older style tongue clamps did have a low frequency response due to the limitations of the magnetic circuit and the introduction of Rogowski coils provided a much higher frequency capability.

     

    The Fluke i2000 I have will go up to 20kHz, so it must be a design choice by Flir to reduce the frequency capability within the electronics.

     

    Kind regards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 7 years ago

    Many thanks Gene. I did go and check the frequency response of the CM55 myself and it did surprise me how low it was. The older style tongue clamps did have a low frequency response due to the limitations of the magnetic circuit and the introduction of Rogowski coils provided a much higher frequency capability.

     

    The Fluke i2000 I have will go up to 20kHz, so it must be a design choice by Flir to reduce the frequency capability within the electronics.

     

    Kind regards.