Energy Harvesting
  • Challenges & Projects
  • Project14
  • Energy Harvesting
  • More
  • Cancel
Energy Harvesting
Documents Project14 | Energy Harvesting: Build Projects that Scavenge Energy from Wasted Energy Sources!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Energy Harvesting to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 29 Jul 2019 5:19 PM Date Created
  • Last Updated Last Updated: 10 Sep 2019 4:10 AM
  • Views 13915 views
  • Likes 11 likes
  • Comments 39 comments
Related
Recommended

Project14 | Energy Harvesting: Build Projects that Scavenge Energy from Wasted Energy Sources!

image

Energy Harvesting

Enter Your Project for a chance to win an Energy Harvesting Grand Prize for Inspiring the World to Reuse Wasted Energy!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

In the Comments Below:  What Ideas do You Have for Projects that Harvest Energy from Wasted Energy Sources?

 

The Project that Does the Best Job of Inspiring the World to Reuse Wasted Energy Wins an Energy Harvesting Kit to Go!

 

image
Buy NowBuy Now
The Grand Prize is an energy harvesting board and a Giant Gecko starter kit plus a $200 Shopping Cart!

 

The theme this month is Energy Harvesting and it comes from a suggestion from fmilburn.  Energy harvesting, sometimes called energy scavenging, involves capturing small amounts of energy that would otherwise be lost. The idea is to build projects that involve capturing energy from ambient sources (such solar, wind, vibration, heat, motion, sound) and storing it in an associated storage such as rechargeable batteries, super capacitors, ceramic capacitors, and polymer capacitors.  Also, share your interest in Energy Harvesting in Project14 | What Type of Energy Harvesting Do You Find Most Interesting?   Because this is a very promising eco-friendly technology, that is yet to meet its potential, we've added an Energy Development Platform Kit as the Grand Prize for the project that inspires the world (the most) to reuse wasted energy!  The kit includes four linear voltage converters that are optimized for different energy sources such as solar, electromagnetic, piezo electric, or thermal energy converters. There's also the usual $100 shopping cart for the 3 first winners.  Energy harvesting can be used as an alternative or a supplement to batteries for low-power, lower voltage applications such as a wireless sensor node, where it may be used as a secondary energy source to recharge a battery. It is well suited for applications that require back-up battery, especially in remote or locations that are difficult to reach.  The energy that is typically captured is small so its ideal for any low voltage, low-power project such as a wearable or portable device. The goal of energy harvesting developers is to create self-sustaining and/or improve the efficiency of non-sustainable systems.

 

image

Harvesting energy from non-conventional sources in the environment has received a lot of attention from researchers looking into how these alternative energy sources can be used for lower power applications. Although energy harvesting involves capturing and storing small amounts of energy, its enough to power wireless sensors and other low-power applications. There's a lot of wasted energy in the environment that could be used to power various circuits as a cheap source of power. When applied to wireless sensor networks and IoT devices, it is an eco-friendly solution that helps eliminate the need for network-based energy and conventional batteries, minimizes costs, and reduces the need for cables and batteries. This makes it advantageous to applications in remote areas, underwater, and other hard to reach places where conventional batteries are not suitable.  Industries that look to capitalize on this potential include those looking for both low-voltage and low-power applications such as what is used in medical equipment, consumer devices, portables, transportation, industrial controls, and the military.

 

Energy that can be harvested by scavengers could be byproducts of natural environmental phenomena (solar, wind, tide), industrial process, and the energy produced by every electronic device or gadget (heat and/or vibrations).  During the  Solar Power Devices,  solar cells were used to capture light from the sun in order to produce energy.  This is also known as photovoltaic harvesting. Other methods, that you can explore are thermoelectric (heat) harvesting, piezoelectric (vibration) harvesting, and RF/Electromagnetic Harvesting (excess energy from transmitted communication signals).  Below are some common energy harvesting techniques.  This list is by no means comprehensive and is just to give you an idea of the different types of energy harvesting techniques you may want to consider for your project.

 

Photovoltaic Harvesting

image

 

Photovoltaic harvesting is the process of turning direct sunlight into electricity.  It is the most popular form of harnessing the power of the sun.  It is the process of turning direct sunlight into electricity. The photoelectric effect, the ability to create voltage and electric current in material upon exposure to light, was first observed in 1839 by French physicist Edmund Bequere.  when he noticed that certain material produces small amounts of electric current when exposed to light.  In 1954, the first commercial photovoltaic cell was built by Bell Laboratories.  It was a solar battery that was too expensive to be anything but a curiosity. The first serious use of the technology was to provide power aboard a spacecraft during the 1960s.  When the energy crisis of the 1970s hit, it began receiving recognition as a power source beyond non-space applications.  Today,  increased efficiency and affordability has led this eco-friendly technology to be used in everything from powering electronics, cars, commercial buildings, and as a supplement to power grids.

 

A photovoltaic system works by using solar panels to capture photons from sunlight. Each panel has many solar cells made up of layers of different material. These solar panels each have many solar cells made up of layers of different materials. Semiconductors (usually silicone) are sandwiched between a negative conductor on the top and a positive conductor on the bottom.  An anti-reflective coating ensures each cell captures as much light as possible.  When photons are captured by the solar sels, they release the the outer electrons of atoms within the semiconductor.  An electric current is created from the pathway between the negative and positive conductors.  This current is sent to wires that capture the DC electric current and leading to a solar inverter which Beneath that is a semiconductor (usually silicone) sandwiched between a negative conductor on top and a positive conductor on bottom. Once the photons are captured by the solar cell, they begin releasing the outer electrons of atoms within then transforms it into the AC electricity.

 

Thermoelectric Harvesting

image

Solar thermal energy is different from the type of energy you get from solar cells using photovoltaic technology. Solar thermal plants use the sun to heat a liquid (usually water) or a gas to a high temperature. Light from the sun is concentrated to create heat which is then used to run a heat engine.  The heat engine turns a generator which produces electricity. As such, thermoelectric energy harvesting is dependent mainly on the operation of the thermoelectric generator (TEG). Thermoelectric energy harvesting, is of particular interest in the automotive and industrial industries, where large amounts of heat are wasted.

 

Piezoelectric Harvesting

 

Piezoelectricity translates to "electrictity under pressure."  Human motion, low-frequency vibrations, and acoustic sounds are all potential sources of piezoelectric energy harvesting. The piezoelectric effect converts kinetic energy in the form of vibrations or shocks into electrical energy. Piezoelectric generators (energy harvesters) offer a robust and reliable solution by converting normally wasted vibration energy in the environment to usable electrical energy. They are ideal in applications that need to charge a battery, super capacitor, or directly power remote sensor systems.  Examples of piezoelectric energy harvesting include battery-less remote controls that produce energy from the force of a push of the button, piezoelectric floor tiles that generate energy from the foot traffic, and in California there was an experiment funded to convert heavily trafficked roads to piezoelectric energy.

image

 

RF/Electromagnetic Harvesting

 

The electromagnetic spectrum is an abundant source of free energy, photovoltaic harvesting is one example, RF energy harvesting is another example.  It's nothing new. One of the earliest examples of capturing ambient electromagnetic radiation (EMR) dates to the beginnings of the 20th century, with an entirely RF powered radio called the crystal radio. The history of radio begins with RF harvesting and you can read more about this in Project14 | Energy Harvesting: RF Harvesting Using a Crystal (or Fox Hole) Radio!  RF is an abundance source of ambient energy for harvesting. Electromagnetic waves can come from satellite stations, wireless internet, radio stations, and digital broadcasts. An RF harvesting system captures and converts electromagnetic energy into usable continuous voltage using an antenna and a rectifier circuit as its fundamental building blocks.  Learn more about Electromagnetism in Project14 | The Force of Electromagnetism: Anything from Solenoids, Motors, to Wireless Transfer!

 

Vibration Harvesting

 

Vibration energy harvesting is a broad category that involves converting vibration energy to electrical energy.  This is possible through several types of technology such as electromagnetic induction or piezoelectric.  Typical applications that would benefit from this would be where sensors or measurement instruments are used to gather data and traditional power sources (batteries or cables) are too expensive or impossible to use. For example, a factory using a monitoring system to make sure pumps that supply machinery with water to cool them down, doesn't break down.  Using vibration energy as a power source the monitor system can function hassle-free and immediately provide the operator with enough information to perform scheduled maintenance, rather than expensive unscheduled maintenance. Commercially successful vibration energy harvesters based on magnetic induction are limited. An example of vibration harvesting can be seen in what's been called a prototype for the first battery-free cell phone which was done by researchers at the University of Washington.  The battery-free phone takes advantage of vibrations that occur whenever a person talks or listens to a call.

 

Wind Harvesting

 

Kinetic energy from wind is used to generate electricity or mechanical power.  This type of energy is practical as a supplemental source of energy for electrical power grids.  Storage for wind energy can have high initial costs and much cheaper to keep wind energy as one piece of a varied and flexible energy grid than to store wind energy.

 

Finally, if you want to watch an inspiring story about how energy harvesting can be used check out the Netfix movie, "The Boy Who Harnessed the Wind", an inspirational true-story based on the memoir of the Malawian engineer William Kamkwamba. In one memorable scene, he rigs up a radio from several drained power cells so that he and his friends can listen to a soccer game. Although he can no longer pay tuition to pay for school, William strikes up a deal with his science teacher (he blackmails his teacher who has a secret relationship with his sister) who allows allows him to continue attending class and this gives him access to the school library where he learns about electrical engineering and energy production.  Using what he has learned he builds a small proof of concept and eventually rigs a full-sized wind turbine to irrigate crops, and become the hero in his famine stricken town.

 

"After two more weeks of reading this book, I found the most fascinating chapter – the discussion of magnets. I knew about magnets because they were used to make the speakers in radios. I'd busted off a few and taken them to school as toys, moving little slivers of metal around through a piece of paper. But as I read further, I discovered that some magnets – called electromagnets – are used to generate electricity, specifically in simple motors, like those found in a radio." - Except from the Boy Who Harnessed the Wind by William Kamkwamba

  .

Better yet, check out the memoir the movie is based on:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Energy harvesting has many exciting applications.  While the tiny amount of energy captured by energy harvesting is too small to power your cell phone, having a phone that never needs charging is one step closer thanks to researchers at UW.  They recently developed what they are calling the first battery-free cell phone to make calls using ambient power.  It works by consuming almost no power, utilizing techniques such as taking advantage of vibrations from the speaker or microphone every time a caller listens or speaks into the phone. Energy is harvested from two separate sources, ambient radio signals transmitted by a base station up to 31 feet away, and power is harvested from ambient light with a tiny solar cell to allow communication with a base station that was 50 feet away.

 

 

Key EventDate
Contest Launches:14th in August 2019
Qualifier Doc:4th in October 2019
Contest Closes / Volunteer Judging:14th in October 2019
Winners Announcement:21st in October 2019

 

 

Your Chance to Win

 

Be Original
Stick to the Theme
  • You could come up with a clever name that make's your project memorable!
    • This project is your baby! Part of the fun of bringing something new into the world is coming up with a name.
  • Your project could introduce something new or that is not commercially available or affordable!
  • If you have an idea for a project that doesn't fit the current theme then submit your idea in the comments section of the monthly poll.
List the Steps
Submit Video Proof
  • Provide the steps you took to complete your project (text, video, or images).
    • This could be a step by step how-to-guide, vlog, schematics, coding, napkin drawings, voice narration, or whatever you think will be useful!
  • If it doesn't work that's fine, this is more about the journey than the end product.
  • A short video is all that is required but you can shoot as much video as you like.
  • You are encouraged to be creative and have as much fun as possible!

 

Your Project Examples

 

Energy Harvesting
Building a Solar Charger Tilt Solar Light
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
Energy Harvesting
Carbon Monoxide Detector: The Road So Far Putting it all together: hardware and software for harvesting!
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
Your Prizes

 

One Grand Prize Winner Wins an Energy Harvesting to Go Kit + a $200 Shopping CartThree First Place Winners Win a $100 Shopping Cart
  • One Grand Prize Winner Wins an Energy Harvesting to Go Kit + a $200 Shopping Cart!
  • 3 First Place Winners Win a $100 Shopping Cart!
imageimage
Buy NowBuy Now
IC-744885IC-744885 is a development platform for Energy Harvesting Solution To Go which provides very easy access to energy harvesting technologies. The transfer of this solution to the development of a batteryless product is made easy by the right selection of components, schematics and software examples. The two basic parts of the kits are an energy harvesting board and the Giant Gecko starter kit. There are four linear voltage converters on the multi source energy harvesting board. They are optimized for different energy sources like for solar, electromagnetic, piezo electric or thermal energy converters. The energy harvesting board provides an integrated solar cell and a thermo generator for immediate evaluation.
  • EFM32 Giant Gecko starter kit provides evaluation of energy friendly EFM32 Gecko family MCU
  • On board EFM32GG990F1024 with ARM Cortex M3
  • Debugging with a SEGGER J-Link debugger
  • Energy debugging with an integrated Advanced Energy Monitoring (AEM) with voltage monitoring
  • 4 harvesters for different source types
  • On board solar cell and thermo electric generator  
  • Connectors for optional external generators

 

Your Project, Your Ideas!

 

 

About Project14
Directions

Every month you'll have a new poll where you'll get to decide an upcoming project competition, based on your interests, that will take place a couple of months in advance. Themes are broad in scope so that everyone can participate regardless of skill set.

 

What are Monthly Themes?

  • Every month (around the 14th of each month) a new theme will be posted on Project14.
  • Submit your ideas (proposals) for your projects to get feedback from the rest of the community.
  • Submit a project entry in the Theme space once you start working on it.

 

What are Monthly Theme Polls?

  • Every month (around the 14th of each month) there is a project theme poll.
  • Vote on which project competition you want to see for the following upcoming theme.
    • The themes voted on during the previous poll decided the upcoming theme.
    • If you submit an idea for a theme that is not used then it can still be used in a future poll.
  • Themes comments and ideas from the comments section of the project theme poll.

Step 1: Log in or register on element14, it's easy and free.

Step 2: Post in the comments section below to begin a discussion on your idea. Videos, pictures and text are all welcomed forms of submission.

Step 3: Submit a blog post of your progress on your project by the end of the month.  You are free to submit as many blog entries as you like until the beginning of the next theme.

 

Be sure to include video proof of your project!

 

Visit:  Energy Harvesting  or tag your project blog EnergyHarvestingCH

 

You have until October 14th End of Day to submit your completed project!

 

A jury consisting of your peers will judge project submissions!

 

In the Comments Below:  What Ideas do You Have for Projects that Harvest Energy from Wasted Energy Sources?

 

The Project that Does the Best Job of Inspiring the World to Reuse Wasted Energy Wins an Energy Harvesting Kit to Go!

  • electromagnetic harvesting
  • kinetic energy
  • piezoelectric_energy_harvesting
  • energyharvestingch
  • wind harvesting
  • thermoelectric energy harvesting
  • vibration harvesting
  • piezo power scavenging
  • vibrational harvesting
  • rf harvesting
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • vlasov01
    vlasov01 over 7 years ago +6
    I've created and implemented a Smart Shower project . It monitors water consumption and its temperature. I've hacked a cheap water flow sensor (Water control DN15 1-30L/min M100) by adding a temperature…
  • dougw
    dougw over 7 years ago +4
    One other type of energy scavenging is mechanical. Regenerative braking is an example, but any motion or momentum can be converted to electrical energy. There are systems to convert walking motion to electrical…
  • genebren
    genebren over 7 years ago +3
    Three other types of harvesting that I have seen, that are more of storage-based harvesting are: Mechanical - Using a high speed fly wheel system, as a UPS type of storage. The wheel is spun up slowly…
Parents
  • calboy102
    calboy102 over 7 years ago

    well i am thinking what if we improve the efficiency of solar using thermoelectric devices on the back sides of the panels to help cool them thus making them more efficient and at the same time make energy with the thermoelectric devices themselves. im not sure how much of an improvement this will make but i have 5.5kw of ground mounted solar with easy access to the backs of the panels i think i am going to experiment with this and see what kind of results i may get. the panels in full sunlight get so hot you cannot touch them so i figure you could produce a fair amount of power with thermoelectric devices and mabee some small fans to move air threw the heat sinks. i doubt that no one has thought of this before so it may only increase efficiency a minimal amount but hey who knows im gonna get to work on it right now in fact ill post my results when i get them hopefully its the best idea since sliced bread.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to calboy102

    Cooling the panels is a good idea - their efficiency increases as the temperature is decreased.

    Thermoelectric cooling is great because it is solid state and quick, but also has a couple of issues:

    • Individual devices aren't usually bigger than 6 cm because of thermal stresses
    • They require significant power to operate and need a good (big) heat sink to work well
    • It costs less to run a refrigerator than a TEC of equivalent cooling

    I don't know if it is cost effective to use a TEC on solar cells, but it would be interesting to know your findings.

    There are other methods of cooling that can help. Some installations run cool water down the face of their solar cells.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • calboy102
    calboy102 over 7 years ago in reply to dougw

    i am thinking more using them to absorb the heat and cooling them activly with airflow to produce power from the thermoelectricc devices themselves im not sure how much energy could be really gathered but the panels are to hot to touch in full sunlight so there is definitely  enough heat there to generate power thermoelectrically

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to calboy102

    You could also cool them passively with a large heatsink (placed on the opposite side of the solar panel) giving you a strong ambient sink source.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • calboy102
    calboy102 over 7 years ago in reply to calboy102

    so anyone know of now of a more efficient thermoelectric device other than pelters im unable to generate enough voltage with them to turn on my charge controller i have about 30 of them hooked up and am getting pleanty of current from them but i need 45 volts for the charge controller i have and im barley getting 20v

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to calboy102

    Robert,

     

    I am unaware of higher voltage thermoelectric devices, but you might be able to use a boost converter circuit to increase the voltage to 45 volts (albeit at a reduced current).

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • calboy102
    calboy102 over 7 years ago in reply to genebren

    each one of these devices is rated 12v but i assume this is just the max voltage they are able to handle when used as an active cooler not what they should be producing when used as a generator am i correct in this assumption? or should i be able to obtain 12v each?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to calboy102

    Robert,

     

    This information is from the Wikipedia site (https://en.wikipedia.org/wiki/Thermoelectric_generator )

     

    Besides low efficiency and relatively high cost, practical problems exist in using thermoelectric devices in certain types of applications resulting from a relatively high electrical output resistance, which increases self-heating, and a relatively low thermal conductivity, which makes them unsuitable for applications where heat removal is critical, as with heat removal from an electrical device such as microprocessors.

    • High generator output resistance:  In order to get voltage output levels in the range required by digital electrical devices, a common approach is to place many thermoelectric elements in series within a generator module. The element's voltages increase , but so does their individual output resistance. The maximum power transfer theorem dictates that maximum power is delivered to a load when the source and load resistances are identically matched. For low impedance loads near zero ohms, as the generator resistance rises the power delivered to the load decreases. To lower the output resistance, some commercial devices place more individual elements in parallel and fewer in series and employ a boost regulator to raise the voltage to the voltage needed by the load.
    • Low thermal conductivity: Because a very high thermal conductivity is required to transport thermal energy away from a heat source such as a digital microprocessor, the low thermal conductivity of thermoelectric generators makes them unsuitable to recover the heat.
    • Cold-side heat removal with air: In air-cooled thermoelectric applications, such as when harvesting thermal energy from a motor vehicle's crankcase, the large amount of thermal energy that must be dissipated into ambient air presents a significant challenge. As a thermoelectric generator's cool side temperature rises, the device's differential working temperature decreases. As the temperature rises, the device's electrical resistance increases causing greater parasitic generator self-heating. In motor vehicle applications a supplementary radiator is sometimes used for improved heat removal, though the use of an electric water pump to circulate a coolant adds an additional parasitic loss to total generator output power. Water cooling the thermoelectric generator's cold side, as when generating thermoelectric power from the hot crank case of an inboard boat motor, would not suffer from this disadvantage. Water is a far easier coolant to use effectively in contrast to air.

     

    The rated voltage likely relates to the maximum power transfer limit (based on the devices output impedance).

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago in reply to calboy102

    Robert,

     

    This information is from the Wikipedia site (https://en.wikipedia.org/wiki/Thermoelectric_generator )

     

    Besides low efficiency and relatively high cost, practical problems exist in using thermoelectric devices in certain types of applications resulting from a relatively high electrical output resistance, which increases self-heating, and a relatively low thermal conductivity, which makes them unsuitable for applications where heat removal is critical, as with heat removal from an electrical device such as microprocessors.

    • High generator output resistance:  In order to get voltage output levels in the range required by digital electrical devices, a common approach is to place many thermoelectric elements in series within a generator module. The element's voltages increase , but so does their individual output resistance. The maximum power transfer theorem dictates that maximum power is delivered to a load when the source and load resistances are identically matched. For low impedance loads near zero ohms, as the generator resistance rises the power delivered to the load decreases. To lower the output resistance, some commercial devices place more individual elements in parallel and fewer in series and employ a boost regulator to raise the voltage to the voltage needed by the load.
    • Low thermal conductivity: Because a very high thermal conductivity is required to transport thermal energy away from a heat source such as a digital microprocessor, the low thermal conductivity of thermoelectric generators makes them unsuitable to recover the heat.
    • Cold-side heat removal with air: In air-cooled thermoelectric applications, such as when harvesting thermal energy from a motor vehicle's crankcase, the large amount of thermal energy that must be dissipated into ambient air presents a significant challenge. As a thermoelectric generator's cool side temperature rises, the device's differential working temperature decreases. As the temperature rises, the device's electrical resistance increases causing greater parasitic generator self-heating. In motor vehicle applications a supplementary radiator is sometimes used for improved heat removal, though the use of an electric water pump to circulate a coolant adds an additional parasitic loss to total generator output power. Water cooling the thermoelectric generator's cold side, as when generating thermoelectric power from the hot crank case of an inboard boat motor, would not suffer from this disadvantage. Water is a far easier coolant to use effectively in contrast to air.

     

    The rated voltage likely relates to the maximum power transfer limit (based on the devices output impedance).

     

    Gene