Hardware Hacking
  • Challenges & Projects
  • Project14
  • Hardware Hacking
  • More
  • Cancel
Hardware Hacking
Forum Hardware hacking an electric fan heater without burning the house down
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hardware Hacking to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 14 subscribers
  • Views 6591 views
  • Users 0 members are here
  • hardwarehackingch
Related

Hardware hacking an electric fan heater without burning the house down

BigG
BigG over 6 years ago

I recently purchased a 2kW electric fan heater for $12 (it was on sale). This was an offer too good to refuse, especially as the latest Project14 competition is hardware hacking.

 

image

 

These fan heaters, like any other personal heater, are great for the winter months.

 

However, as I have on the very odd occasion left an oil heater on over night (it is very easily done), I certainly wouldn't want to do the same with an electric fan heater.

 

So I want to add in some "smarts" or electronics to ensure that it can automatically turn off if I leave the room etc. and it would also be handy to remotely adjust heat and fan speed.

 

The nice thing about this particular fan heater is that it has a safety cut off switch, should it tip over. I thought that this would be my starting point for my project, as this part can be readily enhanced.

 

image

 

 

The part I am struggling with is how to or what electronic options could I use to hack the heater settings switch, which is mechanical. How could I do this electronically, bearing in mind we are dealing with mains voltage.

 

{gallery:autoplay=false} Heater Settings Switch

image

image

 

And the other question is what options are out there on how to hack the fan speed controller... this also is mains voltage, so I'm out of my depth in terms of using a digital potentiometer, for example.

 

image

 

Any suggestions / ideas would be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 6 years ago in reply to shabaz +1
    I am still unpacking and tearing it down myself to understand the wiring and the rest. I've yet to sketch out a wiring diagram and it's quite hard to capture the key elements in photos. It looks like two…
  • shabaz
    shabaz over 6 years ago in reply to BigG +1
    Hi Colin, I was looking at your photos earlier, and think that's a bimetallic strip (it bends when it gets hot, and self-disconnects). the rotary control just adjusts the point it occurs by moving it closer…
  • ralphjy
    ralphjy over 6 years ago +1
    Very interesting teardown. Always fun figuring out these electromechanical gadgets. You've almost inspired me to hack an old thermostatically controlled window fan but summer is here and I use it all the…
  • BigG
    BigG over 6 years ago

    I'm assuming the switch on the heater is a 4-way 2 pole switch, similar to this more robust version: https://uk.farnell.com/schneider-electric/k1f013qch/rotary-switch-2-pole-5-6a-230v/dp/3108333

     

    As such, I started looking at 4 way double pole power relays and I found that there are a few options available, such as this one:

     

    https://uk.farnell.com/schneider-electric/rxm4ab2jd/relay-4pdt-250vac-6a/dp/2056435

     

    Looking at the photo of the fan switch, it looks like there are two ratings one at 6A and the other at 15A. Now, if I went for a 4PDT relay rated at 15A, the price shoots up for that rated current and for the price of one 4PDT relay I could buy two fans.

     

    So I am wondering if I could craft my own hybrid relay circuit using a suitably rated DPDT or SPST power relay, where one is for 15A and the other one is for 6A. This could saves quite a few bob but the circuit wiring will need thought as I wouldn't want a case of two relays turning on at the same time.

     

    Any suggestions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 6 years ago

    I've worked out a possible logic table for the fan and the two heater elements.

     

    image

     

    So I think 2 x SPST (NO) 16A relays (not sure if this could be combined somehow) and then 1 x SPST(NO) 6A relay would work in this context.

     

    Would this be correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to BigG

    It's hard to say, I'm not sure I understand the existing wiring unfortunately : (

    It might be two separate elements, but I've never taken apart a modern fan heater.

    Heaters are quite high-power, so might need some care if modifying, since wires could get hot.

    This is quite an advanced mod, not sure how it will be implemented, will the relays and circuitry be installed inside the heater? It could he hard to install everything in there.

    It could be way easier to use a remote controlled mains socket adapter, but it may take some of the fun out of the project too, if the aim was to modify the heater product itself.

    So, not really sure what to suggest : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 6 years ago in reply to shabaz

    I am still unpacking and tearing it down myself to understand the wiring and the rest.

     

    I've yet to sketch out a wiring diagram and it's quite hard to capture the key elements in photos.

     

    It looks like two separate elements to me based on the wiring.

     

    image

     

     

    shabaz  wrote:

     

    Heaters are quite high-power, so might need some care if modifying, since wires could get hot.

    This is quite an advanced mod, not sure how it will be implemented, will the relays and circuitry be installed inside the heater? It could he hard to install everything in there. Will the relays and circuitry be installed inside the heater?

     

    No the idea is to remove this top covering and then have the control hardware outside of the enclosure. Not sure just yet as to where to place. As you say, the wires can get quite hot.

     

    image

     

    It's actually quite neatly designed, in my opinion.

     

    {gallery:autoplay=false} Motor

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago

    When I started reading you post I thought, why didn't I think of that. My initial response is how fail safe the mains using solid state components like triac verses relays. A logic device that monitors the environment controls the triac. The logic device gives me the advantage of creating doors to options that I can come back to and use when I need them. Unfortunately this type of design is not cost efficient and you wind up with project like a car block heater being controlled with a Raspberry Pi. It is cool but way to expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 6 years ago in reply to colporteur

    "It is cool but way to expensive."

     

    A common trait amongst many entrepreneurs is "naive optimism". They set off on a quest believing they can make a difference without knowing the full picture. Then when looking back, years later having done it, they realise that if they knew what they know now they would never have begun that journey in the first place.

     

    In this case it's beginning to look like it's going to be pricey before the journey has even started. Still, I had forgotten about triac switches. So, thanks for that. It may just be the jolt I'm looking for to spark further ideas...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 6 years ago

    The part that has me perplexed is the mechanism behind the dial:

     

    image

    What is this component called and how does it work. It looks to me like a beefy potentiometer with an on-off switching mechanism, but not sure has cannot confirm via google (and how did I survive before googling).

     

    image

    image

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to BigG

    Hi Colin,

     

    I was looking at your photos earlier, and think that's a bimetallic strip (it bends when it gets hot, and self-disconnects). the rotary control just adjusts the point it occurs by moving it closer or further away by a fraction.

    These were popular in older thermostats (nowadays it will be a semiconductor or perhaps a thermistor, and an electronic circuit, but the older (but quite reliable) designs had the bimetallic strip.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 6 years ago

    Very interesting teardown.  Always fun figuring out these electromechanical gadgets.  You've almost inspired me to hack an old thermostatically controlled window fan but summer is here and I use it all the time image.  Plus have too many other projects - never enough time.

     

    I'll be watching to see what you come up with....   Have fun hacking.

     

    Also meant to ask - what is the meaning of the symbol in the picture?

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 6 years ago in reply to ralphjy

    Thanks. Yes, not sure how far I'll get by July 14 for the Project 14 hardware hacking deadline as this project requires a cautious "spark free" approach. I believe that symbol indicates that you should not hang clothes over the fan heater.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>