IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - How Long until the Next Recharge?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Mar 2019 8:05 PM Date Created
  • Views 10178 views
  • Likes 17 likes
  • Comments 33 comments
  • mqtt
  • p14 mkr 1010
  • arduino_mkr_wifi_1010
  • aws
  • ssl
  • iotcloudch
Related
Recommended

Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - How Long until the Next Recharge?

Jan Cumps
Jan Cumps
16 Mar 2019
image

IoT: In the Cloud

Enter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

My project for Arduino Day 2019 is an autonomous sensor device that reports data from a (randomly chosen) sensor and how long it's expected to run before you need to recharge its battery.

The focus is not on the sensor (although I'll try to make that meaningful too)

I want to build a base that can be used for other designs in the Cloud that need battery monitoring.

 

I want to have this device reporting how long it's expected to continue living without charging, and raise alarm at near death.

image

I will be using a 3.7 V LiPo battery with a charge / recharge manager to monitor the battery health. That will tell me how much power budget I have.

And I want to specify my design's power profile to predict how much energy it will use in the future.

With that data I can predict how long it will run by itself.

 

An additional goal is to make the design low-power.

 

Ingredients:

  • WiFi
  • Secure MQTT with Certificate based authentication
  • Amazon Web Sevices (AWS)
  • Low Power
  • Battery Management - external charge circuit with fuel gauge

 

image

 

Step 1: Low Power operation

 

My design is going to sleep most of the time.

At predefined wake-up intervals, it'll do its business (a sensor query and battery check).

It will post data to an Amazon Web Service, where that info can be collected and acted upon.

 

image

 

Because I want to start the design with low power use as a basis, I decided to investigate that first.

Arduino has published a Low Power Library for SAMD21 based boards. I'm using it's TimedWakeup sketch as the core for my program.

This example puts the device to sleep for a given period. At each wakeup, it calls an interrupt handler, then runs one loop().

That's a decent start for my low power device.

 

Library dependencies:

  • RTCZero: real time clock library for Arduino Zero. Also works on this MKR 1010.
  • Arduino Low Power: Functions to make the MKR WIFI 1010 go to sleep. I use the RTC to make it wake up at given intervals.

 

Most of the time, the biggest consumer is that the green ON LED was is always lit.

That consumes 7.7 mA. That's why it's marked NO on the pcb image.

I removed it from the Arduino.

 

image

image: the ON LED desoldered from the pcb.

 

TimedWakeup

 

That's the name of the sketch from the Low Power lib that I use as starting point.

At the end of each loop(), it tells the Arduino to go sleep for a while.

You can choose the sleep mode: sleep or deep sleep, by defining DEEP_SLEEP as 0  or 1.

At wakeup, it first calls an interrupt service routine.

You can perform some quick things there, like setting flags. Don't put slow code in the ISR.

 

Then, it lets the loop() execute another cycle and goes back to sleep.

Repeat forever.

 

Because it's hard to re-program a device that's in sleep mode most of the time (the USB port is inactive during sleep), I made a construct to keep it awake when needed.

When you drive D0 high, the firmware will not call the next sleep mode and you can happily reprogram the Arduino.

 

 

#include "ArduinoLowPower.h"

#define SLEEP_MILLIS 900000U
#define DEEP_SLEEP 1
#define PIN_KEEPAWAKE 0 

void setup() {
  pinMode(PIN_KEEPAWAKE, INPUT_PULLDOWN);
  LowPower.attachInterruptWakeup(RTC_ALARM_WAKEUP, lpISR, CHANGE);
}

void loop() {
  // Triggers a 2000 ms sleep (the device will be woken up only by the registered wakeup sources and by internal RTC)
  // The power consumption of the chip will drop consistently
  if (!digitalRead(PIN_KEEPAWAKE)) { // skip sleep if D0 is driven high.
#if DEEP_SLEEP == 1    
    LowPower.deepSleep((uint32_t)(SLEEP_MILLIS));
#else 
    LowPower.sleep((uint32_t)(SLEEP_MILLIS));
#endif
  }
}

void lpISR() {
  // This function will be called once on device wakeup
  // You can do some little operations here (like changing variables which will be used in the loop)
  // Remember to avoid calling delay() and long running functions since this functions executes in interrupt context
}

 

 

 

Step 2: Hardware

 

image

image: connections between the battery pack and the MKR WIFI 1010

 

 

Why an External Battery Manager?

 

The MKR WIFI 1010 has a battery manager on board. But that one can't report battery health.

I'm using a battery charger with embedded fuel gauge (the element14 /TI Battery BoosterPack - modded for efficiency).

That one has a bq27510-G3bq27510-G3 Li-ion battery fuel gauge on board that maintains stats on the battery capacity.

I can ask it how many Ah remain in the battery, an indication for how long it can survive before charging is needed.

 

image

image: fuel gauge and battery charger from the BoosterPack. Source: BOOSTXL-BATTPACK User's Guide

 

 

i2c Bus

 

There's a decent amount of devices connected to the i2c bus:

  • WiFI module
  • Battery Charger (that I don't use)
  • CryptoAuthentication Device
  • External fuel gauge IC

 

The Arduino has 4k7 pull-ups on board. I disabled the ones on the battery management module.

 

Step 3: Collect Battery Statistics

image

image: fuel gauge standard commands available via i2c. Source: bq27510-G3 datasheet

 

Battery Statistics Sketch

 

Our very own Robert Peter Oakes wrote a sketch to read the statistics from the fuel gauge.

It worked straight way on the MKR WIFI 1010.

image

image: the MKR WIFI 1010 runs Peter Oakes' sketch to get data from the Fuel Tank BoosterPack

 

Definition of the not-so-common stats:

TTE: Time-to-empty

TTF: Time-to-full

SOC: State-of-charge in percent related to FCC

FCC:  Full charge capacity. Total capacity of the battery compensated for present load current, temperature, and aging effects (reduction in chemical capacity and increase in internal impedance).

DCAP: Design Capacity

RCAP: Remaining Capacity

FRM:filtered compensated battery capacity remaining

 

 

Calculate Remaining Authonomy

 

There's a rule of thumb approach on the Arduino website: https://www.arduino.cc/en/Tutorial/MKR1000BatteryLife

The formule they use is:

Battery Life = (Battery Capacity) / (Average Current Consumption) * 0.7

When the battery is 70 %discharged, they advise you to charge it again, to avoid deep discharge and deal with variations (like temperature).

I'm taking over the 70% rule.

However, because I have a good estimate of remaining capacity from the fuel gauge, I will not take in account the on-time and average current consumption to calculate the battery statistics.

I will use the average current consumption to extrapolate remaining on-time though.

Measuring that average current is done in a different blog post. I will use the results here once that's finished.

 

Step 4: Set up the Amazone Web Service

 

Secure Connection

 

Setting up a secure connection with AWS is a topic on its own. Arduino has provided an excellent how-to that brings you from "Zero" to "MQTT Working".

I dedicated a separate blog post on that topic.

image

 

Use the Data and AWS Rules

 

In this blog post I'm focusing on getting the data safely to the AWS MQTT server.

I'm writing another post on how to move it from the MQTT server to a database, how to report on it, and how to set up a rule if the battery capacity drops below 70%.

It is a topic that is fully independent from the device design, so a separate post will be less clutter. And I still have to learn it image.

 

(edit: I learned it now. Here is the flow between the AWS services, for data capture,  analysis and alerting)

Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - AWS, Graphs and Alerts

image

 

Step 5: Send Structured MQTT Messages

 

JSON

 

To make it easier to parse data on the AWS side, I want to structure the payload.

I'm formatting the info into a JSON structure. That structure holds data name and value, and can be extracted without manual parsing later.

I'm conservative here, and use printf to construct the data. The better me would create a class that has members for all data points and a method to stream itself to a JSON string.

Maybe later...

 

void publishMessage() {
#if DEBUG_TO_SERIAL == 1
  Serial.println("Publishing message");
#endif

  char output[80];
  // send message, the Print interface can be used to set the message contents
  mqttClient.beginMessage("MKR1010/batterystats");
  mqttClient.print("{ "); // JSON START
  
  sprintf(output, "\"volts\": %d", Volts);
  mqttClient.print(output);

  sprintf(output, ", \"temp\": %d", Temp);
  mqttClient.print(output);

  sprintf(output, ", \"soc\": %d", SOC);
  mqttClient.print(output);

  sprintf(output, ", \"dcap\": %d", DCAP);
  mqttClient.print(output);

  sprintf(output, ", \"rcap\": %d", RCAP);
  mqttClient.print(output);

  sprintf(output, ", \"frcap\": %d", FRCAP);
  mqttClient.print(output);

  sprintf(output, ", \"tte\": %d", TTE);
  mqttClient.print(output);

  mqttClient.print(" }"); // JSON END
  mqttClient.endMessage();
}

 

In the AWS testbed, you can see the message arriving:

 

image

 

 

The sketch is attached.

 

related blog posts
Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - How Long until the Next Recharge?
Arduino MKR WIFI 1010 and Amazon Web Services: Safe MQTT with SSL and Certificate
Project14 | IoT in the Cloud: Make Use of a Wireless Technology and a Cloud Provider!
Keithley DMM6500: Measure Amp-Hours of an Arduino MKR WIFI 1010
Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - AWS, Graphs and Alerts
Arduino MKR 10xx, ETH Shield and Amazon Web Services: Safe MQTT with SSL and Certificate
Attachments:
Project14_Arduino_Day.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps +4
    Jan Cumps wrote: So I won a price with this design . An Arduino MKR GSM 1400, MKR CAN Shield, MKR-RS485 Shield, MKR Eth Shield, and a $100 Shopping Cart. ... I started testing the Arduino MKR GSM 1400…
  • Jan Cumps
    Jan Cumps over 7 years ago +3
    I've added the obligatory video www.youtube.com/watch
  • Jan Cumps
    Jan Cumps over 7 years ago +3
    So I won a price with this design . An Arduino MKR GSM 1400, MKR CAN Shield, MKR-RS485 Shield, MKR Eth Shield, and a $100 Shopping Cart. Here's how I plan to spend the cart: 1 2725884 5 IRF3205ZSTRLPBF…
  • tariq.ahmad
    tariq.ahmad over 7 years ago in reply to Jan Cumps

    That's a good idea!   Hoping to have a Mesh Network competition sometime next year and will be sure to mention RF in the description.   Likewise, will mention a wireless Mesh Network as a possibility in the upcoming theme doc. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to tariq.ahmad

    tariq.ahmad  wrote:

     

    The RF (Radio Frequency) Competition is right around the corner....   image

    The poll was mentioning Mesh networks. Would be great if that topic could stretch a little so that "all things RF" could be snugged in.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tariq.ahmad
    tariq.ahmad over 7 years ago in reply to Jan Cumps

    The RF (Radio Frequency) Competition is right around the corner....   image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    There's a sketch that shows the available providers and the signal strength to the connected provider.

     

    image

     

    I have an extensive antenna kit here with several designs for GSM range. Unfortunately the kit uses µSMA (JSC) and the Arduino has a U.FL connector ...

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    So I won a price with this design image.

     

    An Arduino MKR GSM 1400, MKR CAN Shield, MKR-RS485 Shield, MKR Eth Shield, and a $100 Shopping Cart.

    ...

     

    I started testing the Arduino MKR GSM 1400. I had to purchase a GSM SIM card first.

    I tried to buy one from the typical IOT SIM card providers (a card as used in alarms and IoT devices).

    They aren't interested in selling a single card, or providing a sample if you don't have a business case for higher volume purchases later on.

    So I bought the cheapest customer SIM card available in Belgium that works with prepaid budget.

     

    The test worked perfect:

      imageimage

     

    I'll write a blog later on. Thanks Project14 and tariq.ahmad for the goodies.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
>