NanoRama
  • Challenges & Projects
  • Project14
  • NanoRama
  • More
  • Cancel
NanoRama
Blog Arduino Nano -- controlling things using a RC controllers - Servos
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NanoRama to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: carmelito
  • Date Created: 10 May 2020 9:12 PM Date Created
  • Views 6760 views
  • Likes 8 likes
  • Comments 5 comments
  • flysky
  • arduino-ide
  • rc remote controller
  • servo
  • nanoramach
Related
Recommended

Arduino Nano -- controlling things using a RC controllers - Servos

carmelito
carmelito
10 May 2020
image

NanoRama

Enter Your Project for a chance to win a Nano Grand Prize bundle for the most innovative use of Arduino plus a $400 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

This blog post will show you how you can use a FLYSKY RC controller with an Arduino. As part of this demo project I am using the RC controller to control a couple of servos, this concept can be used to control animatronic projects which need DC motors and servos or any other kind of lighting setup. Basically, this project is just a demo and could have achieved by connecting the servo's directly to the receiver, but my plan as part of a couple of future projects is to drive DC motors/steppers and servos to build battle bots..

 

image

 

Circuit

 

The RC controller receiver FLYSKY AFHDS 6 channel is connected to the Arduino Nano PWM pins, the receiver pins are meant to connect servos

  • Any middle pin on the receiver is connected to 5V pin on the Arduino Nano
  • and the outermost pin is connected to the GND pin
  • CH1 is connected to PWM pin#6 on the Nano, which corresponds to roll on the plane
  • CH2 is connected to PWM pin#10 on the Nano, which corresponds to pitch on the plane

 

And the servos are connect to

  • Servo for the base of the 3D printed arm is connected to PWM pin#3
  • And the Arm is connected to PWM pin#5

image

 

Arduino Code

 

Here is the Arduino Code used to print the RC controller inputs to Serial monitor of the Arduino IDE, and control  the two servos

 

//Created for Project14 using Arduino Nano , Flysky RC(AFHDS) controller and Servos.


#include <Servo.h>


int ch1=6; //roll on the RC controller 
int ch3=10;//pitch on the RC controller 
const int servoBasePin = 3;   //Servo connected to the top base of the 3D printed part  
const int servoTeaArmPin = 5; //Servo connected to the Tea bag holder arm of the 3D printed part  
Servo servoBase;  
Servo servoTeaArm;  
int servoValRoll, servoValPitch;
   
void setup() {
   Serial.begin(9600);
   pinMode(ch1, INPUT);
   pinMode(ch3, INPUT);
   servoBase.attach(servoBasePin);  
   servoTeaArm.attach(servoTeaArmPin);

}


void loop() {
  int ch3Pitch = pulseIn(ch3,HIGH,25000);
  int ch1Roll = pulseIn(ch1,HIGH,25000);
  Serial.print("ch3_pitch : ");
  Serial.println(ch3Pitch);
  Serial.print("ch1_roll: ");
  Serial.println(ch1Roll);


  //Mapping the postions to the servos  
  servoValPitch = map(ch3Pitch, 1000, 2000, 0, 180);//values from pitch from 900 to 2000
  servoBase.write(servoValPitch);    
  servoValRoll = map(ch1Roll, 1000, 2000, 0, 180);//values for roll from 1000 to 2000
  servoTeaArm.write(servoValRoll); 


  delay(50);// increase/decrease the delay to match the movement on the gimbal of the RC controller.
}

 

image

 

 

3D printed parts

For the 3D printed parts i used the STL files from the Automated Tea Dunker , to print all the 3D printed parts I used Hatchbox 1.75mm  PLA  and a Flashforge creator pro.

 

image

 

Here is a quick video demo of the Automated Tea Dunker in action with the RC controller

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
TeaDunkerSTLs.zip
  • Sign in to reply

Top Comments

  • yuricts
    yuricts over 6 years ago +1
    Looking forward to your battle bots. Sooo many things you can do with this... but indeed, first Tea Time! Nice! Thank you for sparkling my mind. Yuri
  • ankur608
    ankur608 over 6 years ago +1
    Nice.
  • dubbie
    dubbie over 6 years ago +1
    Carmelito, This is an interesting project. I have tried something similar to this in the past but I could not get it to operate reliably as sometimes it would miss 'pulses' and then the servos do not get…
Parents
  • dubbie
    dubbie over 6 years ago

    Carmelito,

     

    This is an interesting project. I have tried something similar to this in the past but I could not get it to operate reliably as sometimes it would miss 'pulses' and then the servos do not get a fully continuous sequence. This wasn't a serious problem until we connect the system to a 40 kg mobile robot with dual DC motor drive controlled from an RC servo controller similar to the one you have. When an Arduino was inserted into the loop in order to control acceleration and so on, the system became unreliable as the DC motor module was designed to stop if the RC signal was intermittent - as a safety feature. The health and safety people looking at the robot were very unhappy.

     

    I'm not sure how you could check this as it is quite hard to detect when something isn't there!

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • carmelito
    carmelito over 6 years ago in reply to dubbie

    I think for something which you need more precision and reliability, I would try something like Ardupilot https://ardupilot.org/ , I have not tried it my self, but I know my friend in California who run camera rigs swears by it.. 

    - Carmelito

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to carmelito

    Carmelito,

     

    Thanks for the link. It was very interesting. It looks like some really good things are happening out there. There were even some mobile robots.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago in reply to carmelito

    Carmelito,

     

    Thanks for the link. It was very interesting. It looks like some really good things are happening out there. There were even some mobile robots.

     

    Dubbie