Op-Amp-a-Palooza
  • Challenges & Projects
  • Project14
  • Op-Amp-a-Palooza
  • More
  • Cancel
Op-Amp-a-Palooza
Blog Op-Amp Line Follower - Blog 3 The Line Follower
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Op-Amp-a-Palooza to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 27 Apr 2022 5:34 PM Date Created
  • Views 34606 views
  • Likes 11 likes
  • Comments 11 comments
  • opampsch
  • line follower
  • pwm
  • opamps
  • Op-amp-a-Palooza
Related
Recommended

Op-Amp Line Follower - Blog 3 The Line Follower

javagoza
javagoza
27 Apr 2022
Op-Amp Line Follower - Blog 3 The Line Follower

In the two previous blogs we have been describing the problems we have encountered to finish this project and the decisions made. We were initially going to build a line following vehicle built with op amps with a PID controller. Due to errors in the tests we had to limit the scope of the project and in the end the vehicle is finished but only with proportional control. In this blog we describe the final construction and show proofs of its operation. For the construction of the vehicle we have used parts of the TI-RSLK kit manufactured by Element14, the chassis, the DC motors and the motor driver and power distribution board.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Op-Amp Line Follower

This line following vehicle uses two light dependent resistors, LDR, to capture the light emitted by two yellow LEDs that is reflected by the surface of the track on which the vehicle is traveling. In this way it can detect the black line that reflects less light and by means of a proportional control correct the direction of the vehicle by modifying the speed of the motors.

image

The proportional control of the motors is carried out according to the intensity level of the light received by the photocell sensor. A pulse width modulation PWM signal is used to finely control the motor speed.

The vehicle control can be fine-tuned by means of two potentiometers that adjust the voltage level that will be obtained when the photoresistors are on the lightest surface, the darkest or in between.

The brightest light intensity level received by the sensor, when the sensor is out of line to follow, will result in a higher PWM duty cycle percentage and the darkest light intensity level received by the photoresistor, when the sensor is over line to follow, will result in a lower PWM duty cycle percentage.

image

The vehicle uses only analog electronics. The PWM controller works by comparing a triangle wave with the voltage received from the two sensors. The two sensors are adjusted by a voltage divider. When comparing the received voltage with the ramps of the triangular wave, two comparators generate the amplitude modulated pulses.

The triangle wave generator circuit has three blocks. A block that generates a reference voltage that will be half the supply voltage of the circuit. A comparator circuit with hysteresis or Schmitt Trigger that will generate a square wave and an integrating circuit. By integrating the two constants that the square wave gives us, it will generate two ramps, one increasing and then another decreasing, our triangular wave.

image

Schematics

image

image

R4 = 40 kohm, R6 = 40 kohm. In the PCB R4 = 47 kohm and R6 = 180 kohm, experimental values

image


Bill of Materials:

Product Name Manufacturer Quantity
Trimpot, Multi Turn, Cermet, Top Adjust, 50 kohm, Through Hole, 12 Turns BOURNS 2 Buy Now

Through Hole Resistor, 470 kΩ,

MULTICOMP PRO​ 2 Buy Now

Through Hole Resistor, 10kΩ

MULTICOMP PRO​ 1 Buy Now
 Through Hole Resistor, 100 Ω MULTICOMP PRO 2 Buy Now
 Through Hole Resistor, 120 kΩ MULTICOMP PRO 1 Buy Now
 Through Hole Resistor, 180 kΩ MULTICOMP PRO 1  Buy Now
Through Hole Resistor, 47 kΩ MULTICOMP PRO 1 Buy Now
Capacitor, Metallized PET, 0.1 µF VISHAY 2 Buy Now
LDR, 1 Mohm, 250 mW, 320 V ADVANCED PHOTONIX 2 Buy Now
LM358P Operational Amplifier, 2 Amplifier TEXAS INSTRUMENTS Buy Now
MCP6007 2 OpAmps , 1 MHz, 1.9 V/µs, 1.8V to 5.5V, MSOP, 8 Pin MICROCHIP 2 Buy Now
OP484 Operational Amplifier, Quad, 4 Amplifier, 4.25 MHz ANALOG DEVICES 1 Buy Now

Wire-To-Board Terminal Block, 3.81 mm, 2 Ways, 26 AWG, 16 AWG, Screw

MULTICOMP PRO 4 Buy Now

Prototyping Board, Eurocard, FR2, Epoxy Paper, 1.5mm, 100mm x 160mm

ROTH ELEKTRONIK 1 Buy Now

LED, Yellow, Through Hole, T-1 3/4 (5mm), 20 mA, 2.1 V, 592 nm

MULTICOMP PRO 2 Buy Now

8 Contacts, DIP Socket, 2.54 mm, 

ARIES 1 Buy Now

14 Contacts, DIP Socket, 2.54 mm

ARIES 1 Buy Now

The OP484 is borrowed from this kit: Digilent - Analogue Part Kit

Alternative Parts:

Initially we started working with two MCP6007. See Op-Amp Line Follower - Blog 1 First Steps

MCP6007 2 OpAmps , 1 MHz, 1.9 V/µs, 1.8V to 5.5V, MSOP, 8 Pin MICROCHIP 2 Buy Now
IC Adapter, Fibreglass, 8-MSOP, 2.54mm Pitch Spacing, 7.62mm Row Pitch ROTH ELEKTRONIK 2 Buy Now

Chassis and motors:

Product Name Manufacturer Quantity
Basic Robotic Kit, TI-RSLK Maze Edition, Mobile Platform ELEMENT14 1 Buy Now
Standoff spacers

Protoboard

With the help of Fritzing, we tested the layout of the components on the strip prototyping board.

image

For the prototype we use an Eurocard Prototyping Board , FR2, Epoxy Paper, 1.5mm, 100mm x 160mm, cut so that it does not protrude from the chassis and drilled in 4 places so that it can be fixed to the chassis with standoff spacers.

To cut the tracks that were not supposed to be connected we used a Duratool Track Cutter

image

This was the end result once the components were soldered to the prototyping board.

The fine adjustment potentiometers are located at the rear, in the most stable area of the robot so that the robot does not swing and change the distance of the sensors to the ground while adjustments are made.

A potentiometer has been placed to the right and another to the left corresponding to the motor on each side and in a position such that turning clockwise decreases the speed of the motor and turning counterclockwise of the clock increases the speed of the corresponding motor.

Top view of the control board.

image

And the back of the board.

image

The controller board is connected with Dupont cables to the line sensor and to the the Pololu motor driver and power distribution board.

image

Line sensor board

The line sensor with the two photoresistors and the two yellow LEDs are built on another board.

image

The line sensor is placed in the lower part of the chassis separated with standoff spacers at a small distance from the surface on which the vehicle is going to navigate. If the surface is not completely smooth, you have to leave more space with the ground.

image

Adjusting sensors sensitivity

Using the two trim-pots you can calibrate the sensitivity of the two sensors. The trim pots form a voltage divider with the photoresistors. You can adjust the input voltage to be between the peaks of the triangle wave. The Trim Pot Adjustment Tool for Bourns Trimmers is very useful for this task. Trim Pot Adjustement Tool

image

Quality Assurance

The quality assurance team testing the vehicle.

image

Testing his small circuit:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Trying to fool the line follower

This time the four colored squares along the line act as small traps, swerving the vehicle sharply. Finally the robot corrects the trajectory.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

https://youtu.be/corH7r6yXTU

Next Steps: Playing with Line Follower - Puzzle pieces

Playing with the line follower is really fun. To increase its game possibilities, we have decided to create a series of puzzle pieces that allow us to make configurable paths.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The different kinds of puzzle pieces.

imageimage

imageimage

image

A couple of possible path configurations.

imageimage

Thanks and conclusion

Thanks to the Project14 team for this opportunity to learn more about op amps and to the community members who have read the blogs and given us feedback and guided us through troubleshooting.

Project Blogs

  • Op-Amp Line Follower - Blog 1 First Steps
  • Op-Amp Line Follower - Blog 2 Following the research
  • Op-Amp Line Follower - Blog 3 The Line Follower
  • Sign in to reply
Parents
  • mp2100
    mp2100 over 4 years ago

    Good finish. Even  with the trouble  you had. We can see the proportional (only) control in the video. But it works. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mp2100
    mp2100 over 4 years ago

    Good finish. Even  with the trouble  you had. We can see the proportional (only) control in the video. But it works. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • javagoza
    javagoza over 4 years ago in reply to mp2100

    Thank you. We are amazed at how well it works.