Restoration & Repair
  • Challenges & Projects
  • Project14
  • Restoration & Repair
  • More
  • Cancel
Restoration & Repair
Blog Service my Philips 212 Turntable - Part 2: initial measurements
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Restoration & Repair to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 5 Apr 2020 12:32 PM Date Created
  • Views 18178 views
  • Likes 11 likes
  • Comments 16 comments
  • audio
  • turntable
  • restorerepairch
  • philips
Related
Recommended

Service my Philips 212 Turntable - Part 2: initial measurements

Jan Cumps
Jan Cumps
5 Apr 2020

For Project 14's Restoration and Repair month, I'm going to service a Philips GA-212 Electronic turntable that needs some TLC.

image

In this post, I'll check the overall health of the electronic circuit: power supply voltage and related signals.

 

In this blog, all photos are mine. The exerpts from the service manuals come from vinylengine.com.

 

Supply Voltage

 

"Thou shalt measure voltages."

 

I have worked on this turntable earlier. When I opened it, I had measured the voltage and it was down to less than -7 V, while -9 V is expected.

It turned out that the two electrolytic capacitors on the PCB board were dead. Not uncommon for Philips electrolytics of that time.

image

I replaced them and the power moved to a respectable to -8.85 V.

image

image

 

-8.85 V is good. Good enough. But the service manual says -9 V.

So I adjusted the trimmer until the specified voltage was set.

 

image

 

Here's the result. Very close to the expected level.

 

image

 

 

Auto Switch-Off LDR

 

The auto switch-off doesn't work. It's part of the start / stop circuit of the turntable.

The LDR is mounted under a light bulb that's always on when the TT is powered.

 

image

 

When the arm reaches the end of the record, an optical filter blocks the light reaching the LDR, and changes its resistance.

 

image

If you look at the optical filter, you'll notice that it has a funnel-form light lock.

 

image

 

 

This is a nifty trick. The filter moves very slow over the LDR. A groove per turn.

But because the filter narrows exponential, and there's a high-pass filter after the circuit, the table will only switch off when the narrow part of the filter is reached.

 

image

 

You put the table in START by activating either 33 or 45 RPM (more on that circuit later). Note that the power source is -9 V.

The signal for that arrives via either R532 (33) or R542 (45).

The circuit is held in that state until either the STOP capacitive touch button is used, or the LDR brings TS425 out of conduction.

 

I knew that the stop circuit works, because the capacitive circuit works. The LDR stop doesn't though.

That's when I detected that someone had a go at the circuit before me. Look at the pins of trimmer R465:

 

image

 

I think that the previous service tech was confused by the service manual. The trimmer is a 4K7 one but the schematic says 10K.

However, a later revision of the service manual is in line with my TT.

 

image

 

I can understand that this confused the repair person and that he tried to replace it with a 10K to no avail ...

Anyways, I soldered the 4K7 one properly and trimmed the LDR level as per spec: 0.75 V.

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Thoughts About the Speed Switch Circuit

 

At that same time I did a first overhaul, I also replaced the light bulbs in the capacitive touch buttons. They were blown.

This isn't something you '"just can do". The lamps resistance plays a part in the discrete flip-flops that lets you select the speed.

An interesting circuit. I left away the start / stop sub-circuit in the middle. It's described earlier in this post.

 

image

The two speed controls are capacitive touch switches with a light bulb underneath them.

The bulb under the 33 RPM button will light up when that's the selected speed.

The 45 one in case that the table runs at 45 RPM.

The default status, not shown here, is the off-position.

You can see two bistable multivibrators, each controlling one speed.

 

In the "off" case, both multivibrators are in their "inactive" position: left transistor on, right one off.

When you touch the 33 control, it will flip the upper multivibrator.

TS426 off, TS428 on. The light LA 410 will go on. And the 33 rpm signal will activate the motor circuit for 33 RPM.

Meanwhile, the upper multivibrator (33), via D445 and R538, will lock the lower multivabrator (45). It can't be used as long as the TT is running 33 RPM.

The STOP circuit first has to be activated before you can switch speed.

The 45 RPM side works exactly the same.

 

In essence, this is a state machine with 3 states: Off, 33 or 45.

You can migrate from Off to 33 by touching the 33 control

Off to 45 by touching the 45 control

Either 33 or 45 to Off by touching the Off control or blocking the LDR at the end of the record.

These days, you'd probably use a microcontroller for this?

image

 

Adjust the Speed

 

In the first post in this series, I created a stroboscope. That's the tool we need now to adjust the speed.

image

 

Because I adjusted the supply voltage, a little work is needed to reset the speed dials.

There are two variable resistors per speed. One on the outside, user adjustable. And a trimpot on the inside.

The inside trimmers are the calibrators. They have to be adjusted so that, when the ones on the outside are in the mid position, the speed is spot on.

 

Here it gets a little tricky, because you have to turn trimmers inside the turntable while it spins.

jw0752 mentioned in a previous post that he uses a construct hanging from the ceiling. I use the backs of two chairs (very unsafe).

I balance the TT on them, with the bottom cover removed.

Then there's the fiddly part (remember to put the 2 outside potentiometers in their middle position first) where you kneel, insert a little plastic screwdriver in the correct trimmer.

Then stand up while trying to keep the screwdriver in place. Then switch the table to 45 RPM, and use a stroboscobe to check speed.

Then carefully fiddle with the little trimmer until the speed is spot on.

image

Once 45 is ok, do the same ith 33 RPM. Try to not knock over the whole structure ...

 

On the schematic below, R468 and R470 are the user accessible potentiometers. R469 and R471 are the calibration trimmers.

The circuit is worth looking at. It's a controlled DC motor circuit with feedback.

 

image

 

The feedback circuit is very simple.

The voltage generated by the tacho (mounted on the motor axle) is turned into a signal that will push the driving circuit when the motor slows down, and vise versa.

C730 averages the effect so that it's smooth correction.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago +4
    ~ The End ~ www.youtube.com/watch I deleted the video because of a copyright claim.
  • three-phase
    three-phase over 6 years ago +4
    A very interesting blog to read and great to see the turntable operating - it has been a long long time since I have seen one in someones house. Kind regards
  • jw0752
    jw0752 over 6 years ago +4
    Hi Jan, Great Compromise on working under the table. Reminds me of putting the car up on a hoist. John
Parents
  • neptunium
    neptunium over 5 years ago

    Great article! I also have a 212 in need of some care, so I've been studying the schematic as well. Two of the indicator bulbs are burned out and the auto-shutoff one is probably dead too. I may replace them with LEDs and series-parallel resistor arrangements to keep the same load. Philips actually did that in a later model so I think they would approve.

     

    But what greatly puzzles me is why the designers have used positive ground in this system. Is there any inherent advantage to doing so compared to the ubiquitous negative ground? I've read that on older cars with a positive ground chassis it was done because it allegedly provided a better spark and less galvanic corrosion, but that doesn't apply here. The schematic feels very "upside-down" in places! image

     

    Another oddity is the use of germanium transistors in the power supply. I'm guessing this was done for efficiency/dissipation reasons because of the lower voltage drop?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to neptunium

    neptunium  wrote:

     

    ...

    But what greatly puzzles me is why the designers have used positive ground in this system. Is there any inherent advantage to doing so compared to the ubiquitous negative ground? I've read that on older cars with a positive ground chassis it was done because it allegedly provided a better spark and less galvanic corrosion, but that doesn't apply here. The schematic feels very "upside-down" in places! image

     

    Another oddity is the use of germanium transistors in the power supply. I'm guessing this was done for efficiency/dissipation reasons because of the lower voltage drop?

    You see two artifacts of the early silicon years of Philips.

    Part of the design was still exactly inherited from its predecessors, that were germanium only. You'll find the exact same DC regulation circuit in the previous Philips turntables.

     

    PNP transistors were the stock transistors in the day (the Science Fair 1xx-in-ONE kits had mostly PNP germanium transistors, 2SB56, and their schemas were also often "+ as ground"), and the power supply polarisation reflects that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to neptunium

    neptunium  wrote:

     

    ...

    But what greatly puzzles me is why the designers have used positive ground in this system. Is there any inherent advantage to doing so compared to the ubiquitous negative ground? I've read that on older cars with a positive ground chassis it was done because it allegedly provided a better spark and less galvanic corrosion, but that doesn't apply here. The schematic feels very "upside-down" in places! image

     

    Another oddity is the use of germanium transistors in the power supply. I'm guessing this was done for efficiency/dissipation reasons because of the lower voltage drop?

    You see two artifacts of the early silicon years of Philips.

    Part of the design was still exactly inherited from its predecessors, that were germanium only. You'll find the exact same DC regulation circuit in the previous Philips turntables.

     

    PNP transistors were the stock transistors in the day (the Science Fair 1xx-in-ONE kits had mostly PNP germanium transistors, 2SB56, and their schemas were also often "+ as ground"), and the power supply polarisation reflects that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neptunium
    neptunium over 5 years ago in reply to Jan Cumps

    Thanks for the explanation. It does indeed make sense to further improve upon their existing designs that already work well.

    Another question if I may: the service manual states that C731 (a 10nF in the tacho control section) is used "to prevent generating". What does that mean? Because the tacho generator is always generating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to neptunium

    neptunium  wrote:

     

    Another question if I may: the service manual states that C731 (a 10nF in the tacho control section) is used "to prevent generating". What does that mean? Because the tacho generator is always generating.

    I checked the explanation in all languages (I have a manual in English, Dutch, German and French). They all use the same wording.

    I'd say it is to prevent oscillation.